#include <SPIMSP432E4DMA.h>
§ hwiHandle
HwiP_Handle SPIMSP432E4DMA_Object::hwiHandle |
§ transferComplete
SemaphoreP_Handle SPIMSP432E4DMA_Object::transferComplete |
§ transferCallbackFxn
§ dmaHandle
§ headPtr
§ tailPtr
§ framesQueued
size_t SPIMSP432E4DMA_Object::framesQueued |
§ framesTransferred
size_t SPIMSP432E4DMA_Object::framesTransferred |
§ priTransferSize
size_t SPIMSP432E4DMA_Object::priTransferSize |
§ altTransferSize
size_t SPIMSP432E4DMA_Object::altTransferSize |
§ bitRate
uint32_t SPIMSP432E4DMA_Object::bitRate |
§ dataSize
uint32_t SPIMSP432E4DMA_Object::dataSize |
§ transferTimeout
uint32_t SPIMSP432E4DMA_Object::transferTimeout |
§ activeChannel
uint32_t SPIMSP432E4DMA_Object::activeChannel |
§ busyBit
uint32_t SPIMSP432E4DMA_Object::busyBit |
§ rxScratchBuf
uint16_t SPIMSP432E4DMA_Object::rxScratchBuf |
§ spiMode
§ transferMode
§ format
uint8_t SPIMSP432E4DMA_Object::format |
§ isOpen
bool SPIMSP432E4DMA_Object::isOpen |
The documentation for this struct was generated from the following file: