SPIMSP432E4DMA Hardware attributes. More...
#include <SPIMSP432E4DMA.h>
Data Fields | |
uint32_t | baseAddr |
uint32_t | intNum |
uint32_t | intPriority |
uint16_t * | scratchBufPtr |
uint16_t | defaultTxBufValue |
uint32_t | rxDmaChannel |
uint32_t | txDmaChannel |
uint16_t | minDmaTransferSize |
uint32_t | clkPinMask |
uint32_t | fssPinMask |
uint32_t | xdat0PinMask |
uint32_t | xdat1PinMask |
SPIMSP432E4DMA Hardware attributes.
These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432E4 driverlib these definitions are found in:
intPriority is the SPI peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
uint32_t SPIMSP432E4DMA_HWAttrs::baseAddr |
SSI Peripheral's base address
uint32_t SPIMSP432E4DMA_HWAttrs::intNum |
SSI MSP432E4DMA Peripheral's interrupt vector
uint32_t SPIMSP432E4DMA_HWAttrs::intPriority |
SPIMSP432E4DMA Peripheral's interrupt priority
uint16_t* SPIMSP432E4DMA_HWAttrs::scratchBufPtr |
Address of a scratch buffer of size uint32_t
uint16_t SPIMSP432E4DMA_HWAttrs::defaultTxBufValue |
Default TX value if txBuf == NULL
uint32_t SPIMSP432E4DMA_HWAttrs::rxDmaChannel |
uDMA channel for RX data
uint32_t SPIMSP432E4DMA_HWAttrs::txDmaChannel |
uDMA channel for TX data
uint16_t SPIMSP432E4DMA_HWAttrs::minDmaTransferSize |
Minimum amount of data frames for DMA transfer
uint32_t SPIMSP432E4DMA_HWAttrs::clkPinMask |
Pin mask for SSI CLK
uint32_t SPIMSP432E4DMA_HWAttrs::fssPinMask |
Pin mask for SSI FSS
uint32_t SPIMSP432E4DMA_HWAttrs::xdat0PinMask |
Pin mask for SSI XDAT0
uint32_t SPIMSP432E4DMA_HWAttrs::xdat1PinMask |
Pin mask for SSI XDAT1