Data Structures | Macros | Typedefs | Variables
UARTMSP432E4.h File Reference

Detailed Description

UART driver implementation for a MSP432E4 UART controller.

============================================================================

The UART header file should be included in an application as follows:

Refer to UART.h for a complete description of APIs & example of use.


#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/devices/msp432e4/inc/msp432.h>
#include <ti/devices/msp432e4/driverlib/gpio.h>
#include <ti/devices/msp432e4/driverlib/pin_map.h>
#include <ti/drivers/dpl/ClockP.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/gpio/GPIOMSP432E4.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/utils/RingBuf.h>
Include dependency graph for UARTMSP432E4.h:

Go to the source code of this file.

Data Structures

struct  UARTMSP432E4_FxnSet
 Complement set of read functions to be used by the UART ISR and UARTMSP432E4_read(). Internal use only. More...
 
struct  UARTMSP432E4_HWAttrs
 UARTMSP432E4 Hardware attributes. More...
 
struct  UARTMSP432E4_Object
 UARTMSP432E4 Object. More...
 

Macros

#define UARTMSP432E4_PIN_UNASSIGNED   0xFFFFFFFF
 Indicates a pin is not being used. More...
 
#define UARTMSP432E4_FLOWCTRL_NONE   0
 No hardware flow control. More...
 
#define UARTMSP432E4_FLOWCTRL_HARDWARE   1
 Hardware flow control. More...
 
#define UARTMSP432E4_PA0_U0RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 0, GPIO_PA0_U0RX)
 PA0 is used for UART0 RX. More...
 
#define UARTMSP432E4_PA1_U0TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 1, GPIO_PA1_U0TX)
 PA1 is used for UART0 RX. More...
 
#define UARTMSP432E4_PH1_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 1, GPIO_PH1_U0CTS)
 PH1 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PM4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTM, 4, GPIO_PM4_U0CTS)
 PM4 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PB4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 4, GPIO_PB4_U0CTS)
 PB4 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PE6_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 6, GPIO_PE6_U0CTS)
 PE6 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PG4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 4, GPIO_PG4_U0CTS)
 PG4 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PH0_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 0, GPIO_PH0_U0RTS)
 PH0 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PB5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 5, GPIO_PB5_U0RTS)
 PB5 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PE7_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 7, GPIO_PE7_U0RTS)
 PE7 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PG5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 5, GPIO_PG5_U0RTS)
 PG5 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PB0_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 0, GPIO_PB0_U1RX)
 PB0 is used for UART1 RX. More...
 
#define UARTMSP432E4_PQ4_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 4, GPIO_PQ4_U1RX)
 PQ4 is used for UART1 RX. More...
 
#define UARTMSP432E4_PR5_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 5, GPIO_PR5_U1RX)
 PR5 is used for UART1 RX. More...
 
#define UARTMSP432E4_PB1_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 1, GPIO_PB1_U1TX)
 PB1 is used for UART1 TX. More...
 
#define UARTMSP432E4_PQ5_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 5, GPIO_PQ5_U1TX)
 PQ5 is used for UART1 TX. More...
 
#define UARTMSP432E4_PR6_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 6, GPIO_PR6_U1TX)
 PR6 is used for UART1 TX. More...
 
#define UARTMSP432E4_PP3_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 3, GPIO_PP3_U1CTS)
 PP3 is used for UART1 CTS. More...
 
#define UARTMSP432E4_PN1_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 1, GPIO_PN1_U1CTS)
 PN1 is used for UART1 CTS. More...
 
#define UARTMSP432E4_PE0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 0, GPIO_PE0_U1RTS)
 PE0 is used for UART1 RTS. More...
 
#define UARTMSP432E4_PN0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 0, GPIO_PN0_U1RTS)
 PN0 is used for UART1 RTS. More...
 
#define UARTMSP432E4_PN7_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U1RTS)
 PN7 is used for UART1 RTS. More...
 
#define UARTMSP432E4_PA6_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 6, GPIO_PA6_U2RX)
 PA6 is used for UART2 RX. More...
 
#define UARTMSP432E4_PD4_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 4, GPIO_PD4_U2RX)
 PD4 is used for UART2 RX. More...
 
#define UARTMSP432E4_PA7_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 7, GPIO_PA7_U2TX)
 PA7 is used for UART2 TX. More...
 
#define UARTMSP432E4_PD5_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 5, GPIO_PD5_U2TX)
 PD5 is used for UART2 TX. More...
 
#define UARTMSP432E4_PN3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 3, GPIO_PN3_U2CTS)
 PN3 is used for UART2 CTS. More...
 
#define UARTMSP432E4_PD7_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 7, GPIO_PD7_U2CTS)
 PD7 is used for UART2 CTS. More...
 
#define UARTMSP432E4_PJ3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 3, GPIO_PJ3_U2CTS)
 PJ3 is used for UART2 CTS. More...
 
#define UARTMSP432E4_PN2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 2, GPIO_PN2_U2RTS)
 PN2 is used for UART2 RTS. More...
 
#define UARTMSP432E4_PD6_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 6, GPIO_PD6_U2RTS)
 PD6 is used for UART2 RTS. More...
 
#define UARTMSP432E4_PJ2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 2, GPIO_PJ2_U2RTS)
 PJ2 is used for UART2 RTS. More...
 
#define UARTMSP432E4_PA4_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 4, GPIO_PA4_U3RX)
 PA4 is used for UART3 RX. More...
 
#define UARTMSP432E4_PJ0_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 0, GPIO_PJ0_U3RX)
 PJ0 is used for UART3 RX. More...
 
#define UARTMSP432E4_PA5_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 5, GPIO_PA5_U3TX)
 PA5 is used for UART3 TX. More...
 
#define UARTMSP432E4_PJ1_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 1, GPIO_PJ1_U3TX)
 PJ1 is used for UART3 TX. More...
 
#define UARTMSP432E4_PP5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 5, GPIO_PP5_U3CTS)
 PP5 is used for UART3 CTS. More...
 
#define UARTMSP432E4_PN5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 5, GPIO_PN5_U3CTS)
 PN5 is used for UART3 CTS. More...
 
#define UARTMSP432E4_PJ5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 5, GPIO_PJ5_U3CTS)
 PJ5 is used for UART3 CTS. More...
 
#define UARTMSP432E4_PP4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 4, GPIO_PP4_U3RTS)
 PP4 is used for UART3 RTS. More...
 
#define UARTMSP432E4_PN4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 4, GPIO_PN4_U3RTS)
 PN4 is used for UART3 RTS. More...
 
#define UARTMSP432E4_PJ4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 4, GPIO_PJ4_U3RTS)
 PJ4 is used for UART3 RTS. More...
 
#define UARTMSP432E4_PA2_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 2, GPIO_PA2_U4RX)
 PA2 is used for UART4 RX. More...
 
#define UARTMSP432E4_PK0_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 0, GPIO_PK0_U4RX)
 PK0 is used for UART4 RX. More...
 
#define UARTMSP432E4_PR1_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 1, GPIO_PR1_U4RX)
 PR1 is used for UART4 RX. More...
 
#define UARTMSP432E4_PA3_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 3, GPIO_PA3_U4TX)
 PA3 is used for UART4 TX. More...
 
#define UARTMSP432E4_PK1_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 1, GPIO_PK1_U4TX)
 PK1 is used for UART4 TX. More...
 
#define UARTMSP432E4_PR0_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 0, GPIO_PR0_U4TX)
 PR0 is used for UART4 TX. More...
 
#define UARTMSP432E4_PK3_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 3, GPIO_PK3_U4CTS)
 PK3 is used for UART4 CTS. More...
 
#define UARTMSP432E4_PJ7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 7, GPIO_PJ7_U4CTS)
 PJ7 is used for UART4 CTS. More...
 
#define UARTMSP432E4_PN7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U4CTS)
 PN7 is used for UART4 CTS. More...
 
#define UARTMSP432E4_PK2_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 2, GPIO_PK2_U4RTS)
 PK2 is used for UART4 RTS. More...
 
#define UARTMSP432E4_PJ6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 6, GPIO_PJ6_U4RTS)
 PJ6 is used for UART4 RTS. More...
 
#define UARTMSP432E4_PN6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 6, GPIO_PN6_U4RTS)
 PN6 is used for UART4 RTS. More...
 
#define UARTMSP432E4_PC6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 6, GPIO_PC6_U5RX)
 PC6 is used for UART5 RX. More...
 
#define UARTMSP432E4_PH6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U5RX)
 PH6 is used for UART5 RX. More...
 
#define UARTMSP432E4_PC7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 7, GPIO_PC7_U5TX)
 PC7 is used for UART5 TX. More...
 
#define UARTMSP432E4_PH7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U5TX)
 PH7 is used for UART5 TX. More...
 
#define UARTMSP432E4_PP0_U6RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 0, GPIO_PP0_U6RX)
 PP0 is used for UART6 RX. More...
 
#define UARTMSP432E4_PP1_U6TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 1, GPIO_PP1_U6TX)
 PP1 is used for UART6 TX. More...
 
#define UARTMSP432E4_PC4_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 4, GPIO_PC4_U7RX)
 PC4 is used for UART7 RX. More...
 
#define UARTMSP432E4_PH6_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U7RX)
 PH6 is used for UART7 RX. More...
 
#define UARTMSP432E4_PC5_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 5, GPIO_PC5_U7TX)
 PC5 is used for UART7 TX. More...
 
#define UARTMSP432E4_PH7_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U7TX)
 PH7 is used for UART7 TX. More...
 

Typedefs

typedef void(* UARTMSP432E4_ErrorCallback) (UART_Handle handle, uint32_t error)
 The definition of an optional callback function used by the UART driver to notify the application when a receive error (FIFO overrun, parity error, etc) occurs. More...
 
typedef struct UARTMSP432E4_FxnSet UARTMSP432E4_FxnSet
 Complement set of read functions to be used by the UART ISR and UARTMSP432E4_read(). Internal use only. More...
 
typedef struct UARTMSP432E4_HWAttrs UARTMSP432E4_HWAttrs
 UARTMSP432E4 Hardware attributes. More...
 
typedef struct UARTMSP432E4_Object UARTMSP432E4_Object
 UARTMSP432E4 Object. More...
 
typedef struct UARTMSP432E4_ObjectUARTMSP432E4_Handle
 

Variables

const UART_FxnTable UARTMSP432E4_fxnTable
 

Macro Definition Documentation

§ UARTMSP432E4_PIN_UNASSIGNED

#define UARTMSP432E4_PIN_UNASSIGNED   0xFFFFFFFF

Indicates a pin is not being used.

If hardware flow control is not being used, the UART CTS and RTS pins should be set to UARTMSP432E4_PIN_UNASSIGNED.

§ UARTMSP432E4_FLOWCTRL_NONE

#define UARTMSP432E4_FLOWCTRL_NONE   0

No hardware flow control.

§ UARTMSP432E4_FLOWCTRL_HARDWARE

#define UARTMSP432E4_FLOWCTRL_HARDWARE   1

Hardware flow control.

§ UARTMSP432E4_PA0_U0RX

#define UARTMSP432E4_PA0_U0RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 0, GPIO_PA0_U0RX)

PA0 is used for UART0 RX.

§ UARTMSP432E4_PA1_U0TX

#define UARTMSP432E4_PA1_U0TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 1, GPIO_PA1_U0TX)

PA1 is used for UART0 RX.

§ UARTMSP432E4_PH1_U0CTS

#define UARTMSP432E4_PH1_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 1, GPIO_PH1_U0CTS)

PH1 is used for UART0 CTS.

§ UARTMSP432E4_PM4_U0CTS

#define UARTMSP432E4_PM4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTM, 4, GPIO_PM4_U0CTS)

PM4 is used for UART0 CTS.

§ UARTMSP432E4_PB4_U0CTS

#define UARTMSP432E4_PB4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 4, GPIO_PB4_U0CTS)

PB4 is used for UART0 CTS.

§ UARTMSP432E4_PE6_U0CTS

#define UARTMSP432E4_PE6_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 6, GPIO_PE6_U0CTS)

PE6 is used for UART0 CTS.

§ UARTMSP432E4_PG4_U0CTS

#define UARTMSP432E4_PG4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 4, GPIO_PG4_U0CTS)

PG4 is used for UART0 CTS.

§ UARTMSP432E4_PH0_U0RTS

#define UARTMSP432E4_PH0_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 0, GPIO_PH0_U0RTS)

PH0 is used for UART0 RTS.

§ UARTMSP432E4_PB5_U0RTS

#define UARTMSP432E4_PB5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 5, GPIO_PB5_U0RTS)

PB5 is used for UART0 RTS.

§ UARTMSP432E4_PE7_U0RTS

#define UARTMSP432E4_PE7_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 7, GPIO_PE7_U0RTS)

PE7 is used for UART0 RTS.

§ UARTMSP432E4_PG5_U0RTS

#define UARTMSP432E4_PG5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 5, GPIO_PG5_U0RTS)

PG5 is used for UART0 RTS.

§ UARTMSP432E4_PB0_U1RX

#define UARTMSP432E4_PB0_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 0, GPIO_PB0_U1RX)

PB0 is used for UART1 RX.

§ UARTMSP432E4_PQ4_U1RX

#define UARTMSP432E4_PQ4_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 4, GPIO_PQ4_U1RX)

PQ4 is used for UART1 RX.

§ UARTMSP432E4_PR5_U1RX

#define UARTMSP432E4_PR5_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 5, GPIO_PR5_U1RX)

PR5 is used for UART1 RX.

§ UARTMSP432E4_PB1_U1TX

#define UARTMSP432E4_PB1_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 1, GPIO_PB1_U1TX)

PB1 is used for UART1 TX.

§ UARTMSP432E4_PQ5_U1TX

#define UARTMSP432E4_PQ5_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 5, GPIO_PQ5_U1TX)

PQ5 is used for UART1 TX.

§ UARTMSP432E4_PR6_U1TX

#define UARTMSP432E4_PR6_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 6, GPIO_PR6_U1TX)

PR6 is used for UART1 TX.

§ UARTMSP432E4_PP3_U1CTS

#define UARTMSP432E4_PP3_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 3, GPIO_PP3_U1CTS)

PP3 is used for UART1 CTS.

§ UARTMSP432E4_PN1_U1CTS

#define UARTMSP432E4_PN1_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 1, GPIO_PN1_U1CTS)

PN1 is used for UART1 CTS.

§ UARTMSP432E4_PE0_U1RTS

#define UARTMSP432E4_PE0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 0, GPIO_PE0_U1RTS)

PE0 is used for UART1 RTS.

§ UARTMSP432E4_PN0_U1RTS

#define UARTMSP432E4_PN0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 0, GPIO_PN0_U1RTS)

PN0 is used for UART1 RTS.

§ UARTMSP432E4_PN7_U1RTS

#define UARTMSP432E4_PN7_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U1RTS)

PN7 is used for UART1 RTS.

§ UARTMSP432E4_PA6_U2RX

#define UARTMSP432E4_PA6_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 6, GPIO_PA6_U2RX)

PA6 is used for UART2 RX.

§ UARTMSP432E4_PD4_U2RX

#define UARTMSP432E4_PD4_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 4, GPIO_PD4_U2RX)

PD4 is used for UART2 RX.

§ UARTMSP432E4_PA7_U2TX

#define UARTMSP432E4_PA7_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 7, GPIO_PA7_U2TX)

PA7 is used for UART2 TX.

§ UARTMSP432E4_PD5_U2TX

#define UARTMSP432E4_PD5_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 5, GPIO_PD5_U2TX)

PD5 is used for UART2 TX.

§ UARTMSP432E4_PN3_U2CTS

#define UARTMSP432E4_PN3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 3, GPIO_PN3_U2CTS)

PN3 is used for UART2 CTS.

§ UARTMSP432E4_PD7_U2CTS

#define UARTMSP432E4_PD7_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 7, GPIO_PD7_U2CTS)

PD7 is used for UART2 CTS.

§ UARTMSP432E4_PJ3_U2CTS

#define UARTMSP432E4_PJ3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 3, GPIO_PJ3_U2CTS)

PJ3 is used for UART2 CTS.

§ UARTMSP432E4_PN2_U2RTS

#define UARTMSP432E4_PN2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 2, GPIO_PN2_U2RTS)

PN2 is used for UART2 RTS.

§ UARTMSP432E4_PD6_U2RTS

#define UARTMSP432E4_PD6_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 6, GPIO_PD6_U2RTS)

PD6 is used for UART2 RTS.

§ UARTMSP432E4_PJ2_U2RTS

#define UARTMSP432E4_PJ2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 2, GPIO_PJ2_U2RTS)

PJ2 is used for UART2 RTS.

§ UARTMSP432E4_PA4_U3RX

#define UARTMSP432E4_PA4_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 4, GPIO_PA4_U3RX)

PA4 is used for UART3 RX.

§ UARTMSP432E4_PJ0_U3RX

#define UARTMSP432E4_PJ0_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 0, GPIO_PJ0_U3RX)

PJ0 is used for UART3 RX.

§ UARTMSP432E4_PA5_U3TX

#define UARTMSP432E4_PA5_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 5, GPIO_PA5_U3TX)

PA5 is used for UART3 TX.

§ UARTMSP432E4_PJ1_U3TX

#define UARTMSP432E4_PJ1_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 1, GPIO_PJ1_U3TX)

PJ1 is used for UART3 TX.

§ UARTMSP432E4_PP5_U3CTS

#define UARTMSP432E4_PP5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 5, GPIO_PP5_U3CTS)

PP5 is used for UART3 CTS.

§ UARTMSP432E4_PN5_U3CTS

#define UARTMSP432E4_PN5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 5, GPIO_PN5_U3CTS)

PN5 is used for UART3 CTS.

§ UARTMSP432E4_PJ5_U3CTS

#define UARTMSP432E4_PJ5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 5, GPIO_PJ5_U3CTS)

PJ5 is used for UART3 CTS.

§ UARTMSP432E4_PP4_U3RTS

#define UARTMSP432E4_PP4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 4, GPIO_PP4_U3RTS)

PP4 is used for UART3 RTS.

§ UARTMSP432E4_PN4_U3RTS

#define UARTMSP432E4_PN4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 4, GPIO_PN4_U3RTS)

PN4 is used for UART3 RTS.

§ UARTMSP432E4_PJ4_U3RTS

#define UARTMSP432E4_PJ4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 4, GPIO_PJ4_U3RTS)

PJ4 is used for UART3 RTS.

§ UARTMSP432E4_PA2_U4RX

#define UARTMSP432E4_PA2_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 2, GPIO_PA2_U4RX)

PA2 is used for UART4 RX.

§ UARTMSP432E4_PK0_U4RX

#define UARTMSP432E4_PK0_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 0, GPIO_PK0_U4RX)

PK0 is used for UART4 RX.

§ UARTMSP432E4_PR1_U4RX

#define UARTMSP432E4_PR1_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 1, GPIO_PR1_U4RX)

PR1 is used for UART4 RX.

§ UARTMSP432E4_PA3_U4TX

#define UARTMSP432E4_PA3_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 3, GPIO_PA3_U4TX)

PA3 is used for UART4 TX.

§ UARTMSP432E4_PK1_U4TX

#define UARTMSP432E4_PK1_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 1, GPIO_PK1_U4TX)

PK1 is used for UART4 TX.

§ UARTMSP432E4_PR0_U4TX

#define UARTMSP432E4_PR0_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 0, GPIO_PR0_U4TX)

PR0 is used for UART4 TX.

§ UARTMSP432E4_PK3_U4CTS

#define UARTMSP432E4_PK3_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 3, GPIO_PK3_U4CTS)

PK3 is used for UART4 CTS.

§ UARTMSP432E4_PJ7_U4CTS

#define UARTMSP432E4_PJ7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 7, GPIO_PJ7_U4CTS)

PJ7 is used for UART4 CTS.

§ UARTMSP432E4_PN7_U4CTS

#define UARTMSP432E4_PN7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U4CTS)

PN7 is used for UART4 CTS.

§ UARTMSP432E4_PK2_U4RTS

#define UARTMSP432E4_PK2_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 2, GPIO_PK2_U4RTS)

PK2 is used for UART4 RTS.

§ UARTMSP432E4_PJ6_U4RTS

#define UARTMSP432E4_PJ6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 6, GPIO_PJ6_U4RTS)

PJ6 is used for UART4 RTS.

§ UARTMSP432E4_PN6_U4RTS

#define UARTMSP432E4_PN6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 6, GPIO_PN6_U4RTS)

PN6 is used for UART4 RTS.

§ UARTMSP432E4_PC6_U5RX

#define UARTMSP432E4_PC6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 6, GPIO_PC6_U5RX)

PC6 is used for UART5 RX.

§ UARTMSP432E4_PH6_U5RX

#define UARTMSP432E4_PH6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U5RX)

PH6 is used for UART5 RX.

§ UARTMSP432E4_PC7_U5TX

#define UARTMSP432E4_PC7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 7, GPIO_PC7_U5TX)

PC7 is used for UART5 TX.

§ UARTMSP432E4_PH7_U5TX

#define UARTMSP432E4_PH7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U5TX)

PH7 is used for UART5 TX.

§ UARTMSP432E4_PP0_U6RX

#define UARTMSP432E4_PP0_U6RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 0, GPIO_PP0_U6RX)

PP0 is used for UART6 RX.

§ UARTMSP432E4_PP1_U6TX

#define UARTMSP432E4_PP1_U6TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 1, GPIO_PP1_U6TX)

PP1 is used for UART6 TX.

§ UARTMSP432E4_PC4_U7RX

#define UARTMSP432E4_PC4_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 4, GPIO_PC4_U7RX)

PC4 is used for UART7 RX.

§ UARTMSP432E4_PH6_U7RX

#define UARTMSP432E4_PH6_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U7RX)

PH6 is used for UART7 RX.

§ UARTMSP432E4_PC5_U7TX

#define UARTMSP432E4_PC5_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 5, GPIO_PC5_U7TX)

PC5 is used for UART7 TX.

§ UARTMSP432E4_PH7_U7TX

#define UARTMSP432E4_PH7_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U7TX)

PH7 is used for UART7 TX.

Typedef Documentation

§ UARTMSP432E4_ErrorCallback

typedef void(* UARTMSP432E4_ErrorCallback) (UART_Handle handle, uint32_t error)

The definition of an optional callback function used by the UART driver to notify the application when a receive error (FIFO overrun, parity error, etc) occurs.

Parameters
UART_HandleUART_Handle
errorThe current value of the receive status register. Please refer to the device data sheet to interpret this value.

§ UARTMSP432E4_FxnSet

Complement set of read functions to be used by the UART ISR and UARTMSP432E4_read(). Internal use only.

These functions are intended solely for the UARTMSP432E4 driver, and should not be used by the application. The UARTMSP432E4_FxnSet is a pair of functions that are designed to operate with one another in a task context and in an ISR context. The readTaskFxn is called by UARTMSP432E4_read() to drain a circular buffer, whereas the readIsrFxn is used by the UARTMSP432E4_hwiIntFxn to fill up the circular buffer.

readTaskFxn: Function called by UART read These variables are set and avilalable for use to the readTaskFxn. object->readBuf = buffer; //Pointer to a user buffer object->readSize = size; //Desired no. of bytes to read object->readCount = size; //Remaining no. of bytes to read

readIsrFxn: The required ISR counterpart to readTaskFxn

§ UARTMSP432E4_HWAttrs

UARTMSP432E4 Hardware attributes.

The baseAddr, intNum, and flowControl fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432E4 driverlib these definitions are found in:

  • ti/devices/msp432e4/driverlib/inc/msp432e4xxx.h
  • ti/devices/msp432e4/driverlib/interrupt.h
  • ti/devices/msp432e4/driverlib/uart.h

intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

unsigned char uartMSP432E4RingBuffer[2][32];
const UARTMSP432E4_HWAttrs uartMSP432E4HWAttrs[] = {
{
.baseAddr = UART0_BASE,
.intNum = INT_UART0,
.intPriority = (~0),
.ringBufPtr = uartMSP432E4RingBuffer[0],
.ringBufSize = sizeof(uartMSP432E4RingBuffer[0]),
.errorFxn = NULL
},
{
.baseAddr = UART1_BASE,
.intNum = INT_UART1,
.intPriority = (~0),
.flowControl = UARTMSP432E4_FLOWCTRL_NONE,,
.ringBufPtr = uartMSP432E4RingBuffer[1],
.ringBufSize = sizeof(uartMSP432E4RingBuffer[1]),
.errorFxn = NULL
}
};

§ UARTMSP432E4_Object

UARTMSP432E4 Object.

The application must not access any member variables of this structure!

§ UARTMSP432E4_Handle

Variable Documentation

§ UARTMSP432E4_fxnTable

const UART_FxnTable UARTMSP432E4_fxnTable
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale