USBLib API Guide  1.00.00.01
Data Structures | Macros | Typedefs | Functions | Variables
Audio_device_class_api

Data Structures

struct  tAudioInstance
 
struct  tUSBDAudioDevice
 

Macros

#define AUDIO_IN_TERMINAL_ID   1
 
#define AUDIO_OUT_TERMINAL_ID   2
 
#define AUDIO_CONTROL_ID   3
 
#define AUDIO_INTERFACE_CONTROL   0
 
#define AUDIO_INTERFACE_OUTPUT   1
 
#define ISOC_OUT_ENDPOINT   USB_EP_1
 
#define ISOC_OUT_EP_MAX_SIZE   ((48000*4)/1000)
 
#define NUM_AUDIO_SECTIONS
 
#define AUDIODESCRIPTOR_SIZE   (8)
 
#define CONTROLINTERFACE_SIZE   (52)
 
#define STREAMINTERFACE_SIZE   (52)
 
#define COMPOSITE_DAUDIO_SIZE
 
#define USBD_AUDIO_EVENT_IDLE   (USBD_AUDIO_EVENT_BASE + 0)
 This USB audio event indicates that the device is connected but not active. More...
 
#define USBD_AUDIO_EVENT_ACTIVE   (USBD_AUDIO_EVENT_BASE + 1)
 
#define USBD_AUDIO_EVENT_DATAOUT   (USBD_AUDIO_EVENT_BASE + 2)
 
#define USBD_AUDIO_EVENT_VOLUME   (USBD_AUDIO_EVENT_BASE + 4)
 
#define USBD_AUDIO_EVENT_MUTE   (USBD_AUDIO_EVENT_BASE + 5)
 

Typedefs

typedef void(* tUSBAudioBufferCallback) (void *pvBuffer, uint32_t ui32Param, uint32_t ui32Event)
 

Functions

void * USBDAudioInit (uint32_t ui32Index, tUSBDAudioDevice *psAudioDevice)
 
void * USBDAudioCompositeInit (uint32_t ui32Index, tUSBDAudioDevice *psAudioDevice, tCompositeEntry *psCompEntry)
 
void USBDAudioTerm (void *pvAudioDevice)
 
int32_t USBAudioBufferOut (void *pvAudioDevice, void *pvBuffer, uint32_t ui32Size, tUSBAudioBufferCallback pfnCallback)
 

Variables

uint8_t g_pui8IADAudioDescriptor [AUDIODESCRIPTOR_SIZE]
 
const tConfigSection g_sIADAudioConfigSection
 
const uint8_t g_pui8AudioControlInterface [CONTROLINTERFACE_SIZE]
 
const uint8_t g_pui8AudioStreamInterface [STREAMINTERFACE_SIZE]
 
const tConfigSection g_sAudioConfigSection
 
const tConfigSection g_sAudioStreamInterfaceSection
 
const tConfigSection g_sAudioControlInterfaceSection
 
const tConfigSectiong_psAudioSections []
 
const tConfigHeader g_sAudioConfigHeader
 
const tConfigHeader *const g_ppAudioConfigDescriptors []
 

Detailed Description

Macro Definition Documentation

§ AUDIO_IN_TERMINAL_ID

#define AUDIO_IN_TERMINAL_ID   1

§ AUDIO_OUT_TERMINAL_ID

#define AUDIO_OUT_TERMINAL_ID   2

§ AUDIO_CONTROL_ID

#define AUDIO_CONTROL_ID   3

§ AUDIO_INTERFACE_CONTROL

#define AUDIO_INTERFACE_CONTROL   0

§ AUDIO_INTERFACE_OUTPUT

#define AUDIO_INTERFACE_OUTPUT   1

§ ISOC_OUT_ENDPOINT

#define ISOC_OUT_ENDPOINT   USB_EP_1

§ ISOC_OUT_EP_MAX_SIZE

#define ISOC_OUT_EP_MAX_SIZE   ((48000*4)/1000)

Referenced by USBAudioBufferOut().

§ NUM_AUDIO_SECTIONS

#define NUM_AUDIO_SECTIONS
Value:
(sizeof(g_psAudioSections) / \
sizeof(g_psAudioSections[0]))
const tConfigSection * g_psAudioSections[]
Definition: usbdaudio.c:366

§ AUDIODESCRIPTOR_SIZE

#define AUDIODESCRIPTOR_SIZE   (8)

§ CONTROLINTERFACE_SIZE

#define CONTROLINTERFACE_SIZE   (52)

§ STREAMINTERFACE_SIZE

#define STREAMINTERFACE_SIZE   (52)

§ COMPOSITE_DAUDIO_SIZE

#define COMPOSITE_DAUDIO_SIZE
Value:
CONTROLINTERFACE_SIZE + STREAMINTERFACE_SIZE)
#define AUDIODESCRIPTOR_SIZE
Definition: usbdaudio.h:172
#define STREAMINTERFACE_SIZE
Definition: usbdaudio.h:186

The size of the memory that should be allocated to create a configuration descriptor for a single instance of the USB Audio Device. This does not include the configuration descriptor which is automatically ignored by the composite device class.

§ USBD_AUDIO_EVENT_IDLE

#define USBD_AUDIO_EVENT_IDLE   (USBD_AUDIO_EVENT_BASE + 0)

This USB audio event indicates that the device is connected but not active.

§ USBD_AUDIO_EVENT_ACTIVE

#define USBD_AUDIO_EVENT_ACTIVE   (USBD_AUDIO_EVENT_BASE + 1)

This USB audio event indicates that the device is connected and is now active.

§ USBD_AUDIO_EVENT_DATAOUT

#define USBD_AUDIO_EVENT_DATAOUT   (USBD_AUDIO_EVENT_BASE + 2)

This USB audio event indicates that the device is returning a data buffer provided by the USBAudioBufferOut() function back to the application with valid audio data received from the USB host controller. The pvBuffer parameter holds the pointer to the buffer with the new audio data and the ui32Param value holds the amount of valid data in bytes that are contained in the pvBuffer parameter.

§ USBD_AUDIO_EVENT_VOLUME

#define USBD_AUDIO_EVENT_VOLUME   (USBD_AUDIO_EVENT_BASE + 4)

This USB audio event indicates that a volume change has occurred. The ui32Param value contains a signed 8.8 fixed point value that represents the current volume gain/attenuation in decibels(dB). The provided message handler should be prepared to handle negative and positive values with the value 0x8000 indicating maximum attenuation. The pvBuffer parameter should be ignored.

§ USBD_AUDIO_EVENT_MUTE

#define USBD_AUDIO_EVENT_MUTE   (USBD_AUDIO_EVENT_BASE + 5)

This USB audio event indicates that a mute request has occurred. The ui32Param value will either be a 1 to indicate that the audio is now muted, and a value of 0 indicates that the audio has been unmuted.

Typedef Documentation

§ tUSBAudioBufferCallback

typedef void(* tUSBAudioBufferCallback) (void *pvBuffer, uint32_t ui32Param, uint32_t ui32Event)

Function Documentation

§ USBDAudioInit()

void * USBDAudioInit ( uint32_t  ui32Index,
tUSBDAudioDevice psAudioDevice 
)

This function should be called once for the audio class device to initialized basic operation and prepare for enumeration.

Parameters
ui32Indexis the index of the USB controller to initialize for audio class device operation.
psAudioDevicepoints to a structure containing parameters customizing the operation of the audio device.

In order for an application to initialize the USB audio device class, it must first call this function with the a valid audio device class structure in the psAudioDevice parameter. This allows this function to initialize the USB controller and device code to be prepared to enumerate and function as a USB audio device.

This function returns a void pointer that must be passed in to all other APIs used by the audio class.

See the documentation on the tUSBDAudioDevice structure for more information on how to properly fill the structure members.

Returns
Returns 0 on failure or a non-zero void pointer on success.

References tUSBDAudioDevice::ppui8StringDescriptors, and USBDAudioCompositeInit().

§ USBDAudioCompositeInit()

void * USBDAudioCompositeInit ( uint32_t  ui32Index,
tUSBDAudioDevice psAudioDevice,
tCompositeEntry psCompEntry 
)

This function should be called once for the audio class device to initialized basic operation and prepare for enumeration.

Parameters
ui32Indexis the index of the USB controller to initialize for audio class device operation.
psAudioDevicepoints to a structure containing parameters customizing the operation of the audio device.
psCompEntryis the composite device entry to initialize when creating a composite device.

In order for an application to initialize the USB audio device class, it must first call this function with the a valid audio device class structure in the psAudioDevice parameter. This allows this function to initialize the USB controller and device code to be prepared to enumerate and function as a USB audio device. When this audio device is part of a composite device, then the psCompEntry should point to the composite device entry to initialize. This is part of the array that is passed to the USBDCompositeInit() function.

This function returns a void pointer that must be passed in to all other APIs used by the audio class.

See the documentation on the tUSBDAudioDevice structure for more information on how to properly fill the structure members.

Returns
Returns zero on failure or a non-zero instance value that should be used with the remaining USB audio APIs.

References tUSBDAudioDevice::ppui8StringDescriptors, tDeviceInfo::psCallbacks, tCompositeEntry::psDevInfo, tCompositeEntry::pvInstance, tAudioInstance::sDevInfo, tUSBDAudioDevice::sPrivateData, and tAudioInstance::ui32USBBase.

Referenced by USBDAudioInit().

§ USBDAudioTerm()

void USBDAudioTerm ( void *  pvAudioDevice)

Shuts down the audio device.

Parameters
pvAudioDeviceis the pointer to the device instance structure as returned by USBDAudioInit().

This function terminates audio interface for the instance supplied. This function should not be called if the audio device is part of a composite device and instead the USBDCompositeTerm() function should be called for the full composite device. Following this call, the pvAudioDevice instance should not me used in any other calls.

Returns
None.

References USBDCDTerm().

§ USBAudioBufferOut()

int32_t USBAudioBufferOut ( void *  pvAudioDevice,
void *  pvBuffer,
uint32_t  ui32Size,
tUSBAudioBufferCallback  pfnCallback 
)

This function is used to supply buffers to the audio class to be filled from the USB host device.

Parameters
pvAudioDeviceis the pointer to the device instance structure as returned by USBDAudioInit() or USBDAudioCompositeInit().
pvBufferis a pointer to the buffer to fill with audio data.
ui32Sizeis the size in bytes of the buffer pointed to by the pvBuffer parameter.
pfnCallbackis a callback that will provide notification when this buffer has valid data.

This function fills the buffer pointed to by the pvBuffer parameter with at most ui32Size one packet of data from the host controller. The ui32Size has a minimum value of ISOC_OUT_EP_MAX_SIZE since each USB packet can be at most ISOC_OUT_EP_MAX_SIZE bytes in size. Since the audio data may not be received in amounts that evenly fit in the buffer provided, the buffer may not be completely filled. The pfnCallback function will provide the amount of valid data that was actually stored in the buffer provided. The function will return zero if the buffer could be scheduled to be filled, otherwise the function will return a non-zero value if there was some reason that the buffer could not be added.

Returns
Returns 0 to indicate success any other value indicates that the buffer will not be filled.

References ISOC_OUT_EP_MAX_SIZE, tAudioInstance::pfnCallback, tAudioInstance::pvData, tAudioInstance::sBuffer, tUSBDAudioDevice::sPrivateData, tAudioInstance::ui32NumBytes, and tAudioInstance::ui32Size.

Variable Documentation

§ g_pui8IADAudioDescriptor

uint8_t g_pui8IADAudioDescriptor[AUDIODESCRIPTOR_SIZE]
Initial value:
=
{
8,
0x0,
0x2,
0
}
#define USB_CLASS_AUDIO
Definition: usblib.h:420
#define USB_SUBCLASS_UNDEFINED
Definition: usblib.h:445
#define USB_PROTOCOL_UNDEFINED
Definition: usblib.h:446
#define USB_DTYPE_INTERFACE_ASC
Definition: usblib.h:289

§ g_sIADAudioConfigSection

const tConfigSection g_sIADAudioConfigSection
Initial value:
=
{
}
uint8_t g_pui8IADAudioDescriptor[AUDIODESCRIPTOR_SIZE]
Definition: usbdaudio.c:133

§ g_pui8AudioControlInterface

const uint8_t g_pui8AudioControlInterface[CONTROLINTERFACE_SIZE]

§ g_pui8AudioStreamInterface

const uint8_t g_pui8AudioStreamInterface[STREAMINTERFACE_SIZE]

§ g_sAudioConfigSection

const tConfigSection g_sAudioConfigSection
Initial value:
=
{
sizeof(g_pui8AudioDescriptor),
g_pui8AudioDescriptor
}

§ g_sAudioStreamInterfaceSection

const tConfigSection g_sAudioStreamInterfaceSection
Initial value:
=
{
}
const uint8_t g_pui8AudioStreamInterface[STREAMINTERFACE_SIZE]
Definition: usbdaudio.c:252

§ g_sAudioControlInterfaceSection

const tConfigSection g_sAudioControlInterfaceSection
Initial value:
=
{
}
const uint8_t g_pui8AudioControlInterface[CONTROLINTERFACE_SIZE]
Definition: usbdaudio.c:158

§ g_psAudioSections

const tConfigSection* g_psAudioSections[]
Initial value:
=
{
}
const tConfigSection g_sIADAudioConfigSection
Definition: usbdaudio.c:146
const tConfigSection g_sAudioControlInterfaceSection
Definition: usbdaudio.c:354
const tConfigSection g_sAudioConfigSection
Definition: usbdaudio.c:342
const tConfigSection g_sAudioStreamInterfaceSection
Definition: usbdaudio.c:348

§ g_sAudioConfigHeader

const tConfigHeader g_sAudioConfigHeader
Initial value:
=
{
}
const tConfigSection * g_psAudioSections[]
Definition: usbdaudio.c:366
#define NUM_AUDIO_SECTIONS
Definition: usbdaudio.c:374

§ g_ppAudioConfigDescriptors

const tConfigHeader* const g_ppAudioConfigDescriptors[]
Initial value:
=
{
}
const tConfigHeader g_sAudioConfigHeader
Definition: usbdaudio.c:384
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale