Data Fields
NVS_Config_ Struct Reference

NVS Global configuration. More...

#include <NVS.h>

Data Fields

NVS_FxnTable const * fxnTablePtr
 
void * object
 
void const * hwAttrs
 

Detailed Description

NVS Global configuration.

The NVS_Config structure contains a set of pointers used to characterize the NVS driver implementation.

This structure needs to be defined before calling NVS_init() and it must not be changed thereafter.

See also
NVS_init()

Field Documentation

§ fxnTablePtr

NVS_FxnTable const* NVS_Config_::fxnTablePtr

Pointer to a table of driver-specific implementations of NVS APIs

§ object

void* NVS_Config_::object

Pointer to a driver specific data object

§ hwAttrs

void const* NVS_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated