Network Services API  2.00.00.16
Data Fields
_SlNetSock_linger_t Struct Reference

The SlNetSock_linger_t structure is used in SLNETSOCK_OPSOCK_LINGER socket level option. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_linger_t:
Collaboration graph

Data Fields

uint32_t l_onoff
 
uint32_t l_linger
 

Detailed Description

The SlNetSock_linger_t structure is used in SLNETSOCK_OPSOCK_LINGER socket level option.

Field Documentation

§ l_onoff

uint32_t _SlNetSock_linger_t::l_onoff

§ l_linger

uint32_t _SlNetSock_linger_t::l_linger

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated