Network Services API  2.00.00.16
Data Fields
_SlNetSock_SdSet_t Struct Reference

The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_SdSet_t:
Collaboration graph

Data Fields

uint32_t sdSetBitmap [((32)+(uint8_t) 31)/(uint8_t) 32]
 

Detailed Description

The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function.

Field Documentation

§ sdSetBitmap

uint32_t _SlNetSock_SdSet_t::sdSetBitmap[((32)+(uint8_t) 31)/(uint8_t) 32]

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated