Network Services API  2.00.00.16
Data Fields
_SlNetSock_Nonblocking_t Struct Reference

The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_Nonblocking_t:
Collaboration graph

Data Fields

uint32_t nonBlockingEnabled
 

Detailed Description

The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option.

Field Documentation

§ nonBlockingEnabled

uint32_t _SlNetSock_Nonblocking_t::nonBlockingEnabled

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated