Network Services API  2.00.00.16
Data Fields
_SlNetSock_NonIpBoundary_t Struct Reference

The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_NonIpBoundary_t:
Collaboration graph

Data Fields

int32_t nonIpBoundaryEnabled
 

Detailed Description

The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option.

Field Documentation

§ nonIpBoundaryEnabled

int32_t _SlNetSock_NonIpBoundary_t::nonIpBoundaryEnabled

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated