Network Services API  2.00.00.16
Data Fields
_SlNetSock_Keepalive_t Struct Reference

The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_Keepalive_t:
Collaboration graph

Data Fields

uint32_t keepaliveEnabled
 

Detailed Description

The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option.

Field Documentation

§ keepaliveEnabled

uint32_t _SlNetSock_Keepalive_t::keepaliveEnabled

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated