Network Services API  2.00.00.16
Data Fields
_SlNetSock_IpV6Mreq_t Struct Reference

The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP/SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_IpV6Mreq_t:
Collaboration graph

Data Fields

SlNetSock_In6Addr_t ipv6mr_multiaddr
 
uint32_t ipv6mr_interface
 

Detailed Description

The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP/SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option.

Field Documentation

§ ipv6mr_multiaddr

SlNetSock_In6Addr_t _SlNetSock_IpV6Mreq_t::ipv6mr_multiaddr

§ ipv6mr_interface

uint32_t _SlNetSock_IpV6Mreq_t::ipv6mr_interface

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated