Network Services API  2.00.00.16
Data Fields
_SlNetSock_IpMreq_t Struct Reference

The SlNetSock_IpMreq_t structure is used in SLNETSOCK_OPIP_ADD_MEMBERSHIP/SLNETSOCK_OPIP_DROP_MEMBERSHIP IP level option. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_IpMreq_t:
Collaboration graph

Data Fields

SlNetSock_InAddr_t imr_multiaddr
 
uint32_t imr_interface
 

Detailed Description

The SlNetSock_IpMreq_t structure is used in SLNETSOCK_OPIP_ADD_MEMBERSHIP/SLNETSOCK_OPIP_DROP_MEMBERSHIP IP level option.

Field Documentation

§ imr_multiaddr

SlNetSock_InAddr_t _SlNetSock_IpMreq_t::imr_multiaddr

§ imr_interface

uint32_t _SlNetSock_IpMreq_t::imr_interface

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated