Network Services API  2.00.00.16
Data Fields
_SlNetSock_AddrIn_t Struct Reference

SlNetSock IPv4 address, Internet style. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_AddrIn_t:
Collaboration graph

Data Fields

uint16_t sin_family
 
uint16_t sin_port
 
SlNetSock_InAddr_t sin_addr
 
int8_t sin_zero [8]
 

Detailed Description

SlNetSock IPv4 address, Internet style.

Field Documentation

§ sin_family

uint16_t _SlNetSock_AddrIn_t::sin_family

§ sin_port

uint16_t _SlNetSock_AddrIn_t::sin_port

§ sin_addr

SlNetSock_InAddr_t _SlNetSock_AddrIn_t::sin_addr

§ sin_zero

int8_t _SlNetSock_AddrIn_t::sin_zero[8]

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated