Network Services API  2.00.00.16
Data Fields
_SlNetSock_AddrIn6_t Struct Reference

SlNetSock IPv6 address, Internet style. More...

#include <slnetsock.h>

Collaboration diagram for _SlNetSock_AddrIn6_t:
Collaboration graph

Data Fields

uint16_t sin6_family
 
uint16_t sin6_port
 
uint32_t sin6_flowinfo
 
SlNetSock_In6Addr_t sin6_addr
 
uint32_t sin6_scope_id
 

Detailed Description

SlNetSock IPv6 address, Internet style.

Field Documentation

§ sin6_family

uint16_t _SlNetSock_AddrIn6_t::sin6_family

§ sin6_port

uint16_t _SlNetSock_AddrIn6_t::sin6_port

§ sin6_flowinfo

uint32_t _SlNetSock_AddrIn6_t::sin6_flowinfo

§ sin6_addr

SlNetSock_In6Addr_t _SlNetSock_AddrIn6_t::sin6_addr

§ sin6_scope_id

uint32_t _SlNetSock_AddrIn6_t::sin6_scope_id

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated