Data Structures | Macros | Typedefs | Functions
PowerMSP432.h File Reference

Detailed Description

Power manager interface for the MSP432.

============================================================================

The Power header file should be included in an application as follows:

Refer to Power.h for a complete description of APIs.


#include <stdint.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/drivers/utils/List.h>
#include <ti/drivers/Power.h>
#include <ti/devices/msp432p4xx/driverlib/pcm.h>
#include <ti/devices/msp432p4xx/driverlib/cs.h>

Go to the source code of this file.

Data Structures

struct  PowerMSP432_PerfLevel
 Structure defining a performance level. More...
 
struct  PowerMSP432_Freqs
 Structure holding device frequencies (in Hz) More...
 
struct  PowerMSP432_ConfigV1
 Power global configuration (MSP432-specific) More...
 

Macros

#define PowerMSP432_RESUMETIMESLEEP   32
 
#define PowerMSP432_TOTALTIMESLEEP   40
 
#define PowerMSP432_RESUMETIMEDEEPSLEEP_0   16
 
#define PowerMSP432_TOTALTIMEDEEPSLEEP_0   40
 
#define PowerMSP432_RESUMETIMEDEEPSLEEP_1   16
 
#define PowerMSP432_TOTALTIMEDEEPSLEEP_1   40
 
#define PowerMSP432_PERIPH_ADC14   0
 
#define PowerMSP432_PERIPH_DMA   1
 
#define PowerMSP432_PERIPH_EUSCI_A0   2
 
#define PowerMSP432_PERIPH_EUSCI_A1   3
 
#define PowerMSP432_PERIPH_EUSCI_A2   4
 
#define PowerMSP432_PERIPH_EUSCI_A3   5
 
#define PowerMSP432_PERIPH_EUSCI_B0   6
 
#define PowerMSP432_PERIPH_EUSCI_B1   7
 
#define PowerMSP432_PERIPH_EUSCI_B2   8
 
#define PowerMSP432_PERIPH_EUSCI_B3   9
 
#define PowerMSP432_PERIPH_TIMER_A0   10
 
#define PowerMSP432_PERIPH_TIMER_A1   11
 
#define PowerMSP432_PERIPH_TIMER_A2   12
 
#define PowerMSP432_PERIPH_TIMER_A3   13
 
#define PowerMSP432_PERIPH_TIMER_T32   14
 
#define PowerMSP432_DISALLOW_SLEEP   0
 
#define PowerMSP432_DISALLOW_DEEPSLEEP_0   1
 
#define PowerMSP432_DISALLOW_DEEPSLEEP_1   2
 
#define PowerMSP432_DISALLOW_SHUTDOWN_0   3
 
#define PowerMSP432_DISALLOW_SHUTDOWN_1   4
 
#define PowerMSP432_DISALLOW_PERFLEVEL_0   5
 
#define PowerMSP432_DISALLOW_PERFLEVEL_1   6
 
#define PowerMSP432_DISALLOW_PERFLEVEL_2   7
 
#define PowerMSP432_DISALLOW_PERFLEVEL_3   8
 
#define PowerMSP432_DISALLOW_PERFLEVEL_4   9
 
#define PowerMSP432_DISALLOW_PERFLEVEL_5   10
 
#define PowerMSP432_DISALLOW_PERFLEVEL_6   11
 
#define PowerMSP432_DISALLOW_PERFLEVEL_7   12
 
#define PowerMSP432_DISALLOW_PERF_CHANGES   13
 
#define PowerMSP432_ENTERING_SLEEP   0x1
 
#define PowerMSP432_ENTERING_DEEPSLEEP   0x2
 
#define PowerMSP432_ENTERING_SHUTDOWN   0x4
 
#define PowerMSP432_AWAKE_SLEEP   0x8
 
#define PowerMSP432_AWAKE_DEEPSLEEP   0x10
 
#define PowerMSP432_START_CHANGE_PERF_LEVEL   0x20
 
#define PowerMSP432_DONE_CHANGE_PERF_LEVEL   0x40
 
#define PowerMSP432_SLEEP   0x1
 
#define PowerMSP432_DEEPSLEEP_0   0x2
 
#define PowerMSP432_DEEPSLEEP_1   0x4
 
#define PowerMSP432_SHUTDOWN_0   0x0
 
#define PowerMSP432_SHUTDOWN_1   0x1
 

Typedefs

typedef struct PowerMSP432_PerfLevel PowerMSP432_PerfLevel
 Structure defining a performance level. More...
 
typedef struct PowerMSP432_Freqs PowerMSP432_Freqs
 Structure holding device frequencies (in Hz) More...
 
typedef struct PowerMSP432_ConfigV1 PowerMSP432_ConfigV1
 Power global configuration (MSP432-specific) More...
 

Functions

void PowerMSP432_initPolicy (void)
 The Power Policy initialization function. More...
 
void PowerMSP432_sleepPolicy (void)
 The SLEEP Power Policy. More...
 
void PowerMSP432_deepSleepPolicy (void)
 The DEEPSLEEP Power Policy. More...
 

Macro Definition Documentation

§ PowerMSP432_RESUMETIMESLEEP

#define PowerMSP432_RESUMETIMESLEEP   32

The latency to reserve for resume from SLEEP (usec)

§ PowerMSP432_TOTALTIMESLEEP

#define PowerMSP432_TOTALTIMESLEEP   40

The total latency to reserve for entry and exit of SLEEP (usec)

§ PowerMSP432_RESUMETIMEDEEPSLEEP_0

#define PowerMSP432_RESUMETIMEDEEPSLEEP_0   16

The latency to reserve for resume from DEEPSLEEP_0 (usec)

§ PowerMSP432_TOTALTIMEDEEPSLEEP_0

#define PowerMSP432_TOTALTIMEDEEPSLEEP_0   40

The total latency to reserve for entry and exit of DEEPSLEEP_0 (usec)

§ PowerMSP432_RESUMETIMEDEEPSLEEP_1

#define PowerMSP432_RESUMETIMEDEEPSLEEP_1   16

The latency to reserve for resume from DEEPSLEEP_1 (usec)

§ PowerMSP432_TOTALTIMEDEEPSLEEP_1

#define PowerMSP432_TOTALTIMEDEEPSLEEP_1   40

The total latency to reserve for entry and exit of DEEPSLEEP_1 (usec)

§ PowerMSP432_PERIPH_ADC14

#define PowerMSP432_PERIPH_ADC14   0

Resource ID: ADC14

§ PowerMSP432_PERIPH_DMA

#define PowerMSP432_PERIPH_DMA   1

Resource ID: DMA

§ PowerMSP432_PERIPH_EUSCI_A0

#define PowerMSP432_PERIPH_EUSCI_A0   2

Resource ID: EUSCI_A0

§ PowerMSP432_PERIPH_EUSCI_A1

#define PowerMSP432_PERIPH_EUSCI_A1   3

Resource ID: EUSCI_A1

§ PowerMSP432_PERIPH_EUSCI_A2

#define PowerMSP432_PERIPH_EUSCI_A2   4

Resource ID: EUSCI_A2

§ PowerMSP432_PERIPH_EUSCI_A3

#define PowerMSP432_PERIPH_EUSCI_A3   5

Resource ID: EUSCI_A3

§ PowerMSP432_PERIPH_EUSCI_B0

#define PowerMSP432_PERIPH_EUSCI_B0   6

Resource ID: EUSCI_B0

§ PowerMSP432_PERIPH_EUSCI_B1

#define PowerMSP432_PERIPH_EUSCI_B1   7

Resource ID: EUSCI_B1

§ PowerMSP432_PERIPH_EUSCI_B2

#define PowerMSP432_PERIPH_EUSCI_B2   8

Resource ID: EUSCI_B2

§ PowerMSP432_PERIPH_EUSCI_B3

#define PowerMSP432_PERIPH_EUSCI_B3   9

Resource ID: EUSCI_B3

§ PowerMSP432_PERIPH_TIMER_A0

#define PowerMSP432_PERIPH_TIMER_A0   10

Resource ID: Timer_A0

§ PowerMSP432_PERIPH_TIMER_A1

#define PowerMSP432_PERIPH_TIMER_A1   11

Resource ID: Timer_A1

§ PowerMSP432_PERIPH_TIMER_A2

#define PowerMSP432_PERIPH_TIMER_A2   12

Resource ID: Timer_A2

§ PowerMSP432_PERIPH_TIMER_A3

#define PowerMSP432_PERIPH_TIMER_A3   13

Resource ID: Timer_A3

§ PowerMSP432_PERIPH_TIMER_T32

#define PowerMSP432_PERIPH_TIMER_T32   14

Resource ID: Timer32

§ PowerMSP432_DISALLOW_SLEEP

#define PowerMSP432_DISALLOW_SLEEP   0

Constraint: Disallow a transition to the SLEEP state

§ PowerMSP432_DISALLOW_DEEPSLEEP_0

#define PowerMSP432_DISALLOW_DEEPSLEEP_0   1

Constraint: Disallow a transition to the DEEPSLEEP_0 state

§ PowerMSP432_DISALLOW_DEEPSLEEP_1

#define PowerMSP432_DISALLOW_DEEPSLEEP_1   2

Constraint: Disallow a transition to the DEEPSLEEP_1 state

§ PowerMSP432_DISALLOW_SHUTDOWN_0

#define PowerMSP432_DISALLOW_SHUTDOWN_0   3

Constraint: Disallow a transition to the SHUTDOWN_0 state

§ PowerMSP432_DISALLOW_SHUTDOWN_1

#define PowerMSP432_DISALLOW_SHUTDOWN_1   4

Constraint: Disallow a transition to the SHUTDOWN_1 state

§ PowerMSP432_DISALLOW_PERFLEVEL_0

#define PowerMSP432_DISALLOW_PERFLEVEL_0   5

Constraint: Disallow a transition to PERFLEVEL_0

§ PowerMSP432_DISALLOW_PERFLEVEL_1

#define PowerMSP432_DISALLOW_PERFLEVEL_1   6

Constraint: Disallow a transition to PERFLEVEL_1

§ PowerMSP432_DISALLOW_PERFLEVEL_2

#define PowerMSP432_DISALLOW_PERFLEVEL_2   7

Constraint: Disallow a transition to PERFLEVEL_2

§ PowerMSP432_DISALLOW_PERFLEVEL_3

#define PowerMSP432_DISALLOW_PERFLEVEL_3   8

Constraint: Disallow a transition to PERFLEVEL_3

§ PowerMSP432_DISALLOW_PERFLEVEL_4

#define PowerMSP432_DISALLOW_PERFLEVEL_4   9

Constraint: Disallow a transition to PERFLEVEL_4

§ PowerMSP432_DISALLOW_PERFLEVEL_5

#define PowerMSP432_DISALLOW_PERFLEVEL_5   10

Constraint: Disallow a transition to PERFLEVEL_5

§ PowerMSP432_DISALLOW_PERFLEVEL_6

#define PowerMSP432_DISALLOW_PERFLEVEL_6   11

Constraint: Disallow a transition to PERFLEVEL_6

§ PowerMSP432_DISALLOW_PERFLEVEL_7

#define PowerMSP432_DISALLOW_PERFLEVEL_7   12

Constraint: Disallow a transition to PERFLEVEL_7

§ PowerMSP432_DISALLOW_PERF_CHANGES

#define PowerMSP432_DISALLOW_PERF_CHANGES   13

Constraint: Disallow any performance level changes

§ PowerMSP432_ENTERING_SLEEP

#define PowerMSP432_ENTERING_SLEEP   0x1

Power event: The device is entering the SLEEP state

§ PowerMSP432_ENTERING_DEEPSLEEP

#define PowerMSP432_ENTERING_DEEPSLEEP   0x2

Power event: The device is entering a DEEPSLEEP state

§ PowerMSP432_ENTERING_SHUTDOWN

#define PowerMSP432_ENTERING_SHUTDOWN   0x4

Power event: The device is entering a SHUTDOWN state

§ PowerMSP432_AWAKE_SLEEP

#define PowerMSP432_AWAKE_SLEEP   0x8

Power event: The device is waking from the SLEEP state

§ PowerMSP432_AWAKE_DEEPSLEEP

#define PowerMSP432_AWAKE_DEEPSLEEP   0x10

Power event: The device is waking from a DEEPSLEEP state

§ PowerMSP432_START_CHANGE_PERF_LEVEL

#define PowerMSP432_START_CHANGE_PERF_LEVEL   0x20

Power event: A performance level change has been initiated

§ PowerMSP432_DONE_CHANGE_PERF_LEVEL

#define PowerMSP432_DONE_CHANGE_PERF_LEVEL   0x40

Power event: A performance level change has completed

§ PowerMSP432_SLEEP

#define PowerMSP432_SLEEP   0x1

Device state of LPM0

§ PowerMSP432_DEEPSLEEP_0

#define PowerMSP432_DEEPSLEEP_0   0x2

Device state of LPM3

§ PowerMSP432_DEEPSLEEP_1

#define PowerMSP432_DEEPSLEEP_1   0x4

Device state of LPM4

§ PowerMSP432_SHUTDOWN_0

#define PowerMSP432_SHUTDOWN_0   0x0

Device state of LPM3.5

§ PowerMSP432_SHUTDOWN_1

#define PowerMSP432_SHUTDOWN_1   0x1

Device state of LPM4.5

Typedef Documentation

§ PowerMSP432_PerfLevel

Structure defining a performance level.

The MCU performance level can be set with Power_setPerformanceLevel(). A performance level is defined by this PowerMSP432_PerfLevel structure.

The Power driver currently supports four pre-defined performance levels:

Level MCLK (MHz) HSMCLK (MHz) SMCLK (MHz) ACLK (Hz)
----- ---------- ------------ ----------- ---------
0 12 3 3 32768
1 24 6 6 32768
2 48 24 12 32768
3 48 48 24 32768

Up to four optional 'custom' performance levels can be defined by the user. Performance levels are designated by an index, starting with zero. Any custom performance levels will be indexed following the last pre-defined level. For example, if there are 4 pre-defined levels, they will have indices from '0' to '3'. If there are custom levels defined, they will be indexed starting with '4'.

Eight performance level constraints are supported, one for each of the four pre-defined levels:

plus four for the optional custom performance levels:

The parameters that are used to define a performance level are shown below.

Warning
There is very limited runtime error checking of the different parameters, and no checking that the ratios and parameter combinations do not result in an invalid device configuration (which could overclock or damage the device). It is therefore critical that the user ensures the values specified for a custom performance level are correct.

To define custom performance levels the user must add an array of PowerMSP432_PerfLevel structures to their board file, and then reference this array in the PowerMSP432_config structure. An example is shown below.

First, if not already included in the board file, add the includes of cs.h and pcm.h

#include <ti/devices/msp432p4xx/driverlib/cs.h>
#include <ti/devices/msp432p4xx/driverlib/pcm.h>

Next, add an array with two new performance levels:

PowerMSP432_PerfLevel myPerfLevels[] = {
{ .activeState = PCM_AM_DCDC_VCORE0,
.VCORE = 0,
.DCORESEL = CS_DCO_FREQUENCY_12,
.SELM = CS_HFXTCLK_SELECT,
.DIVM = CS_CLOCK_DIVIDER_4,
.SELS = CS_HFXTCLK_SELECT,
.DIVHS = CS_CLOCK_DIVIDER_16,
.DIVS = CS_CLOCK_DIVIDER_16,
.SELB = CS_LFXTCLK_SELECT,
.SELA = CS_LFXTCLK_SELECT,
.DIVA = CS_CLOCK_DIVIDER_1,
.flashWaitStates = 0,
.enableFlashBuffer = false,
.MCLK = 12000000,
.HSMCLK = 3000000,
.SMCLK = 3000000,
.BCLK = 32768,
.ACLK = 32768
},
{ .activeState = PCM_AM_DCDC_VCORE0,
.VCORE = 0,
.DCORESEL = CS_DCO_FREQUENCY_24,
.SELM = CS_DCOCLK_SELECT,
.DIVM = CS_CLOCK_DIVIDER_1,
.SELS = CS_DCOCLK_SELECT,
.DIVHS = CS_CLOCK_DIVIDER_4,
.DIVS = CS_CLOCK_DIVIDER_4,
.SELB = CS_REFOCLK_SELECT,
.SELA = CS_REFOCLK_SELECT,
.DIVA = CS_CLOCK_DIVIDER_1,
.flashWaitStates = 1,
.enableFlashBuffer = true,
.MCLK = 24000000,
.HSMCLK = 6000000,
.SMCLK = 6000000,
.BCLK = 32768,
.ACLK = 32768
},
};

Then, update the PowerMSP432_config structure to 1) reference the new custom levels, and 2) as appropriate, enable extended performance scaling support, and define the relevant extended configuration parameters. In the first custom perf level shown above the HFXT and LFXT crystals are used as clock sources, so for this example the extended support parameters need to be specfied.

The code below shows additions to the PowerMSP432_config structure for this example. The first two additions to PowerMSP432_config reference the array of custom perf levels, and indicate the number of custom levels. The third addition enables extended support for crystals. The remaining parameters define crystal settings, plus an application-provided ISR function for handling any Clock System fault interrupts.

const PowerMSP432_ConfigV1 PowerMSP432_config = {
...
.customPerfLevels = myPerfLevels,
.numCustom = sizeof(myPerfLevels) / sizeof(PowerMSP432_PerfLevel),
.useExtendedPerf = true,
.HFXTFREQ = CS_48MHZ,
.configurePinHFXT = true,
.bypassHFXT = false,
.configurePinLFXT = true,
.bypassLFXT = false,
.LFXTDRIVE = CS_LFXT_DRIVE3,
.enableInterruptsCS = true,
.priorityInterruptsCS = ~0,
.isrCS = &isrCS
};

§ PowerMSP432_Freqs

Structure holding device frequencies (in Hz)

§ PowerMSP432_ConfigV1

Power global configuration (MSP432-specific)

Function Documentation

§ PowerMSP432_initPolicy()

void PowerMSP432_initPolicy ( void  )

The Power Policy initialization function.

This is an optional policy initialization function that will be called during application startup, during Power Manager initialization.

§ PowerMSP432_sleepPolicy()

void PowerMSP432_sleepPolicy ( void  )

The SLEEP Power Policy.

This is a simple Power Policy that will transition the device to the PowerMSP432_SLEEP state, unless there is a constraint prohibiting this. If PowerMSP432_SLEEP cannot be activated, CPU Wait For Interrupt (WFI) will be chosen instead.

In order for this policy to run, 1) it must be selected as the Power Policy (either by being specified as the 'policyFxn' in the PowerMSP432_config structure, or specified at runtime with Power_setPolicy()), and 2) the Power Policy must be enabled (either via 'enablePolicy' in the PowerMSP432_config structure, or via a call to Power_enablePolicy() at runtime).

§ PowerMSP432_deepSleepPolicy()

void PowerMSP432_deepSleepPolicy ( void  )

The DEEPSLEEP Power Policy.

This is an agressive Power Policy which checks active constraints and automatically transitions the device into the deepest sleep state possible.

The first goal is to enter PowerMSP432_DEEPSLEEP_1; if that is not allowed, the secondary goal is PowerMSP432_DEEPSLEEP_0; if that is not allowed, the next goal is PowerMSP432_SLEEP; and finally, if that is not allowed, CPU Wait For Interrupt (WFI) will be chosen.

In order for this policy to run, 1) it must be selected as the Power Policy (either by being specified as the 'policyFxn' in the PowerMSP432_config structure, or specified at runtime with Power_setPolicy()), and 2) the Power Policy must be enabled (either via 'enablePolicy' in the PowerMSP432_config structure, or via a call to Power_enablePolicy() at runtime).

Copyright 2017, Texas Instruments Incorporated