I2C driver implementation for the EUSCI controller on MSP432.
============================================================================
This I2C driver implementation is designed to operate on a EUCSI controller in I2C mode. The I2CMSP432 header file should be included in an application as follows:
Refer to I2C.h for a complete description of APIs & example of use.
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/I2C.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/Power.h>
Go to the source code of this file.
Data Structures | |
struct | I2CMSP432_HWAttrsV1 |
I2CMSP432 Hardware attributes. More... | |
Macros | |
#define | I2CMSP432_P1_6_UCB0SDA 0x00000116 |
#define | I2CMSP432_P1_7_UCB0SCL 0x00000117 |
#define | I2CMSP432_P2_0_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x20) |
#define | I2CMSP432_P2_0_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x20) |
#define | I2CMSP432_P2_0_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x20) |
#define | I2CMSP432_P2_0_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x20) |
#define | I2CMSP432_P2_1_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x21) |
#define | I2CMSP432_P2_1_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x21) |
#define | I2CMSP432_P2_1_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x21) |
#define | I2CMSP432_P2_1_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x21) |
#define | I2CMSP432_P2_2_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x22) |
#define | I2CMSP432_P2_2_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x22) |
#define | I2CMSP432_P2_2_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x22) |
#define | I2CMSP432_P2_2_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x22) |
#define | I2CMSP432_P2_3_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x23) |
#define | I2CMSP432_P2_3_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x23) |
#define | I2CMSP432_P2_3_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x23) |
#define | I2CMSP432_P2_3_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x23) |
#define | I2CMSP432_P2_4_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x24) |
#define | I2CMSP432_P2_4_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x24) |
#define | I2CMSP432_P2_4_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x24) |
#define | I2CMSP432_P2_4_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x24) |
#define | I2CMSP432_P2_5_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x25) |
#define | I2CMSP432_P2_5_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x25) |
#define | I2CMSP432_P2_5_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x25) |
#define | I2CMSP432_P2_5_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x25) |
#define | I2CMSP432_P2_6_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x26) |
#define | I2CMSP432_P2_6_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x26) |
#define | I2CMSP432_P2_6_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x26) |
#define | I2CMSP432_P2_6_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x26) |
#define | I2CMSP432_P2_7_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x27) |
#define | I2CMSP432_P2_7_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x27) |
#define | I2CMSP432_P2_7_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x27) |
#define | I2CMSP432_P2_7_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x27) |
#define | I2CMSP432_P3_0_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x30) |
#define | I2CMSP432_P3_0_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x30) |
#define | I2CMSP432_P3_0_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x30) |
#define | I2CMSP432_P3_0_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x30) |
#define | I2CMSP432_P3_1_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x31) |
#define | I2CMSP432_P3_1_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x31) |
#define | I2CMSP432_P3_1_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x31) |
#define | I2CMSP432_P3_1_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x31) |
#define | I2CMSP432_P3_2_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x32) |
#define | I2CMSP432_P3_2_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x32) |
#define | I2CMSP432_P3_2_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x32) |
#define | I2CMSP432_P3_2_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x32) |
#define | I2CMSP432_P3_3_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x33) |
#define | I2CMSP432_P3_3_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x33) |
#define | I2CMSP432_P3_3_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x33) |
#define | I2CMSP432_P3_3_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x33) |
#define | I2CMSP432_P3_4_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x34) |
#define | I2CMSP432_P3_4_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x34) |
#define | I2CMSP432_P3_4_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x34) |
#define | I2CMSP432_P3_4_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x34) |
#define | I2CMSP432_P3_5_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x35) |
#define | I2CMSP432_P3_5_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x35) |
#define | I2CMSP432_P3_5_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x35) |
#define | I2CMSP432_P3_5_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x35) |
#define | I2CMSP432_P3_6_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x36) |
#define | I2CMSP432_P3_6_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x36) |
#define | I2CMSP432_P3_6_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x36) |
#define | I2CMSP432_P3_6_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x36) |
#define | I2CMSP432_P3_7_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x37) |
#define | I2CMSP432_P3_7_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x37) |
#define | I2CMSP432_P3_7_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x37) |
#define | I2CMSP432_P3_7_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x37) |
#define | I2CMSP432_P6_4_UCB1SDA 0x00000164 |
#define | I2CMSP432_P6_5_UCB1SCL 0x00000165 |
#define | I2CMSP432_P6_6_UCB3SDA 0x00000266 |
#define | I2CMSP432_P6_7_UCB3SCL 0x00000267 |
#define | I2CMSP432_P7_0_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x70) |
#define | I2CMSP432_P7_0_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x70) |
#define | I2CMSP432_P7_0_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x70) |
#define | I2CMSP432_P7_0_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x70) |
#define | I2CMSP432_P7_1_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x71) |
#define | I2CMSP432_P7_1_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x71) |
#define | I2CMSP432_P7_1_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x71) |
#define | I2CMSP432_P7_1_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x71) |
#define | I2CMSP432_P7_2_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x72) |
#define | I2CMSP432_P7_2_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x72) |
#define | I2CMSP432_P7_2_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x72) |
#define | I2CMSP432_P7_2_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x72) |
#define | I2CMSP432_P7_3_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x73) |
#define | I2CMSP432_P7_3_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x73) |
#define | I2CMSP432_P7_3_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x73) |
#define | I2CMSP432_P7_3_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x73) |
#define | I2CMSP432_P7_4_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x74) |
#define | I2CMSP432_P7_4_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x74) |
#define | I2CMSP432_P7_4_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x74) |
#define | I2CMSP432_P7_4_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x74) |
#define | I2CMSP432_P7_5_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x75) |
#define | I2CMSP432_P7_5_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x75) |
#define | I2CMSP432_P7_5_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x75) |
#define | I2CMSP432_P7_5_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x75) |
#define | I2CMSP432_P7_6_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x76) |
#define | I2CMSP432_P7_6_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x76) |
#define | I2CMSP432_P7_6_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x76) |
#define | I2CMSP432_P7_6_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x76) |
#define | I2CMSP432_P7_7_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x77) |
#define | I2CMSP432_P7_7_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x77) |
#define | I2CMSP432_P7_7_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x77) |
#define | I2CMSP432_P7_7_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x77) |
#define | I2CMSP432_P10_2_UCB3SDA 0x000001A2 |
#define | I2CMSP432_P10_3_UCB3SCL 0x000001A3 |
Typedefs | |
typedef struct I2CMSP432_HWAttrsV1 | I2CMSP432_HWAttrsV1 |
I2CMSP432 Hardware attributes. More... | |
Variables | |
const I2C_FxnTable | I2CMSP432_fxnTable |
#define I2CMSP432_P1_6_UCB0SDA 0x00000116 |
Port 1 Pin 6 is EUSCI B0 SDA
#define I2CMSP432_P1_7_UCB0SCL 0x00000117 |
Port 1 Pin 7 is EUSCI B0 SCL
#define I2CMSP432_P2_0_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x20) |
Port 2 Pin 0 is EUSCI B0 SDA
#define I2CMSP432_P2_0_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x20) |
Port 2 Pin 0 is EUSCI B0 SCL
#define I2CMSP432_P2_0_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x20) |
Port 2 Pin 0 is EUSCI B2 SDA
#define I2CMSP432_P2_0_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x20) |
Port 2 Pin 0 is EUSCI B2 SCL
#define I2CMSP432_P2_1_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x21) |
Port 2 Pin 1 is EUSCI B0 SDA
#define I2CMSP432_P2_1_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x21) |
Port 2 Pin 1 is EUSCI B0 SCL
#define I2CMSP432_P2_1_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x21) |
Port 2 Pin 1 is EUSCI B2 SDA
#define I2CMSP432_P2_1_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x21) |
Port 2 Pin 1 is EUSCI B2 SCL
#define I2CMSP432_P2_2_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x22) |
Port 2 Pin 2 is EUSCI B0 SDA
#define I2CMSP432_P2_2_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x22) |
Port 2 Pin 2 is EUSCI B0 SCL
#define I2CMSP432_P2_2_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x22) |
Port 2 Pin 2 is EUSCI B2 SDA
#define I2CMSP432_P2_2_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x22) |
Port 2 Pin 2 is EUSCI B2 SCL
#define I2CMSP432_P2_3_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x23) |
Port 2 Pin 3 is EUSCI B0 SDA
#define I2CMSP432_P2_3_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x23) |
Port 2 Pin 3 is EUSCI B0 SCL
#define I2CMSP432_P2_3_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x23) |
Port 2 Pin 3 is EUSCI B2 SDA
#define I2CMSP432_P2_3_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x23) |
Port 2 Pin 3 is EUSCI B2 SCL
#define I2CMSP432_P2_4_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x24) |
Port 2 Pin 4 is EUSCI B0 SDA
#define I2CMSP432_P2_4_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x24) |
Port 2 Pin 4 is EUSCI B0 SCL
#define I2CMSP432_P2_4_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x24) |
Port 2 Pin 4 is EUSCI B2 SDA
#define I2CMSP432_P2_4_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x24) |
Port 2 Pin 4 is EUSCI B2 SCL
#define I2CMSP432_P2_5_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x25) |
Port 2 Pin 5 is EUSCI B0 SDA
#define I2CMSP432_P2_5_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x25) |
Port 2 Pin 5 is EUSCI B0 SCL
#define I2CMSP432_P2_5_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x25) |
Port 2 Pin 5 is EUSCI B2 SDA
#define I2CMSP432_P2_5_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x25) |
Port 2 Pin 5 is EUSCI B2 SCL
#define I2CMSP432_P2_6_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x26) |
Port 2 Pin 6 is EUSCI B0 SDA
#define I2CMSP432_P2_6_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x26) |
Port 2 Pin 6 is EUSCI B0 SCL
#define I2CMSP432_P2_6_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x26) |
Port 2 Pin 6 is EUSCI B2 SDA
#define I2CMSP432_P2_6_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x26) |
Port 2 Pin 6 is EUSCI B2 SCL
#define I2CMSP432_P2_7_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x27) |
Port 2 Pin 7 is EUSCI B0 SDA
#define I2CMSP432_P2_7_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x27) |
Port 2 Pin 7 is EUSCI B0 SCL
#define I2CMSP432_P2_7_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x27) |
Port 2 Pin 7 is EUSCI B2 SDA
#define I2CMSP432_P2_7_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x27) |
Port 2 Pin 7 is EUSCI B2 SCL
#define I2CMSP432_P3_0_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x30) |
Port 3 Pin 0 is EUSCI B0 SDA
#define I2CMSP432_P3_0_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x30) |
Port 3 Pin 0 is EUSCI B0 SCL
#define I2CMSP432_P3_0_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x30) |
Port 3 Pin 0 is EUSCI B2 SDA
#define I2CMSP432_P3_0_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x30) |
Port 3 Pin 0 is EUSCI B2 SCL
#define I2CMSP432_P3_1_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x31) |
Port 3 Pin 1 is EUSCI B0 SDA
#define I2CMSP432_P3_1_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x31) |
Port 3 Pin 1 is EUSCI B0 SCL
#define I2CMSP432_P3_1_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x31) |
Port 3 Pin 1 is EUSCI B2 SDA
#define I2CMSP432_P3_1_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x31) |
Port 3 Pin 1 is EUSCI B2 SCL
#define I2CMSP432_P3_2_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x32) |
Port 3 Pin 2 is EUSCI B0 SDA
#define I2CMSP432_P3_2_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x32) |
Port 3 Pin 2 is EUSCI B0 SCL
#define I2CMSP432_P3_2_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x32) |
Port 3 Pin 2 is EUSCI B2 SDA
#define I2CMSP432_P3_2_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x32) |
Port 3 Pin 2 is EUSCI B2 SCL
#define I2CMSP432_P3_3_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x33) |
Port 3 Pin 3 is EUSCI B0 SDA
#define I2CMSP432_P3_3_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x33) |
Port 3 Pin 3 is EUSCI B0 SCL
#define I2CMSP432_P3_3_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x33) |
Port 3 Pin 3 is EUSCI B2 SDA
#define I2CMSP432_P3_3_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x33) |
Port 3 Pin 3 is EUSCI B2 SCL
#define I2CMSP432_P3_4_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x34) |
Port 3 Pin 4 is EUSCI B0 SDA
#define I2CMSP432_P3_4_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x34) |
Port 3 Pin 4 is EUSCI B0 SCL
#define I2CMSP432_P3_4_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x34) |
Port 3 Pin 4 is EUSCI B2 SDA
#define I2CMSP432_P3_4_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x34) |
Port 3 Pin 4 is EUSCI B2 SCL
#define I2CMSP432_P3_5_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x35) |
Port 3 Pin 5 is EUSCI B0 SDA
#define I2CMSP432_P3_5_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x35) |
Port 3 Pin 5 is EUSCI B0 SCL
#define I2CMSP432_P3_5_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x35) |
Port 3 Pin 5 is EUSCI B2 SDA
#define I2CMSP432_P3_5_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x35) |
Port 3 Pin 5 is EUSCI B2 SCL
#define I2CMSP432_P3_6_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x36) |
Port 3 Pin 6 is EUSCI B0 SDA
#define I2CMSP432_P3_6_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x36) |
Port 3 Pin 6 is EUSCI B0 SCL
#define I2CMSP432_P3_6_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x36) |
Port 3 Pin 6 is EUSCI B2 SDA
#define I2CMSP432_P3_6_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x36) |
Port 3 Pin 6 is EUSCI B2 SCL
#define I2CMSP432_P3_7_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x37) |
Port 3 Pin 7 is EUSCI B0 SDA
#define I2CMSP432_P3_7_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x37) |
Port 3 Pin 7 is EUSCI B0 SCL
#define I2CMSP432_P3_7_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x37) |
Port 3 Pin 7 is EUSCI B2 SDA
#define I2CMSP432_P3_7_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x37) |
Port 3 Pin 7 is EUSCI B2 SCL
#define I2CMSP432_P6_4_UCB1SDA 0x00000164 |
Port 6 Pin 4 is EUSCI B1 SDA
#define I2CMSP432_P6_5_UCB1SCL 0x00000165 |
Port 6 Pin 5 is EUSCI B1 SCL
#define I2CMSP432_P6_6_UCB3SDA 0x00000266 |
Port 6 Pin 6 is EUSCI B3 SDA
#define I2CMSP432_P6_7_UCB3SCL 0x00000267 |
Port 6 Pin 7 is EUSCI B3 SCL
#define I2CMSP432_P7_0_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x70) |
Port 7 Pin 0 is EUSCI B0 SDA
#define I2CMSP432_P7_0_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x70) |
Port 7 Pin 0 is EUSCI B0 SCL
#define I2CMSP432_P7_0_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x70) |
Port 7 Pin 0 is EUSCI B2 SDA
#define I2CMSP432_P7_0_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x70) |
Port 7 Pin 0 is EUSCI B2 SCL
#define I2CMSP432_P7_1_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x71) |
Port 7 Pin 1 is EUSCI B0 SDA
#define I2CMSP432_P7_1_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x71) |
Port 7 Pin 1 is EUSCI B0 SCL
#define I2CMSP432_P7_1_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x71) |
Port 7 Pin 1 is EUSCI B2 SDA
#define I2CMSP432_P7_1_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x71) |
Port 7 Pin 1 is EUSCI B2 SCL
#define I2CMSP432_P7_2_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x72) |
Port 7 Pin 2 is EUSCI B0 SDA
#define I2CMSP432_P7_2_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x72) |
Port 7 Pin 2 is EUSCI B0 SCL
#define I2CMSP432_P7_2_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x72) |
Port 7 Pin 2 is EUSCI B2 SDA
#define I2CMSP432_P7_2_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x72) |
Port 7 Pin 2 is EUSCI B2 SCL
#define I2CMSP432_P7_3_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x73) |
Port 7 Pin 3 is EUSCI B0 SDA
#define I2CMSP432_P7_3_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x73) |
Port 7 Pin 3 is EUSCI B0 SCL
#define I2CMSP432_P7_3_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x73) |
Port 7 Pin 3 is EUSCI B2 SDA
#define I2CMSP432_P7_3_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x73) |
Port 7 Pin 3 is EUSCI B2 SCL
#define I2CMSP432_P7_4_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x74) |
Port 7 Pin 4 is EUSCI B0 SDA
#define I2CMSP432_P7_4_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x74) |
Port 7 Pin 4 is EUSCI B0 SCL
#define I2CMSP432_P7_4_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x74) |
Port 7 Pin 4 is EUSCI B2 SDA
#define I2CMSP432_P7_4_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x74) |
Port 7 Pin 4 is EUSCI B2 SCL
#define I2CMSP432_P7_5_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x75) |
Port 7 Pin 5 is EUSCI B0 SDA
#define I2CMSP432_P7_5_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x75) |
Port 7 Pin 5 is EUSCI B0 SCL
#define I2CMSP432_P7_5_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x75) |
Port 7 Pin 5 is EUSCI B2 SDA
#define I2CMSP432_P7_5_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x75) |
Port 7 Pin 5 is EUSCI B2 SCL
#define I2CMSP432_P7_6_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x76) |
Port 7 Pin 6 is EUSCI B0 SDA
#define I2CMSP432_P7_6_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x76) |
Port 7 Pin 6 is EUSCI B0 SCL
#define I2CMSP432_P7_6_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x76) |
Port 7 Pin 6 is EUSCI B2 SDA
#define I2CMSP432_P7_6_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x76) |
Port 7 Pin 6 is EUSCI B2 SCL
#define I2CMSP432_P7_7_UCB0SDA ((PMAP_UCB0SDA << 10) | 0x77) |
Port 7 Pin 7 is EUSCI B0 SDA
#define I2CMSP432_P7_7_UCB0SCL ((PMAP_UCB0SCL << 10) | 0x77) |
Port 7 Pin 7 is EUSCI B0 SCL
#define I2CMSP432_P7_7_UCB2SDA ((PMAP_UCB2SDA << 10) | 0x77) |
Port 7 Pin 7 is EUSCI B2 SDA
#define I2CMSP432_P7_7_UCB2SCL ((PMAP_UCB2SCL << 10) | 0x77) |
Port 7 Pin 7 is EUSCI B2 SCL
#define I2CMSP432_P10_2_UCB3SDA 0x000001A2 |
Port 10 Pin 2 is EUSCI B3 SDA
#define I2CMSP432_P10_3_UCB3SCL 0x000001A3 |
Port 10 Pin 3 is EUSCI B3 SCL
typedef struct I2CMSP432_HWAttrsV1 I2CMSP432_HWAttrsV1 |
I2CMSP432 Hardware attributes.
The baseAddr and intNum fields define the base address and interrupt number of the EUSCI peripheral. And the clockSource field selects the clock to be used by the EUSCI. These values are passed directly to driverlib APIs, and therefore must be populated by driverlib macro definitions, which are found in:
intPriority is the I2C interrupt priority. This driver uses the ti.dpl interface instead of making OS calls directly, and the corresponding HwiP port handles the interrupt priority in an OS-specific way. For example, in the case of the TI-RTOS kernel port, the intPriority is passed unmodified to Hwi_create() provided by the ti.sysbios.family.arm.m3.Hwi module; so the documentation for the ti.sysbios.family.arm.m3.Hwi module should be referenced for a description of usage of priority.
clkPin and dataPin define the pin mapping to be used for the SCL and SDA pins, respectively. Macro values defined in this header file should be used for these fields.
An example structure is shown below:
const I2C_FxnTable I2CMSP432_fxnTable |