Z-Stack API Reference  3.2.0
_zstackmsg_zdodeviceannouncereq_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
zstack_zdoDeviceAnnounceReq_tpReq
 

Detailed Description

Send this message to the ZStack Thread to send a broadcast ZDO Device Announce.
This command contains the device�s new 16-bit NWK address and its 64-bit IEEE address, as well as the capabilities of the ZigBee device. The command ID for this message is zstackmsg_CmdIDs_ZDO_DEVICE_ANNOUNCE_REQ.

Field Documentation

§ hdr

message header
event field must be set to zstack_CmdIDs

§ pReq

Message command fields


The documentation for this struct was generated from the following file: