Z-Stack API Reference  3.2.0
_zstackmsg_bdbidentifytimeoutind_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
uint8 EndPoint
 

Detailed Description

Message send from the ZStack Thread to let know the application when identify is active or not in the indicated endpoint. The command ID for this message is zstackmsg_CmdIDs_BDB_IDENTIFY_TIME_CB.

Field Documentation

§ EndPoint

uint8 EndPoint

Endpoint in which the time is being updated

§ hdr

message header
event field must be set to zstack_CmdIDs


The documentation for this struct was generated from the following file: