Z-Stack API Reference  3.2.0
_zstackmsg_bdbfilternwkdescriptorind_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
bdbFilterNetworkDesc_t bdbFilterNetworkDesc
 

Detailed Description

Message send from the ZStack Thread to indicate the networks found. The networks are provided as a list of network descriptors. Refer to Zstackapi_bdbFilterNwkDescComplete() and Zstackapi_bdbNwkDescFreeReq(); The command ID for this message is zstackmsg_CmdIDs_BDB_FILTER_NWK_DESCRIPTOR_IND.

Field Documentation

§ bdbFilterNetworkDesc

bdbFilterNetworkDesc_t bdbFilterNetworkDesc

Message command fields NOTE: only the first application registered will receive this notification

§ hdr

message header
event field must be set to zstack_CmdIDs


The documentation for this struct was generated from the following file: