Z-Stack API Reference  3.2.0
_zstack_bdbcbketclinkkeyexchangeattemptreq_t Struct Reference

#include <zstack.h>

Data Fields

bool didSuccess
 

Detailed Description

Structure to send a BDB CBKE TrustCenter Key Exchange Attempt Request.

Field Documentation

§ didSuccess

bool didSuccess

Indicate the stack if the process was success or not. If no Certificate Based Key Exchange (CBKE) procedures was performed, return false so the stack can perform the default Trust Center Link Key exchange procedure


The documentation for this struct was generated from the following file: