Data Fields
I2C_Params_ Struct Reference

I2C Parameters. More...

#include <I2C.h>

Data Fields

I2C_TransferMode transferMode
 
I2C_CallbackFxn transferCallbackFxn
 
I2C_BitRate bitRate
 
void * custom
 

Detailed Description

I2C Parameters.

I2C parameters are used with the I2C_open() call. Default values for these parameters are set using I2C_Params_init().

See also
I2C_Params_init()

Field Documentation

§ transferMode

I2C_TransferMode I2C_Params_::transferMode

Specifies the I2C_TransferMode. Default is blocking.

§ transferCallbackFxn

I2C_CallbackFxn I2C_Params_::transferCallbackFxn

Callback function pointer used when I2C_TransferMode is I2C_MODE_CALLBACK.

§ bitRate

I2C_BitRate I2C_Params_::bitRate

I2C_BitRate_. The default is I2C_100kHz.

§ custom

void* I2C_Params_::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated