This module contains functions for device setup which is not done in boot code.
void SetupTrimDevice |
( |
void |
| ) |
|
Performs the necessary trim of the device which is not done in boot code.
This function should only execute coming from ROM boot. The current implementation does not take soft reset into account. However, it does no damage to execute it again. It only consumes time.
- Returns
- None
115 uint32_t ui32Fcfg1Revision;
116 uint32_t ui32AonSysResetctl;
121 if ( ui32Fcfg1Revision == 0xFFFFFFFF ) {
122 ui32Fcfg1Revision = 0;
136 NOROM_SetupSetCacheModeAccordingToCcfgSetting();
148 if( ! ( HWREGBITW(
AON_IOC_BASE + AON_IOC_O_IOCLATCH, AON_IOC_IOCLATCH_EN_BITN )))
void ThisLibraryIsFor_CC13x2_CC26x2_HwRev1x_HaltIfViolated(void)
Verifies that current chip is CC13x2 or CC26x2 PG1.x and never returns if violated.
Definition: chipinfo.c:199
static void TrimAfterColdResetWakeupFromShutDownWakeupFromPowerDown(void)
Trims to be applied when coming from POWER_DOWN (also called when coming from SHUTDOWN and PIN_RESET)...
Definition: setup.c:226
static void TrimAfterColdResetWakeupFromShutDown(uint32_t ui32Fcfg1Revision)
Trims to be applied when coming from SHUTDOWN (also called when coming from PIN_RESET).
Definition: setup.c:294
void SetupSetCacheModeAccordingToCcfgSetting(void)
Set correct VIMS_MODE according to CCFG setting (CACHE or GPRAM)
Definition: setup_rom.c:884
static void TrimAfterColdReset(void)
Trims to be applied when coming from PIN_RESET.
Definition: setup.c:477