SHA2 Global configuration. More...
#include <SHA2.h>
Data Fields | |
void * | object |
void const * | hwAttrs |
SHA2 Global configuration.
The SHA2_Config structure contains a set of pointers used to characterize the SHA2 driver implementation.
This structure needs to be defined before calling SHA2_init() and it must not be changed thereafter.
void* SHA2_Config_::object |
Pointer to a driver specific data object
void const* SHA2_Config_::hwAttrs |
Pointer to a driver specific hardware attributes structure