![]() |
![]() |
RF Hardware attributes. More...
#include <RF.h>
Data Fields | |
uint8_t | hwiPriority |
Priority for HWIs belong to the RF driver. More... | |
uint8_t | swiPriority |
Priority for SWIs belong to the RF driver. More... | |
bool | xoscHfAlwaysNeeded |
Indicate that the XOSC HF should be turned on by the power driver. More... | |
RF_GlobalCallback | globalCallback |
Pointer to a callback function serving client independent events listed in RF_GlobalEvent. More... | |
RF_GlobalEventMask | globalEventMask |
Event mask which the globalCallback is invoked upon. More... | |
RF Hardware attributes.
This data structure contains platform-specific driver configuration. It is usually defined globally in a board support file.
uint8_t RFCC26XX_HWAttrsV2::hwiPriority |
Priority for HWIs belong to the RF driver.
uint8_t RFCC26XX_HWAttrsV2::swiPriority |
Priority for SWIs belong to the RF driver.
bool RFCC26XX_HWAttrsV2::xoscHfAlwaysNeeded |
Indicate that the XOSC HF should be turned on by the power driver.
RF_GlobalCallback RFCC26XX_HWAttrsV2::globalCallback |
Pointer to a callback function serving client independent events listed in RF_GlobalEvent.
RF_GlobalEventMask RFCC26XX_HWAttrsV2::globalEventMask |
Event mask which the globalCallback is invoked upon.