RAM¶
There is 20kB of RAM available in the system. The various sections of RAM and their associated linker files are as follows.
- CSTACK: This the system callstack used by the C main function and HWIs. See System Stack for more information
- RAM Reset Vector Table: This table holds entries for all supported reset vectors. It is initialized from the flash reset vector table at boot time and is used to plug interrupt table entries at runtime. See RAM Vector Table for more information.
- ROM Reserved RAM: When building a configuration that links to code in
ROM certain sections of RAM must be reserved for the static allocations
performed in ROM. This includes the
RTOSRAM_SIZE
sections in Table 14.. If the active configuration doesn’t use ROM,these sections may be used for other purposes. - HEAP: All configurations require that a heap must be present for dynamic memory allocation. This heap is shared between the app and stack. There are multiple configurations of the heap that may be used, each has associated tradeoffs. See Dynamic Memory Allocation for information about heaps. Additionally see Debugging Common Heap Issues for more information on debugging common heap issues.
For projects where the stack project builds a library:
- Application and Stack statically allocated data: This includes any initialized and uninitialized variables used by the application or stack. (.data,.bss)
RAM Vector Table¶
As detailed in the Flash Vector Table section, this table is
intialized at kernel boot time with the contents of the flash vector table.
The location of this table is controlled by m3Hwi.vectorTableAddress
within
the TI-RTOS config file (*.cfg), it defaults to address 0x20000000.
The VTOR register will point to this table, which allows the creation of
dynamic interrupts at runtime. This table will contain entries for all 50
supported interrupts.
For more information about the vector table format, please refer to Cortex-M3 Vector Table.
System Stack¶
As described in Tasks, each task has its own runtime stack for context switching. Another runtime stack is used by the RTOS for main(), HWIs, and SWIs. This system stack is allocated in the application linker file to be placed at the end of the RAM of the application.
For IAR, this RTOS system stack is defined by the CSTACK symbol:
////////////////////////////////////////////////////////////////////////////////
// Stack
define symbol STACK_SIZE = 0x400;
define symbol STACK_START = RAM_END + 1;
define symbol STACK_END = STACK_START - STACK_SIZE;
//
define symbol STACK_TOP = RAM_END + 1;
export symbol STACK_TOP;
// Runtime Stack
define block CSTACK with alignment = 8, size = STACK_SIZE { section .stack };
place at end of RAM { block CSTACK };
In IAR, to change the size of the CSTACK, adjust the STACK_SIZE symbol value in the linker configuration file (.icf) of the application.
For CCS, depending on the project’s current build configuration the RTOS system
stack is defined by the Program.stack
parameter in the ble_debug.cfg
or
ble_release.cfg
RTOS configuration file:
/* ================ Program configuration ================ */
/* main() and Hwi, Swi stack size */
Program.stack = 1024;
and placed by the linker in the RAM space of the application:
/* Create global constant that points to top of stack */
/* CCS: Change stack size under Project Properties */
__STACK_TOP = __stack + __STACK_SIZE;
Dynamic Memory Allocation¶
The system uses a single heap for dynamic memory allocation. This heap is shared between TI-RTOS, the protocol stack, and the application.
The RTOS configuration file that configures the heap depends on the project’s
build configuration. If the project’s current build configuration is
FlashROM_Debug
the file that configures the heap is ble_debug.cfg
.
If the project’s current build configuration is FlashROM_Release
the file
that configures the heap is ble_release.cfg
.
Using the RTOS configuration file above the heap can be configured in one of three ways. Regardless of the underlying heap implementation, the APIs to access the heap are common.
- OSAL Heap (legacy) - This is the legacy heap manager created to work with the stack. It is implemented by
rtos_heaposal.h
. The OSAL heap suppports creating variable sized blocks as well as freeing blocks.- TI-RTOS HeapMem - The most flexible heap implementation offered by the TI-RTOS kernel. HeapMem supports creating variable sized blocks as well as freeing blocks. It is implemented by
rtos_heapmem.h
when using RTOS in ROM and by direct calls when using RTOS in flash. See HeapMem with TI-RTOS in ROM for details on using the HeapMem module in ROM with the stack.- TI-RTOS HeapMem with HeapTrack - The most flexible heap implementation offered by the TI-RTOS kernel. HeapMem suppports creating variable sized blocks as well as freeing blocks. It is implemented by
rtos_heaptrack.h
when using RTOS in ROM and by direct calls when using RTOS in flash. On top of the functionality offered by HeapMem, HeapTrack offers additional debugging capability, at the cost of runtime performance. See HeapMem with TI-RTOS in ROM for details on using the HeapMem module in ROM with the stack.
Configuring the Heap¶
The active heap configuration is set via the HEAPMGR_CONFIG
variable. If
auto heapsizing is not used, the size of the heap is controlled via
HEAPMGR_SIZE
.The location of both the HEAPMGR_CONFIG
and
HEAPMGR_SIZE
variables are dependent on the project’s current build
configuration. These variables are defined in the app’s .cfg
file.
The system will default to using the OSAL heap with auto heap size. The table
below shows the possible configurations of the heap along with their associated
values of HEAPMGR_CONFIG
and HEAPMGR_SIZE
.
HEAPMGR_CONFIG |
Active Heap Configuration | Heap Size |
0x00 | OSAL HeapMgr, static heap size | Set by HEAPMGR_SIZE |
0x80 | OSAL HeapMgr, automatic heap size | Automatically determined by the amount of free space available at link time between heapStart and heapEnd symbols |
0x01 | HeapMem, static heap size | Set by HEAPMGR_SIZE |
0x81 | HeapMem, automatic heap size | Automatically determined by the amount of free space available at link time between heapStart and heapEnd symbols |
0x02 | HeapMem + HeapTrack, static heap size | Set by HEAPMGR_SIZE |
0x82 | HeapMem + HeapTrack, automatic heap size | Automatically determined by the amount of free space available at link time between heapStart and heapEnd symbols |
Warning
If autoheap size is to be used, heapStart
and heapEnd
symbols must
be defined in the linker file. See your application’s map file for the
location of these sections in the StackLibrary configuration.
heapStart
– Placed at end of static allocation sectionheapEnd
– Placed right before beginning of CSTACK section
See the snippet below from the app’s .cfg
to see how to change the
active heap configuration. Change the variable in the highlighted line to one of
the values supported in the table above.
1 2 3 4 var Memory = xdc.useModule('xdc.runtime.Memory'); var HEAPMGR_CONFIG = 0x00; //set to OSAL HeapMgr, static heap size var HEAPMGR_SIZE = 30000; //only valid if static size is used. This is the //size of the buffer allocated for Heap.
HeapMem with TI-RTOS in ROM¶
When using any HeapMem based configuration combined with TI-RTOS in ROM, the heap will be implemented by HeapCallback module. HeapCallback will call a user defined function whenever a dynamic memory operation is required. The user defined functions are located in the following files.
rtos_heapmem.h
– HeapMemrtos_heaptrack.h
– HeapMem + HeapTrack
This is required because the HeapMem implementation in ROM uses the GateMutex
module, which prevents malloc()
from being called in a hwi or
swi. In order to allow safe use of the heap a GateHWI must be used. To
work around this, the HeapCallback implementation will wrap any access to the
heap in a HWI lock. See the following example from rtos_heapmem.h
.
/* Protect since HeapMem_allocUnprotected does not */ hwikey = (uint_least16_t)Hwi_disable(); /* Using the default system heap for this example */ tmp = HeapMem_allocUnprotected(stackHeap, size, FORCED_ALIGNEMENT); // .. /* restore the hwi mutex */ Hwi_restore(hwikey);Note
Note that the legacy OSAL heap always protects heap operations with a HWI lock.
When using a flash based kernel, the HeapMem module is configured to use a
GateHWI, see the following excerpt from ble_debug.cfg
.
Program.global.stackHeap = HeapMem.create(heapMemParams); var GateHwi = xdc.useModule('ti.sysbios.gates.GateHwi'); HeapMem.common$.gate = GateHwi.create(); Memory.defaultHeapInstance = Program.global.stackHeap;
Profiling the Heap¶
Refer to Debugging Common Heap Issues for tips on debugging common heap issues. Each heap implementation has its benefits for debugging and some come with performance tradeoffs. Note the metrics function may be used by any supported heap configuration.
Note
The auto heap size feature does not determine the amount of heap needed for the application. The system designer must ensure that the heap has the required space to meet the application’s runtime memory requirements.
Heap APIs¶
Note that regardless of the heap implementation selected, the APIs are compatible across all supported heap implementations. The following APIs may be used to access the heap:
ICall_heapMalloc
– Dynamically allocate a block of memoryICall_heapFree
– Dynamically free a block of memoryICall_heapRealloc
– Resize an existing heap blockICall_heapGetStats
– Get information about the state of the heap
The following is an example of dynamically allocating a variable length (n) array using the ICall heap:
//define pointer
uint8_t *pArray;
// Create dynamic pointer to array.
if (pArray = (uint8_t*)ICall_malloc(n*sizeof(uint8_t)))
{
//fill up array
}
else
{
//not able to allocate
}
The following is an example of freeing the previous array:
ICall_free(pMsg->payload);
Cache¶
The cache is an 8 KB section of the device’s RAM reserved for the processor. The cache module temporarily stores data that has been read from the Flash, so that frequently used data is not fetched from Flash on each access. This reduces the number of CPU wait-states and saves power. When the cache is not used, it is not powered. This is true for Standby and Idle states where the cache is not in use.
AUX RAM¶
The AUX RAM is a 2 KB memory area belonging to the Sensor Controller.