TI BLE5-Stack API Documentation  2.02.00.00
Data Fields
attAttribute_t Struct Reference

GATT Attribute format. More...

Data Fields

uint16 handle
 Attribute handle - assigned internally by attribute server.
 
uint8 permissions
 Attribute permissions.
 
uint8 *const pValue
 
gattAttrType_t type
 Attribute type (2 or 16 octet UUIDs)
 

Detailed Description

GATT Attribute format.

Note
The list must start with a Service attribute followed by all attributes associated with this Service attribute.

Field Documentation

§ pValue

uint8* const pValue

Attribute value - encoding of the octet array is defined in the applicable profile. The maximum length of an attribute value shall be 512 octets.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale