TI BLE5-Stack API Documentation
2.01.03.00
|
Data Fields | |
uint16_t | connectionHandle |
Connection Handle. | |
uint8_t | deviceAddr [B_ADDR_LEN] |
address of device requesting pairing | |
osal_event_hdr_t | hdr |
GAP_MSG_EVENT and status | |
uint8_t | opcode |
GAP_BOND_LOST_EVENT | |
GAP_BOND_LOST_EVENT message format.
This message is sent to the app as indication that the bond has been removed on peer.
This event will be consumed by the gapbondmgr if it exists.