UART driver implementation for a CC26X2 UART controller.
============================================================================
The UART header file should be included in an application as follows:
Refer to UART2.h for a complete description of APIs and examples of use.
#include <stddef.h>
#include <stdint.h>
#include <stdbool.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(inc/hw_types.h)>
#include <DeviceFamily_constructPath(driverlib/udma.h)>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/UART2.h>
#include <ti/drivers/pin/PINCC26XX.h>
#include <ti/drivers/dma/UDMACC26XX.h>
Go to the source code of this file.
Data Structures | |
struct | UART2CC26X2_HWAttrs |
UART2CC26X2 Hardware attributes. More... | |
struct | UART2CC26X2_Object |
UART2CC26X2 Object. More... | |
Macros | |
#define | UART2CC26X2_FLOWCTRL_NONE 0 |
No hardware flow control. More... | |
#define | UART2CC26X2_FLOWCTRL_HARDWARE 1 |
Hardware flow control. More... | |
#define | UART2CC26X2_FIFO_SIZE 32 |
Typedefs | |
typedef struct UART2CC26X2_Object * | UART2CC26X2_Handle |
Enumerations | |
enum | UART2CC26X2_FifoThreshold { UART2CC26X2_FIFO_THRESHOLD_1_8 = 0, UART2CC26X2_FIFO_THRESHOLD_2_8 = 1, UART2CC26X2_FIFO_THRESHOLD_4_8 = 2, UART2CC26X2_FIFO_THRESHOLD_6_8 = 3, UART2CC26X2_FIFO_THRESHOLD_7_8 = 4 } |
UART TX/RX interrupt FIFO threshold select. More... | |
Functions | |
void | UART2CC26X2_close (UART2_Handle handle) |
void | UART2CC26X2_flushRx (UART2_Handle handle) |
UART2_Handle | UART2CC26X2_open (uint_least8_t, UART2_Params *params) |
int_fast16_t | UART2CC26X2_read (UART2_Handle handle, void *buffer, size_t size, size_t *bytesRead, uint32_t timeout) |
void | UART2CC26X2_readCancel (UART2_Handle handle) |
int_fast16_t | UART2CC26X2_write (UART2_Handle handle, const void *buffer, size_t size, size_t *bytesWritten, uint32_t timeout) |
void | UART2CC26X2_writeCancel (UART2_Handle handle) |
Variables | |
const UART2_FxnTable | UART2CC26X2_fxnTable |
#define UART2CC26X2_FLOWCTRL_NONE 0 |
No hardware flow control.
#define UART2CC26X2_FLOWCTRL_HARDWARE 1 |
Hardware flow control.
#define UART2CC26X2_FIFO_SIZE 32 |
Size of the TX and RX FIFOs is 32 items
typedef struct UART2CC26X2_Object * UART2CC26X2_Handle |
UART TX/RX interrupt FIFO threshold select.
Defined FIFO thresholds for generation of both TX interrupt and RX interrupt. If the RX and TX FIFO and thresholds are not set in the HwAttrs, the RX interrupt FIFO threshold is set to 1/8 full, and the TX interrupt FIFO threshold is set to 1/8 full.
void UART2CC26X2_close | ( | UART2_Handle | handle | ) |
void UART2CC26X2_flushRx | ( | UART2_Handle | handle | ) |
UART2_Handle UART2CC26X2_open | ( | uint_least8_t | , |
UART2_Params * | params | ||
) |
int_fast16_t UART2CC26X2_read | ( | UART2_Handle | handle, |
void * | buffer, | ||
size_t | size, | ||
size_t * | bytesRead, | ||
uint32_t | timeout | ||
) |
void UART2CC26X2_readCancel | ( | UART2_Handle | handle | ) |
int_fast16_t UART2CC26X2_write | ( | UART2_Handle | handle, |
const void * | buffer, | ||
size_t | size, | ||
size_t * | bytesWritten, | ||
uint32_t | timeout | ||
) |
void UART2CC26X2_writeCancel | ( | UART2_Handle | handle | ) |
const UART2_FxnTable UART2CC26X2_fxnTable |