Radio Software Bundle (rflib) 5.10.01.00 Release Notes
Table of Contents
Introduction
The Radio Software Bundle (RFLib) component for CC13x2 and CC26x2 consists of products that were previously hosted in different locations and distributed through TIDRIVERS, TIDRIVERS examples and DriverLib:
- The high-level RF driver
- SysConfig meta data for configuring the RF driver and the front-end
- SysConfig meta data for configuring radio PHYs
- Low-level radio access functions used by the RF driver
- RF Core firmware patches for various PHYs
- API documentation
Documentation
The following documentation is included in RFLib.
- RFLib Software Manifest
- API documentation
- Release Notes (this document)
What’s New
ID | Summary |
---|---|
RFDRIVER-146 | SYSCFG: Add support for configuring BLE/WiFi coexistence interface |
RFDRIVER-144 | Introduce a new global event RF_GlobalEventInit which can be used to initialize pins |
RFDRIVER-304 | SYSCFG: Allow overriding generated rfDriverCallback when custom board is used |
SRFSTUDIO-2582 | SYSCFG: CC1352R/P, CC1312R: Add preview settings for 4.8 kbps OOK PHY |
SRFSTUDIO-2581 | SYSCFG: CC1352P/CC2652P: Add 10 dBm settings |
SRFSTUDIO-2577 | SYSCFG: Provide define to tell index of stack specific overrides |
SRFSTUDIO-2571 | SYSCFG: Add possibility to modify front-end settings from the UI |
SRFSTUDIO-2613 | SYSCFG: CC1352R/P, CC1312R: Add 1 Mbps 2-GFSK 868/915 MHz PHY settings |
SRFSTUDIO-2600 | SYSCFG: CC1352R/P, CC1312R: Add SimpleLink Long Range (SLR) 433 MHz PHY settings |
SRFSTUDIO-2670 | SYSCFG: CC1352R/P, CC1312R: Add 15.4g 50kbps 433 MHz PHY settings |
SRFSTUDIO-2673 | SYSCFG: CC1352P/R, CC1312: Add 200 kbps 433 MHz proprietary PHY settings |
SRFSTUDIO-2672 | SYSCFG: CC1352R/P, CC1312R: Add 4.8 kbps GFSK 433 MHz PHY settings |
Fixed Issues
ID | Summary |
---|---|
RFDRIVER-319 | RF driver enters Error_policySpin with BIOS asserts enabled because PIN_open was called from SWI when using antenna switching |
RFDRIVER-279 | RAT Timer should allow for RAT Channel owner to disable the channel |
RFDRIVER-269 | Bus Error reading RAT registers when RAT module is powered down |
RFDRIVER-305 | SYSCFG: RF driver callback function name will sometimes be used undefined |
RFDRIVER-335 | Add support for BLE/WiFi coexistence interface (Modes: 3-wire, 1-wire GRANT, and 1-wire REQUEST) |
RFCORE-469 | IEEE RX command ending while TX was starting left TX command in active state with no transmission |
SRFSTUDIO-2671 | SYSCFG: CC1352R/P, CC2652R/P: Fixed issue in 100/250 kbps GFSK and 250 kbps MSK PHY settings causing higher current consumption. RF performance is unchanged. |
SRFSTUDIO-2674 | CC1352P/R, CC1312R: Updated settings improving phase noise in Sub-1 GHz narrowband PHYs |
Known Issues
ID | Summary |
---|---|
None | None |
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of the CC13x2/CC26x2 RF driver in the following ways:
- None known
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.