rflib
Data Fields
rfc_CMD_CHANGE_PA_s Struct Reference

Set TX power with possibility to switch between PAs. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0015. More...
 
uint16_t __dummy0
 
uint32_t * pRegOverride
 Pointer to a list of hardware and configuration registers to override as part of the change, including new TX power. More...
 

Detailed Description

Set TX power with possibility to switch between PAs.

Field Documentation

§ commandNo

uint16_t rfc_CMD_CHANGE_PA_s::commandNo

The command ID number 0x0015.

§ __dummy0

uint16_t rfc_CMD_CHANGE_PA_s::__dummy0

§ pRegOverride

uint32_t* rfc_CMD_CHANGE_PA_s::pRegOverride

Pointer to a list of hardware and configuration registers to override as part of the change, including new TX power.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale