TI BLE5-Stack API Documentation  2.01.02.00
Enumerations
GapScan Params

Enumerations

enum  GapScan_ParamId_t {
  SCAN_PARAM_RPT_FIELDS, SCAN_PARAM_PRIM_PHYS, SCAN_PARAM_FLT_POLICY, SCAN_PARAM_FLT_PDU_TYPE,
  SCAN_PARAM_FLT_MIN_RSSI, SCAN_PARAM_FLT_DISC_MODE, SCAN_PARAM_FLT_DUP, SCAN_PARAM_NUM_ADV_RPT = SCAN_NUM_RW_PARAM
}
 

Detailed Description

Params used in the GapAdv module

Enumeration Type Documentation

§ GapScan_ParamId_t

GAP Scanner Parameters

These can be set with GapScan_setParam and read with GapScan_getParam. The default values below refer to the values that are set at initialization.

Enumerator
SCAN_PARAM_RPT_FIELDS 

Advertising Report Fields (R/W)

Bit mask of which fields in the GapScan_Evt_AdvRpt_t need to be stored in the AdvRptList

Note
Change of this parameter shall not be attempted while scanning is active

size: uint16_t

default: SCAN_PARAM_DFLT_RPT_FIELDS

range: combination of individual values in GapScan_AdvRptField_t

SCAN_PARAM_PRIM_PHYS 

Primary Scanning Channel PHYs (R/W)

PHYs on which advertisements should be received on the primary advertising channel.

Note
Change of this parameter will not affect an ongoing scanning. If changed during scanning, it will take effect when the scanning is re-enabled after disabled.

size: uint8_t

default: SCAN_PARAM_DFLT_PHYS

range: GapScan_PrimPhy_t

SCAN_PARAM_FLT_POLICY 

Scanning Filter Policy (R/W)

Policy of how to apply white list to filter out unwanted packets

Note
Change of this parameter will not affect an ongoing scanning. If changed during scanning, it will take effect when the scanning is re-enabled after disabled.

size: uint8_t

default: SCAN_PARAM_DFLT_FLT_POLICY

range: GapScan_FilterPolicy_t

SCAN_PARAM_FLT_PDU_TYPE 

Filter by PDU Type (R/W)

This filter value specifies packets of which types in 6 different category sets are wanted. The 6 sets include Connectable/Non-Connectable, Scannable/Non-Scannable, Directed/Undirected, ScanRsp/Adv, Legacy/Extended, and Complete/Incomplete category sets. Each set has two mutually exclusive types. Only one type in a set can be* chosen. For example, SCAN_FLT_PDU_NONSCANNABLE_ONLY and SCAN_FLT_PDU_SCANNABLE_ONLY cannot be chosen together. Only either one can be used. If neither type is selected in a set, the filter will not care about the category. For example, if neither SCAN_FLT_PDU_NONCONNECTABLE_ONLY nor SCAN_FLT_PDU_CONNECTABLE_ONLY is set in the parameter value, the scanner will accept both connectable packets and non-connectable packets.

Usage example:

With the call above, the scanner will receive only connectable, undirected, extended(non-legacy), and complete packets. It will not be examined whether the packets are scannable or non-scannable and whether they are scan responses or advertisements.

size: uint16_t

default: SCAN_PARAM_DFLT_FLT_PDU

range: combination of individual values in GapScan_FilterPduType_t

SCAN_PARAM_FLT_MIN_RSSI 

Filter by Minimum RSSI (R/W)

Only packets received with the specified RSSI or above will be accepted.

Note
-128 means to ignore RSSI (to not filter out any packet by RSSI)

size: int8_t

default: -128 (ignore)

range: -128 - 127 (dBm)

SCAN_PARAM_FLT_DISC_MODE 

Filter by Discoverable Mode (R/W)

Note
Change of this parameter shall not be attempted while scanning is active

size: uint8_t

default: SCAN_PARAM_DFLT_FLT_DISC

range: GapScan_FilterDiscMode_t

SCAN_PARAM_FLT_DUP 

Duplicate Filtering (R/W)

Specify whether and when to filter out duplicated packets by DID and address

Note
Change of this parameter will not affect an ongoing scanning. If changed during scanning, it will take effect when the scanning is re-enabled after disabled.

size: uint8_t

default: SCAN_PARAM_DFLT_FLT_DUP

range: GapScan_FilterDuplicate_t

SCAN_PARAM_NUM_ADV_RPT 

Number of Reports Recorded (R)

Number of advertising reports recorded since the current scanning started.

Note
This number will be the same as numReport that will come with GAP_EVT_SCAN_DISABLED when the scanning has ended.

size: uint8_t

range: 0 up to maxNumReport specified when GapScan_enable() is called

© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale