This module implements the Generic Access Protocol (GAP)
More...
|
file | gap.h |
| GAP layer interface.
|
|
|
bStatus_t | GAP_Authenticate (gapAuthParams_t *pParams, gapPairingReq_t *pPairReq) |
|
bStatus_t | GAP_Bond (uint16_t connectionHandle, uint8_t authenticated, uint8_t secureConnections, smSecurityInfo_t *pParams, uint8_t startEncryption) |
|
bStatus_t | GAP_DeviceInit (uint8_t profileRole, uint8_t taskID, GAP_Addr_Modes_t addrMode, uint8_t *pRandomAddr) |
|
bStatus_t | GAP_DeviceInit_noGAPBondMgr (uint8_t profileRole, uint8_t taskID, GAP_Addr_Modes_t addrMode, uint8_t *pRandomAddr) |
|
uint8_t * | GAP_GetDevAddress (uint8 wantIA) |
|
uint8_t * | GAP_GetIRK (void) |
|
uint16_t | GAP_GetParamValue (uint16_t paramID) |
|
uint8_t * | GAP_GetSRK (void) |
|
void | GAP_Init (uint8_t task_id) |
|
uint8_t | GAP_isPairing (void) |
|
uint8_t | GAP_NumActiveConnections (void) |
|
bStatus_t | GAP_PasscodeUpdate (uint32_t passcode, uint16_t connectionHandle) |
|
bStatus_t | GAP_PasskeyUpdate (uint8_t *pPasskey, uint16_t connectionHandle) |
|
uint16_t | GAP_ProcessEvent (uint8_t task_id, uint16_t events) |
|
void | GAP_RegisterBondMgrCBs (gapBondMgrCBs_t *pCBs) |
|
bStatus_t | Gap_RegisterConnEventCb (pfnGapConnEvtCB_t cb, GAP_CB_Action_t action, uint16_t connHandle) |
|
void | GAP_RegisterForMsgs (uint8_t taskID) |
|
bStatus_t | GAP_SendSlaveSecurityRequest (uint16_t connectionHandle, uint8_t authReq) |
|
bStatus_t | GAP_SetParamValue (uint16_t paramID, uint16_t paramValue) |
|
bStatus_t | GAP_SetPrivacyMode (GAP_Peer_Addr_Types_t addrType, uint8_t *pAddr, uint8_t mode) |
|
bStatus_t | GAP_Signable (uint16_t connectionHandle, uint8_t authenticated, smSigningInfo_t *pParams) |
|
bStatus_t | GAP_TerminateAuth (uint16_t connectionHandle, uint8_t reason) |
|
bStatus_t | GAP_TerminateLinkReq (uint16_t connectionHandle, uint8_t reason) |
|
bStatus_t | GAP_UpdateLinkParamReq (gapUpdateLinkParamReq_t *pParams) |
|
bStatus_t | GAP_UpdateLinkParamReqReply (gapUpdateLinkParamReqReply_t *pParams) |
|
bStatus_t | GapConfig_SetParameter (Gap_configParamIds_t param, void *pValue) |
|
This module implements the Generic Access Protocol (GAP)
§ GAP_IS_ADDR_RAND
#define GAP_IS_ADDR_RAND |
( |
|
pAddr | ) |
|
Value: GAP_IS_ADDR_RPN(pAddr) | \
GAP_IS_ADDR_RS(pAddr))
#define GAP_IS_ADDR_RPR(pAddr)
Definition: gap.h:55
Is the address any type of random address?
§ GAP_IS_ADDR_RPN
#define GAP_IS_ADDR_RPN |
( |
|
pAddr | ) |
|
Value:#define RANDOM_ADDR_HDR_MASK
Get top 2 bits of address.
Definition: gap.h:619
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
#define PRIVATE_NON_RESOLVE_ADDR_HDR
Random Private Non-Resolvable Address (b10)
Definition: gap.h:623
Is the address random private non-resolvable (NRPA)?
- Parameters
-
- Returns
- TRUE the address is an NRPA
-
FALSE the address is not an NRPA
§ GAP_IS_ADDR_RPR
#define GAP_IS_ADDR_RPR |
( |
|
pAddr | ) |
|
Value:#define RANDOM_ADDR_HDR_MASK
Get top 2 bits of address.
Definition: gap.h:619
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
#define PRIVATE_RESOLVE_ADDR_HDR
Random Private Resolvable Address (b01)
Definition: gap.h:625
Is the address random private resolvable (RPA)?
- Parameters
-
- Returns
- TRUE the address is an RPA
-
FALSE the address is not an RPA
§ GAP_IS_ADDR_RS
#define GAP_IS_ADDR_RS |
( |
|
pAddr | ) |
|
Value:#define STATIC_ADDR_HDR
Random Static Address (b11)
Definition: gap.h:621
#define RANDOM_ADDR_HDR_MASK
Get top 2 bits of address.
Definition: gap.h:619
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
Is the address random static?
- Parameters
-
- Returns
- TRUE the address is random static
-
FALSE the address is not random static
§ GAP_Authenticate()
§ GAP_Bond()
bStatus_t GAP_Bond |
( |
uint16_t |
connectionHandle, |
|
|
uint8_t |
authenticated, |
|
|
uint8_t |
secureConnections, |
|
|
smSecurityInfo_t * |
pParams, |
|
|
uint8_t |
startEncryption |
|
) |
| |
Set up the connection's bound parameters.
- Warning
- This API should not be called by the application if the gapbondmgr exists as it will be used automatically when a connection is formed to a previously bonded device
- Corresponding Events:
- GAP_BOND_COMPLETE_EVENT of type gapBondCompleteEvent_t
- Parameters
-
connectionHandle | connection handle of the signing information |
authenticated | TRUE if bond is authenticated. |
secureConnections | TRUE if bond has Secure Connections strength. |
pParams | the connected device's security parameters |
startEncryption | whether or not to start encryption |
- Returns
- SUCCESS
-
bleIncorrectMode : Not correct profile role
-
INVALIDPARAMETER
-
bleNotConnected
-
FAILURE : not workable
§ GAP_DeviceInit()
GAP Device Initialization
Setup the device. Can only be called once per reset. In order to change the address mode / random address, it is necessary to reset the device and call this API again. In the case where the address mode or random address is different than it was for the last initialization, all bonds and local information stored in NV will be erased.
- Corresponding Events:
- GAP_DEVICE_INIT_DONE_EVENT of type gapDeviceInitDoneEvent_t
- Parameters
-
- Returns
- SUCCESS : initialization started
-
INVALIDPARAMETER : invalid profile role, role combination, or invalid Random Static Address,
-
bleIncorrectMode : initialization has already occurred
-
bleInternalError : error erasing NV
§ GAP_DeviceInit_noGAPBondMgr()
bStatus_t GAP_DeviceInit_noGAPBondMgr |
( |
uint8_t |
profileRole, |
|
|
uint8_t |
taskID, |
|
|
GAP_Addr_Modes_t |
addrMode, |
|
|
uint8_t * |
pRandomAddr |
|
) |
| |
GAP Device Initialization with no GAP Bond Manager
Setup the device. Can only be called once per reset, in case GAPBondMgr is not enabled. In order to change the address mode / random address, it is necessary to reset the device and call this API again. In the case where the address mode or random address is different than it was for the last initialization, all local information stored in NV will be erased.
- Corresponding Events:
- GAP_DEVICE_INIT_DONE_EVENT of type gapDeviceInitDoneEvent_t
- Parameters
-
- Returns
- SUCCESS : initialization started
-
INVALIDPARAMETER : invalid profile role, role combination, or invalid Random Static Address,
-
bleIncorrectMode : initialization has already occurred
§ GAP_GetDevAddress()
uint8_t* GAP_GetDevAddress |
( |
uint8 |
wantIA | ) |
|
Get the address of this device
- Parameters
-
- Returns
- pointer to device address.
§ GAP_GetIRK()
uint8_t* GAP_GetIRK |
( |
void |
| ) |
|
Get the IRK
- Warning
- The memory indicated by the returned pointer should not be modified directly if it is desired to update the IRK. Instead, use the GAP_CONFIG_PARAM_IRK
- Returns
- pointer to the 16-byte IRK
§ GAP_GetParamValue()
uint16_t GAP_GetParamValue |
( |
uint16_t |
paramID | ) |
|
Get a GAP Parameter value.
- Parameters
-
- Returns
- GAP Parameter value
-
0xFFFF if invalid
§ GAP_GetSRK()
uint8_t* GAP_GetSRK |
( |
void |
| ) |
|
Get the SRK
- Warning
- The memory indicated by the returned pointer should not be modified directly if it is desired to update the SRK. Instead, use the GAP_CONFIG_PARAM_SRK
- Returns
- pointer to the 16-byte SRK
§ GAP_Init()
void GAP_Init |
( |
uint8_t |
task_id | ) |
|
Initialization for GAP module
This should only be used in osal_icall_ble.c in osalInitTasks()
- Parameters
-
§ GAP_isPairing()
uint8_t GAP_isPairing |
( |
void |
| ) |
|
Check if GAP is currently pairing.
- Note
- This API is not needed if the gapbondmgr exists as pairing states are returned via the pfnPairStateCB_t callback
- Returns
- TRUE if pairing
-
FALSE otherwise
§ GAP_NumActiveConnections()
uint8_t GAP_NumActiveConnections |
( |
void |
| ) |
|
Returns the number of active connections.
- Returns
- Number of active connections.
§ GAP_PasscodeUpdate()
bStatus_t GAP_PasscodeUpdate |
( |
uint32_t |
passcode, |
|
|
uint16_t |
connectionHandle |
|
) |
| |
Update the passkey in a numeric value (not string).
This API should be called in response to receiving a GAP_PASSKEY_NEEDED_EVENT
- Note
- This function is the same as GAP_PasskeyUpdate, except that the passkey is passed in as a non-string format.
- Parameters
-
passcode | not string - range: 0 - 999,999. |
connectionHandle | connection handle. |
- Returns
- SUCCESS : will start pairing with this entry
-
bleIncorrectMode : Link not found
-
INVALIDPARAMETER : passkey == NULL or passkey isn't formatted properly
§ GAP_PasskeyUpdate()
bStatus_t GAP_PasskeyUpdate |
( |
uint8_t * |
pPasskey, |
|
|
uint16_t |
connectionHandle |
|
) |
| |
Update the passkey in string format.
This API should be called in response to receiving a GAP_PASSKEY_NEEDED_EVENT
- Note
- This function is the same as GAP_PasscodeUpdate, except that the passkey is passed in as a string format.
- Warning
- This API should not be called by the application if the gapbondmgr exists as it is abstracted through GAPBondMgr_PasscodeRsp
- Parameters
-
pPasskey | new passkey - pointer to numeric string (ie. "019655" ) This string's range is "000000" to "999999" |
connectionHandle | connection handle. |
- Returns
- SUCCESS : will start pairing with this entry
-
bleIncorrectMode : Link not found
-
INVALIDPARAMETER : passkey == NULL or passkey isn't formatted properly
§ GAP_ProcessEvent()
uint16_t GAP_ProcessEvent |
( |
uint8_t |
task_id, |
|
|
uint16_t |
events |
|
) |
| |
GAP Module event processing
This should only be used in osal_icall_ble.c in tasksArr[]
- Parameters
-
task_id | OSAL task ID |
events | OSAL event received |
- Returns
- bitmask of events that weren't processed
§ GAP_RegisterBondMgrCBs()
Register bond manager call backs
- Parameters
-
pCBs | pointer to Bond Manager Callbacks. |
§ Gap_RegisterConnEventCb()
Register/Unregister a connection event callback
It is only possible to register for one connection handle of for all connection handles. In the case of unregistering, it does not matter what connHandle or cb is passed in as whatever is currently registered will be unregistered.
- Warning
- The application owns the memory pointed to by pReport in pfnGapConnEvtCB_t. That is, it is responsible for freeing this memory.
- Note
- The callback needs to be registered for each reconnection. It is not retained across a disconnect / reconnect.
- Parameters
-
cb | Function pointer to a callback. |
action | Register or unregister the callback. |
connHandle | if LINKDB_CONNHANDLE_ALL, apply to all connections.
else, apply only for a specific connection. |
- Returns
- SUCCESS
-
bleGAPNotFound : connection handle not found
-
bleInvalidRange : the callback function was NULL or action is invalid
-
bleMemAllocError : there is not enough memory to register the callback.
§ GAP_RegisterForMsgs()
void GAP_RegisterForMsgs |
( |
uint8_t |
taskID | ) |
|
Register for GAP Messages
Register a task ID to receive extra (unprocessed) HCI status and complete, and Host events.
- Parameters
-
taskID | Default task ID to send events. |
§ GAP_SendSlaveSecurityRequest()
bStatus_t GAP_SendSlaveSecurityRequest |
( |
uint16_t |
connectionHandle, |
|
|
uint8_t |
authReq |
|
) |
| |
Generate a Slave Requested Security message to the master.
- Warning
- This API should not be called by the application if the gapbondmgr exists as it will be used automatically based on GAPBOND_PAIRING_MODE and the GAP role of the device
- Parameters
-
connectionHandle | connection handle. |
authReq | Authentication Requirements: Bit 2: MITM, Bits 0-1: bonding (0 - no bonding, 1 - bonding) Bit 3: Secure Connections |
- Returns
- SUCCESS : will send
-
bleNotConnected : Link not found
-
bleIncorrectMode : wrong GAP role, must be a Peripheral Role
§ GAP_SetParamValue()
bStatus_t GAP_SetParamValue |
( |
uint16_t |
paramID, |
|
|
uint16_t |
paramValue |
|
) |
| |
Set a GAP Parameter value
Use this function to change the default GAP parameter values.
- Parameters
-
- Returns
- SUCCESS
-
INVALIDPARAMETER
§ GAP_SetPrivacyMode()
Set the Privacy Mode of the requested device to the desired mode.
- Warning
- This should not be called if the bond manager is present as the bond manager will handle this automatically based on the connected device's capabilities and the own device's capabilities.
- Parameters
-
addrType | remote device's identity address type |
pAddr | pointer to the address |
mode | GAP Privacy Modes to use for this device |
- Returns
- SUCCESS : match
-
FAILURE : don't match
-
INVALIDPARAMETER : parameters invalid
§ GAP_Signable()
Set up the connection to accept signed data.
- Warning
- This API should not be called by the application if the gapbondmgr exists as it will be used automatically when signing occurs
- Parameters
-
connectionHandle | connection handle of the signing information |
authenticated | TRUE if the signing information is authenticated, FALSE otherwise |
pParams | signing parameters |
- Returns
- SUCCESS
-
bleIncorrectMode : Not correct profile role
-
INVALIDPARAMETER
-
bleNotConnected
-
FAILURE : not workable
§ GAP_TerminateAuth()
bStatus_t GAP_TerminateAuth |
( |
uint16_t |
connectionHandle, |
|
|
uint8_t |
reason |
|
) |
| |
§ GAP_TerminateLinkReq()
bStatus_t GAP_TerminateLinkReq |
( |
uint16_t |
connectionHandle, |
|
|
uint8_t |
reason |
|
) |
| |
§ GAP_UpdateLinkParamReq()
Update the link parameters to a Master or Slave device.
As long as LL connection updates are supported on the own device (which is the case by default), an LL Connection Update procedure will be attempted. If this fails, the stack will automatically attempt an L2CAP parameter update request.
- Corresponding Events:
- After the update procedure is complete, the calling task will receive a GAP_LINK_PARAM_UPDATE_EVENT of type gapLinkUpdateEvent_t regardless of the connection parameter update procedure that occurred.
- Parameters
-
pParams | link update parameters |
- Returns
- SUCCESS : update request sent to stack
-
INVALIDPARAMETER : one of the parameters were invalid
-
bleIncorrectMode : invalid profile role
-
bleAlreadyInRequestedMode : already updating link parameters
-
bleNotConnected : not in a connection
§ GAP_UpdateLinkParamReqReply()
§ GapConfig_SetParameter()