Running the Example Applications

This section provides an overview of the Z-Stack out-of-box example applications and instructions on how to run them. The examples are out-of-box compliant with the ZCL v7 Specification but will further Product Certification will be required.

Note

Most examples have a coordinator, end device and router application. Green Power Device examples complement the Sink coordinator/router examples. The Network Processor is standalone.

Note

All the sample applications are supported for the three platforms CC26X2R1, CC1352R1 and CC1352P_2. If a different platform is intended to be used, just replace the board name in the path to find the corresponding README document.(e.g. “examples/rtos/CC1352R1_LAUNCHXL/zstack/zc_doorlock/README.html” if CC1352R1 platform is intended).

Control and Indicating Equipment (CIE)

Door Lock

Door Lock Controller

Generic App

Green Power Switch

Green Power Temperature Sensor

Light

Light Sink

Network Processor

OTA Server

Switch

Switch OTA

Temperature Sensor

Thermostat

Thermostat Sink

Warning Device

Zone Device