![]() |
![]() |
ECB Parameters. More...
#include <AESECB.h>
Data Fields | |
AESECB_ReturnBehavior | returnBehavior |
AESECB_CallbackFxn | callbackFxn |
uint32_t | timeout |
void * | custom |
ECB Parameters.
ECB Parameters are used to with the AESECB_open() call. Default values for these parameters are set using AESECB_Params_init().
AESECB_ReturnBehavior AESECB_Params::returnBehavior |
Blocking, callback, or polling return behavior
AESECB_CallbackFxn AESECB_Params::callbackFxn |
Callback function pointer
uint32_t AESECB_Params::timeout |
Timeout before the driver returns an error in AESECB_RETURN_BEHAVIOR_BLOCKING
void* AESECB_Params::custom |
Custom argument used by driver implementation