TI BLE5-Stack API Documentation
2.00.04.00
|
This module implements the Attribute Protocol and Generic Attribute Protocol. More...
Modules | |
ATT / GATT Constants | |
ATT / GATT Stuctures | |
ATT API Functions | |
Files | |
file | att.h |
ATT layer interface. | |
file | gatt.h |
GATT layer interface. | |
Functions | |
void * | GATT_bm_alloc (uint16 connHandle, uint8 opcode, uint16 size, uint16 *pSizeAlloc) |
GATT implementation of the allocator functionality. More... | |
void | GATT_bm_free (gattMsg_t *pMsg, uint8 opcode) |
GATT implementation of the de-allocator functionality. More... | |
bStatus_t | GATT_DeregisterService (uint16 handle, gattService_t *pService) |
Deregister a service attribute list with the GATT Server. More... | |
bStatus_t | GATT_DiscAllCharDescs (uint16 connHandle, uint16 startHandle, uint16 endHandle, uint8 taskId) |
Discovery All Characteristic Descriptors. More... | |
bStatus_t | GATT_DiscAllChars (uint16 connHandle, uint16 startHandle, uint16 endHandle, uint8 taskId) |
Discover all Characteristics. More... | |
bStatus_t | GATT_DiscAllPrimaryServices (uint16 connHandle, uint8 taskId) |
Discovery All Primary Services. More... | |
bStatus_t | GATT_DiscCharsByUUID (uint16 connHandle, attReadByTypeReq_t *pReq, uint8 taskId) |
Discovery Characteristics by UUID. More... | |
bStatus_t | GATT_DiscPrimaryServiceByUUID (uint16 connHandle, uint8 *pUUID, uint8 len, uint8 taskId) |
Discovery Primary Service by UUID. More... | |
bStatus_t | GATT_ExchangeMTU (uint16 connHandle, attExchangeMTUReq_t *pReq, uint8 taskId) |
Exchange MTU Request. More... | |
bStatus_t | GATT_ExecuteWriteReq (uint16 connHandle, attExecuteWriteReq_t *pReq, uint8 taskId) |
ATT_ExecuteWriteReq More... | |
gattAttribute_t * | GATT_FindHandle (uint16 handle, uint16 *pHandle) |
Find the attribute record for a given handle. More... | |
gattAttribute_t * | GATT_FindHandleUUID (uint16 startHandle, uint16 endHandle, const uint8 *pUUID, uint16 len, uint16 *pHandle) |
Find the attribute record for a given handle and UUID. More... | |
bStatus_t | GATT_FindIncludedServices (uint16 connHandle, uint16 startHandle, uint16 endHandle, uint8 taskId) |
This sub-procedure is used by a client to find include service declarations within a service definition on a server. The service specified is identified by the service handle range. More... | |
gattAttribute_t * | GATT_FindNextAttr (gattAttribute_t *pAttr, uint16 endHandle, uint16 service, uint16 *pLastHandle) |
Find the next attribute of the same type for a given attribute. More... | |
bStatus_t | GATT_Indication (uint16 connHandle, attHandleValueInd_t *pInd, uint8 authenticated, uint8 taskId) |
Send a GATT Indication. More... | |
bStatus_t | GATT_InitClient (void) |
Initialize the Generic Attribute Profile Client. More... | |
bStatus_t | GATT_InitServer (void) |
Initialize the Generic Attribute Profile Server. More... | |
bStatus_t | GATT_Notification (uint16 connHandle, attHandleValueNoti_t *pNoti, uint8 authenticated) |
Send a GATT Notification. More... | |
bStatus_t | GATT_NotifyEvent (uint16 connHandle, uint8 status, uint8 method, gattMsg_t *pMsg) |
Send an event to upper layer application/protocol. More... | |
bStatus_t | GATT_PrepareWriteReq (uint16 connHandle, attPrepareWriteReq_t *pReq, uint8 taskId) |
Request the server to prepare to write the value of an attribute. More... | |
bStatus_t | GATT_ReadCharDesc (uint16 connHandle, attReadReq_t *pReq, uint8 taskId) |
Read Characteristic Descriptor. More... | |
bStatus_t | GATT_ReadCharValue (uint16 connHandle, attReadReq_t *pReq, uint8 taskId) |
Read Characteristic Value. More... | |
bStatus_t | GATT_ReadLongCharDesc (uint16 connHandle, attReadBlobReq_t *pReq, uint8 taskId) |
Read Long Characteristic Descriptor. More... | |
bStatus_t | GATT_ReadLongCharValue (uint16 connHandle, attReadBlobReq_t *pReq, uint8 taskId) |
Read Long Characteristic Value. More... | |
bStatus_t | GATT_ReadMultiCharValues (uint16 connHandle, attReadMultiReq_t *pReq, uint8 taskId) |
Read Multiple Characteristic Values. More... | |
bStatus_t | GATT_ReadUsingCharUUID (uint16 connHandle, attReadByTypeReq_t *pReq, uint8 taskId) |
Read Using Characteristic UUID. More... | |
void | GATT_RegisterForInd (uint8 taskId) |
Register to receive incoming ATT Indications or Notifications of attribute values. More... | |
void | GATT_RegisterForMsgs (uint8 taskID) |
GATT Register for Messages. More... | |
void | GATT_RegisterForReq (uint8 taskId) |
Register to receive incoming ATT Requests. More... | |
bStatus_t | GATT_RegisterService (gattService_t *pService) |
Register a service attribute list with the GATT Server. More... | |
bStatus_t | GATT_ReliableWrites (uint16 connHandle, attPrepareWriteReq_t *pReqs, uint8 numReqs, uint8 flags, uint8 taskId) |
Do a Reliable Write. More... | |
bStatus_t | GATT_SendRsp (uint16 connHandle, uint8 method, gattMsg_t *pRsp) |
Send an ATT Response message out. More... | |
uint8 | GATT_ServiceChangedInd (uint16 connHandle, uint8 taskId) |
Send out a Service Changed Indication. More... | |
uint8 | GATT_ServiceEncKeySize (uint16 handle) |
Get the minimum encryption key size required by a given service. More... | |
uint16 | GATT_ServiceNumAttrs (uint16 handle) |
Get the number of attributes for a given service. More... | |
bStatus_t | GATT_SignedWriteNoRsp (uint16 connHandle, attWriteReq_t *pReq) |
Signed Write No Response. More... | |
bStatus_t | GATT_UpdateMTU (uint16 connHandle, uint16 mtuSize) |
bStatus_t | GATT_VerifyReadPermissions (uint16 connHandle, gattAttribute_t *pAttr, uint16 service) |
Verify the permissions of an attribute for reading. More... | |
bStatus_t | GATT_VerifyWritePermissions (uint16 connHandle, gattAttribute_t *pAttr, uint16 service, attWriteReq_t *pReq) |
Verify the permissions of an attribute for writing. More... | |
bStatus_t | GATT_WriteCharDesc (uint16 connHandle, attWriteReq_t *pReq, uint8 taskId) |
Write Characteristic Descriptor. More... | |
bStatus_t | GATT_WriteCharValue (uint16 connHandle, attWriteReq_t *pReq, uint8 taskId) |
Write Characteristic Value. More... | |
bStatus_t | GATT_WriteLongCharDesc (uint16 connHandle, attPrepareWriteReq_t *pReq, uint8 taskId) |
Write Long Characteristic Descriptor. More... | |
bStatus_t | GATT_WriteLongCharValue (uint16 connHandle, attPrepareWriteReq_t *pReq, uint8 taskId) |
Write Long Characteristic Value. More... | |
bStatus_t | GATT_WriteNoRsp (uint16 connHandle, attWriteReq_t *pReq) |
Write No Response. More... | |
This module implements the Attribute Protocol and Generic Attribute Protocol.
void* GATT_bm_alloc | ( | uint16 | connHandle, |
uint8 | opcode, | ||
uint16 | size, | ||
uint16 * | pSizeAlloc | ||
) |
GATT implementation of the allocator functionality.
connHandle | - connection that message is to be sent on. |
opcode | - opcode of message that buffer to be allocated for. |
size | - number of bytes to allocate from the heap. |
pSizeAlloc | - number of bytes allocated for the caller from the heap. |
void GATT_bm_free | ( | gattMsg_t * | pMsg, |
uint8 | opcode | ||
) |
GATT implementation of the de-allocator functionality.
pMsg | - pointer to GATT message containing the memory to free. |
opcode | - opcode of the message |
bStatus_t GATT_DeregisterService | ( | uint16 | handle, |
gattService_t * | pService | ||
) |
Deregister a service attribute list with the GATT Server.
handle | - handle of service to be deregistered |
pService | - pointer to deregistered service (to be returned) |
bStatus_t GATT_DiscAllCharDescs | ( | uint16 | connHandle, |
uint16 | startHandle, | ||
uint16 | endHandle, | ||
uint8 | taskId | ||
) |
Discovery All Characteristic Descriptors.
This sub-procedure is used by a client to find all the characteristic descriptor's Attribute Handles and Attribute Types within a characteristic definition when only the characteristic handle range is known. The characteristic specified is identified by the characteristic handle range.
ATT_FindInfoReq is used with the Starting Handle set to starting handle of the specified characteristic and the Ending Handle set to the ending handle of the specified characteristic. The UUID Filter parameter is NULL (zero length).
connHandle | - connection to use |
startHandle | - starting handle |
endHandle | - end handle |
taskId | - task to be notified of response |
bStatus_t GATT_DiscAllChars | ( | uint16 | connHandle, |
uint16 | startHandle, | ||
uint16 | endHandle, | ||
uint8 | taskId | ||
) |
Discover all Characteristics.
This sub-procedure is used by a client to find all the characteristic declarations within a service definition on a server when only the service handle range is known. The service specified is identified by the service handle range.
ATT_ReadByTypeReq is used with the Attribute Type parameter set to the UUID for "Characteristic". The Starting Handle is set to starting handle of the specified service and the Ending Handle is set to the ending handle of the specified service.
connHandle | - connection to use |
startHandle | - starting handle |
endHandle | - end handle |
taskId | - task to be notified of response |
bStatus_t GATT_DiscAllPrimaryServices | ( | uint16 | connHandle, |
uint8 | taskId | ||
) |
Discovery All Primary Services.
This sub-procedure is used by a client to discover all the primary services on a server.
ATT_ReadByGrpTypeReq is used with the Attribute Type parameter set to the UUID for "Primary Service". The Starting Handle is set to 0x0001 and the Ending Handle is set to 0xFFFF.
connHandle | - connection to use |
taskId | - task to be notified of response |
bStatus_t GATT_DiscCharsByUUID | ( | uint16 | connHandle, |
attReadByTypeReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Discovery Characteristics by UUID.
This sub-procedure is used by a client to discover service characteristics on a server when only the service handle ranges are known and the characteristic UUID is known. The specific service may exist multiple times on a server. The characteristic being discovered is identified by the characteristic UUID.
ATT_ReadByTypeReq is used with the Attribute Type is set to the UUID for "Characteristic" and the Starting Handle and Ending Handle parameters is set to the service handle range.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_DiscPrimaryServiceByUUID | ( | uint16 | connHandle, |
uint8 * | pUUID, | ||
uint8 | len, | ||
uint8 | taskId | ||
) |
Discovery Primary Service by UUID.
This sub-procedure is used by a client to discover a specific primary service on a server when only the Service UUID is known. The primary specific service may exist multiple times on a server. The primary service being discovered is identified by the service UUID.
ATT_FindByTypeValueReq is used with the Attribute Type parameter set to the UUID for "Primary Service" and the Attribute Value set to the 16-bit Bluetooth UUID or 128-bit UUID for the specific primary service. The Starting Handle shall be set to 0x0001 and the Ending Handle shall be set to 0xFFFF.
connHandle | - connection to use |
pUUID | - pointer to service UUID to look for |
len | - length of value |
taskId | - task to be notified of response |
bStatus_t GATT_ExchangeMTU | ( | uint16 | connHandle, |
attExchangeMTUReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Exchange MTU Request.
This sub-procedure is used by the client to set the ATT_MTU to the maximum possible value that can be supported by both devices when the client supports a value greater than the default ATT_MTU for the Attribute Protocol. This sub-procedure shall only be initiated once during a connection.
ATT_ExchangeMTUReq is used by this sub-procedure.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_ExecuteWriteReq | ( | uint16 | connHandle, |
attExecuteWriteReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Request the server to write or cancel the write of all the prepared values currently held in the prepare queue from this client.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
gattAttribute_t* GATT_FindHandle | ( | uint16 | handle, |
uint16 * | pHandle | ||
) |
Find the attribute record for a given handle.
handle | - handle to look for |
pHandle | - handle of owner of attribute (to be returned) |
gattAttribute_t* GATT_FindHandleUUID | ( | uint16 | startHandle, |
uint16 | endHandle, | ||
const uint8 * | pUUID, | ||
uint16 | len, | ||
uint16 * | pHandle | ||
) |
Find the attribute record for a given handle and UUID.
startHandle | - first handle to look for |
endHandle | - last handle to look for |
pUUID | - pointer to UUID to look for |
len | - length of UUID |
pHandle | - handle of owner of attribute (to be returned) |
bStatus_t GATT_FindIncludedServices | ( | uint16 | connHandle, |
uint16 | startHandle, | ||
uint16 | endHandle, | ||
uint8 | taskId | ||
) |
This sub-procedure is used by a client to find include service declarations within a service definition on a server. The service specified is identified by the service handle range.
ATT_ReadByTypeReq is used with the Attribute Type parameter set to the UUID for "Included Service". The Starting Handle is set to starting handle of the specified service and the Ending Handle is set to the ending handle of the specified service.
connHandle | - connection to use |
startHandle | - starting handle |
endHandle | - end handle |
taskId | - task to be notified of response |
gattAttribute_t* GATT_FindNextAttr | ( | gattAttribute_t * | pAttr, |
uint16 | endHandle, | ||
uint16 | service, | ||
uint16 * | pLastHandle | ||
) |
Find the next attribute of the same type for a given attribute.
pAttr | - pointer to attribute to find a next for |
endHandle | - last handle to look for |
service | - handle of owner service |
pLastHandle | - handle of last attribute (to be returned) |
bStatus_t GATT_Indication | ( | uint16 | connHandle, |
attHandleValueInd_t * | pInd, | ||
uint8 | authenticated, | ||
uint8 | taskId | ||
) |
Send a GATT Indication.
This sub-procedure is used when a server is configured to indicate a characteristic value to a client and expects an attribute protocol layer acknowledgement that the indication was successfully received.
ATT_HandleValueInd is used in this sub-procedure.
connHandle | - connection to use |
pInd | - pointer to indication to be sent |
authenticated | - whether an authenticated link is required 0x01: LE Legacy authenticated 0x02: Secure Connections authenticated |
taskId | - task to be notified of response |
bStatus_t GATT_InitClient | ( | void | ) |
Initialize the Generic Attribute Profile Client.
bStatus_t GATT_InitServer | ( | void | ) |
Initialize the Generic Attribute Profile Server.
bStatus_t GATT_Notification | ( | uint16 | connHandle, |
attHandleValueNoti_t * | pNoti, | ||
uint8 | authenticated | ||
) |
Send a GATT Notification.
This sub-procedure is used when a server is configured to notify a characteristic value to a client without expecting any attribute protocol layer acknowledgement that the notification was successfully received.
ATT_HandleValueNoti is used in this sub-procedure.
connHandle | - connection to use |
pNoti | - pointer to notification to be sent |
authenticated | - whether an authenticated link is required 0x01: LE Legacy authenticated 0x02: Secure Connections authenticated |
Send an event to upper layer application/protocol.
connHandle | - connection event belongs to |
status | - status |
method | - type of message |
pMsg | - pointer to message to be sent |
bStatus_t GATT_PrepareWriteReq | ( | uint16 | connHandle, |
attPrepareWriteReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Request the server to prepare to write the value of an attribute.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_ReadCharDesc | ( | uint16 | connHandle, |
attReadReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Read Characteristic Descriptor.
This sub-procedure is used to read a characteristic descriptor from a server when the client knows the characteristic descriptor declaration's Attribute handle.
ATT_ReadReq is used for this sub-procedure. with the Attribute Handle parameter set to the characteristic descriptor handle.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_ReadCharValue | ( | uint16 | connHandle, |
attReadReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Read Characteristic Value.
This sub-procedure is used to read a Characteristic Value from a server when the client knows the Characteristic Value Handle.
ATT_ReadReq is used with the Attribute Handle parameter set to the Characteristic Value Handle. The Read Response returns the Characteristic Value in the Attribute Value parameter.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_ReadLongCharDesc | ( | uint16 | connHandle, |
attReadBlobReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Read Long Characteristic Descriptor.
This sub-procedure is used to read a characteristic descriptor from a server when the client knows the characteristic descriptor declaration's Attribute handle and the length of the characteristic descriptor declaration is longer than can be sent in a single Read Response attribute protocol message.
ATT_ReadBlobReq is used to perform this sub-procedure. The Attribute Handle parameter shall be set to the characteristic descriptor handle. The Value Offset parameter shall be the offset within the characteristic descriptor to be read.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_ReadLongCharValue | ( | uint16 | connHandle, |
attReadBlobReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Read Long Characteristic Value.
This sub-procedure is used to read a Characteristic Value from a server when the client knows the Characteristic Value Handle and the length of the Characteristic Value is longer than can be sent in a single Read Response Attribute Protocol message.
ATT_ReadBlobReq is used in this sub-procedure.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_ReadMultiCharValues | ( | uint16 | connHandle, |
attReadMultiReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Read Multiple Characteristic Values.
This sub-procedure is used to read multiple Characteristic Values from a server when the client knows the Characteristic Value Handles. The Attribute Protocol Read Multiple Requests is used with the Set Of Handles parameter set to the Characteristic Value Handles. The Read Multiple Response returns the Characteristic Values in the Set Of Values parameter.
ATT_ReadMultiReq is used in this sub-procedure.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_ReadUsingCharUUID | ( | uint16 | connHandle, |
attReadByTypeReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Read Using Characteristic UUID.
This sub-procedure is used to read a Characteristic Value from a server when the client only knows the characteristic UUID and does not know the handle of the characteristic.
ATT_ReadByTypeReq is used to perform the sub-procedure. The Attribute Type is set to the known characteristic UUID and the Starting Handle and Ending Handle parameters shall be set to the range over which this read is to be performed. This is typically the handle range for the service in which the characteristic belongs.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
void GATT_RegisterForInd | ( | uint8 | taskId | ) |
Register to receive incoming ATT Indications or Notifications of attribute values.
taskId | - task to forward indications or notifications to |
void GATT_RegisterForMsgs | ( | uint8 | taskID | ) |
GATT Register for Messages.
Register your task ID to receive GATT local events and ATT Response messages pending for transmission. When the GATT Server fails to respond to an incoming ATT Request due to lack of HCI Tx buffers, the response will be forwarded the app for retransmission.
Note: A pending ATT Response message forwarded to the app should be transmitted using GATT_SendRsp(), or its payload freed using GATT_bm_free() if not transmitted.
taskID | - Default task ID to send GATT events/pending ATT responses. |
void GATT_RegisterForReq | ( | uint8 | taskId | ) |
Register to receive incoming ATT Requests.
taskId | - task to forward requests to |
bStatus_t GATT_RegisterService | ( | gattService_t * | pService | ) |
Register a service attribute list with the GATT Server.
A service is composed of characteristics or references to other services. Each characteristic contains a value and may contain optional information about the value. There are two types of services: primary service and secondary service.
A service definition begins with a service declaration and ends before the next service declaration or the maximum Attribute Handle.
A characteristic definition begins with a characteristic declaration and ends before the next characteristic or service declaration or maximum Attribute Handle.
The attribute server will only keep a pointer to the attribute list, so the calling application will have to maintain the code and RAM associated with this list.
pService | - pointer to service attribute list to be registered |
bStatus_t GATT_ReliableWrites | ( | uint16 | connHandle, |
attPrepareWriteReq_t * | pReqs, | ||
uint8 | numReqs, | ||
uint8 | flags, | ||
uint8 | taskId | ||
) |
Do a Reliable Write.
This sub-procedure is used to write a Characteristic Value to a server when the client knows the Characteristic Value Handle, and assurance is required that the correct Characteristic Value is going to be written by transferring the Characteristic Value to be written in both directions before the write is performed. This sub-procedure can also be used when multiple values must be written, in order, in a single operation.
The sub-procedure has two phases, the first phase prepares the characteristic values to be written. Once this is complete, the second phase performs the execution of all of the prepared characteristic value writes on the server from this client. In the first phase, ATT_PrepareWriteReq is used. In the second phase, ATT_ExecuteWriteReq is used.
connHandle | - connection to use |
pReqs | - pointer to requests to be sent (must be allocated) |
numReqs | - number of requests in pReq |
flags | - ATT_ExecuteWriteReq flags |
taskId | - task to be notified of response |
Send an ATT Response message out.
connHandle | - connection to use |
method | - type of response message |
pRsp | - pointer to ATT response to be sent |
uint8 GATT_ServiceChangedInd | ( | uint16 | connHandle, |
uint8 | taskId | ||
) |
Send out a Service Changed Indication.
connHandle | - connection to use |
taskId | - task to be notified of confirmation |
uint8 GATT_ServiceEncKeySize | ( | uint16 | handle | ) |
Get the minimum encryption key size required by a given service.
handle | - service handle to look for |
uint16 GATT_ServiceNumAttrs | ( | uint16 | handle | ) |
Get the number of attributes for a given service.
handle | - service handle to look for |
bStatus_t GATT_SignedWriteNoRsp | ( | uint16 | connHandle, |
attWriteReq_t * | pReq | ||
) |
Signed Write No Response.
This sub-procedure is used to write a Characteristic Value to a server when the client knows the Characteristic Value Handle and the ATT Bearer is not encrypted. This sub-procedure shall only be used if the Characteristic Properties authenticated bit is enabled and the client and server device share a bond as defined in the GAP.
This sub-procedure only writes the first (ATT_MTU - 15) octets of an Attribute Value. This sub-procedure cannot be used to write a long Attribute.
ATT_WriteReq is used for this sub-procedure. The Attribute Handle parameter shall be set to the Characteristic Value Handle. The Attribute Value parameter shall be set to the new Characteristic Value authenticated by signing the value, as defined in the Security Manager.
connHandle | - connection to use |
pReq | - pointer to command to be sent |
bStatus_t GATT_UpdateMTU | ( | uint16 | connHandle, |
uint16 | mtuSize | ||
) |
Notify the stack of an updated MTU size for a given connection.
connHandle | - connection handle. |
mtuSize | - new MTU size. |
bStatus_t GATT_VerifyReadPermissions | ( | uint16 | connHandle, |
gattAttribute_t * | pAttr, | ||
uint16 | service | ||
) |
Verify the permissions of an attribute for reading.
connHandle | - connection to use |
pAttr | - pointer to attribute |
service | - service handle |
bStatus_t GATT_VerifyWritePermissions | ( | uint16 | connHandle, |
gattAttribute_t * | pAttr, | ||
uint16 | service, | ||
attWriteReq_t * | pReq | ||
) |
Verify the permissions of an attribute for writing.
connHandle | - connection to use |
pAttr | - pointer to attribute |
service | - service handle |
pReq | - pointer to write request |
bStatus_t GATT_WriteCharDesc | ( | uint16 | connHandle, |
attWriteReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Write Characteristic Descriptor.
This sub-procedure is used to write a characteristic descriptor value to a server when the client knows the characteristic descriptor handle.
ATT_WriteReq is used for this sub-procedure. The Attribute Handle parameter shall be set to the characteristic descriptor handle. The Attribute Value parameter shall be set to the new characteristic descriptor value.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_WriteCharValue | ( | uint16 | connHandle, |
attWriteReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Write Characteristic Value.
This sub-procedure is used to write a characteristic value to a server when the client knows the characteristic value handle. This sub-procedure only writes the first (ATT_MTU-3) octets of a characteristic value. This sub-procedure can not be used to write a long attribute; instead the Write Long Characteristic Values sub-procedure should be used.
ATT_WriteReq is used in this sub-procedure. The Attribute Handle parameter shall be set to the Characteristic Value Handle. The Attribute Value parameter shall be set to the new characteristic.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_WriteLongCharDesc | ( | uint16 | connHandle, |
attPrepareWriteReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Write Long Characteristic Descriptor.
This sub-procedure is used to write a Characteristic Value to a server when the client knows the Characteristic Value Handle but the length of the Characteristic Value is longer than can be sent in a single Write Request Attribute Protocol message.
ATT_PrepareWriteReq and ATT_ExecuteWriteReq are used to perform this sub-procedure.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_WriteLongCharValue | ( | uint16 | connHandle, |
attPrepareWriteReq_t * | pReq, | ||
uint8 | taskId | ||
) |
Write Long Characteristic Value.
This sub-procedure is used to write a Characteristic Value to a server when the client knows the Characteristic Value Handle but the length of the Characteristic Value is longer than can be sent in a single Write Request Attribute Protocol message.
ATT_PrepareWriteReq and ATT_ExecuteWriteReq are used to perform this sub-procedure.
connHandle | - connection to use |
pReq | - pointer to request to be sent |
taskId | - task to be notified of response |
bStatus_t GATT_WriteNoRsp | ( | uint16 | connHandle, |
attWriteReq_t * | pReq | ||
) |
Write No Response.
This sub-procedure is used to write a Characteristic Value to a server when the client knows the Characteristic Value Handle and the client does not need an acknowledgement that the write was successfully performed. This sub-procedure only writes the first (ATT_MTU - 3) octets of a Characteristic Value. This sub-procedure can not be used to write a long characteristic; instead the Write Long Characteristic Values sub-procedure should be used.
ATT_WriteReq is used for this sub-procedure. The Attribute Handle parameter shall be set to the Characteristic Value Handle. The Attribute Value parameter shall be set to the new Characteristic Value.
connHandle | - connection to use |
pReq | - pointer to command to be sent |