Data Fields
RF_AccessParams Struct Reference

RF request access parameter struct. More...

#include <RF.h>

Data Fields

uint32_t duration
 Radio access duration in RAT Ticks requested by the client. More...
 
uint32_t startTime
 Start time window in RAT Time for radio access. More...
 
RF_Priority priority
 Access priority. More...
 

Detailed Description

RF request access parameter struct.

RF request access command parameters are used with the RF_requestAccess() call.

Field Documentation

§ duration

uint32_t RF_AccessParams::duration

Radio access duration in RAT Ticks requested by the client.

§ startTime

uint32_t RF_AccessParams::startTime

Start time window in RAT Time for radio access.

§ priority

RF_Priority RF_AccessParams::priority

Access priority.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale