CTR Parameters. More...
#include <AESCTR.h>
Data Fields | |
AESCTR_ReturnBehavior | returnBehavior |
AESCTR_CallbackFxn | callbackFxn |
uint32_t | timeout |
void * | custom |
CTR Parameters.
CTR Parameters are used to with the AESCTR_open() call. Default values for these parameters are set using AESCTR_Params_init().
AESCTR_ReturnBehavior AESCTR_Params::returnBehavior |
Blocking, callback, or polling return behavior
AESCTR_CallbackFxn AESCTR_Params::callbackFxn |
Callback function pointer
uint32_t AESCTR_Params::timeout |
Timeout before the driver returns an error in AESCTR_RETURN_BEHAVIOR_BLOCKING
void* AESCTR_Params::custom |
Custom argument used by driver implementation