#include <rf_ble_cmd.h>
Data Fields | |
uint16_t | nRxOk |
Number of packets received with CRC OK. More... | |
uint16_t | nRxNok |
Number of packets received with CRC error. More... | |
uint16_t | nRxBufFull |
Number of packets that have been received and discarded due to lack of buffer space. More... | |
int8_t | lastRssi |
The RSSI of the last received packet. More... | |
uint8_t | __dummy0 |
ratmr_t | timeStamp |
Time stamp of the last received packet. More... | |
uint8_t rfc_bleGenericRxOutput_s::__dummy0 |
int8_t rfc_bleGenericRxOutput_s::lastRssi |
The RSSI of the last received packet.
uint16_t rfc_bleGenericRxOutput_s::nRxBufFull |
Number of packets that have been received and discarded due to lack of buffer space.
uint16_t rfc_bleGenericRxOutput_s::nRxNok |
Number of packets received with CRC error.
uint16_t rfc_bleGenericRxOutput_s::nRxOk |
Number of packets received with CRC OK.
ratmr_t rfc_bleGenericRxOutput_s::timeStamp |
Time stamp of the last received packet.