Proprietary Mode Receive Command with Sniff Mode. More...
#include <rf_prop_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x3808. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t bRepeatOk:1 | |
0: End operation after receiving a packet correctly 1: Go back to sync search after receiving a packet correctly More... | |
uint8_t bRepeatNok:1 | |
0: End operation after receiving a packet with CRC error 1: Go back to sync search after receiving a packet with CRC error More... | |
uint8_t bUseCrc:1 | |
0: Do not check CRC 1: Check CRC More... | |
uint8_t bVarLen:1 | |
0: Fixed length 1: Receive length as first byte More... | |
uint8_t bChkAddress:1 | |
0: No address check 1: Check address More... | |
uint8_t endType:1 | |
0: Packet is received to the end if end trigger happens after sync is obtained 1: Packet reception is stopped if end trigger happens More... | |
uint8_t filterOp:1 | |
0: Stop receiver and restart sync search on address mismatch 1: Receive packet and mark it as ignored on address mismatch More... | |
} | pktConf |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically discard ignored packets from RX queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically discard packets with CRC error from RX queue. More... | |
uint8_t __pad0__:1 | |
uint8_t bIncludeHdr:1 | |
If 1, include the received header or length byte in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the RX queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the RX queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status byte to the packet in the RX queue. More... | |
} | rxConf |
RX configuration. More... | |
uint32_t | syncWord |
Sync word to listen for. More... | |
uint8_t | maxPktLen |
Packet length for fixed length, maximum packet length for variable length 0: Unlimited or unknown length. More... | |
uint8_t | address0 |
Address. More... | |
uint8_t | address1 |
Address (set equal to address0 to accept only one address. If 0xFF, accept 0x00 as well) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger classifier for ending the operation. More... | |
ratmr_t | endTime |
Time used together with endTrigger for ending the operation. More... | |
dataQueue_t * | pQueue |
Pointer to receive queue. More... | |
uint8_t * | pOutput |
Pointer to output structure. More... | |
struct { | |
uint8_t bEnaRssi:1 | |
If 1, enable RSSI as a criterion. More... | |
uint8_t bEnaCorr:1 | |
If 1, enable correlation as a criterion. More... | |
uint8_t operation:1 | |
0: Busy if either RSSI or correlation indicates Busy 1: Busy if both RSSI and correlation indicates Busy More... | |
uint8_t busyOp:1 | |
0: Continue carrier sense on channel Busy 1: End carrier sense on channel Busy For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle More... | |
uint8_t idleOp:1 | |
0: Continue on channel Idle 1: End on channel Idle More... | |
uint8_t timeoutRes:1 | |
0: Timeout with channel state Invalid treated as Busy 1: Timeout with channel state Invalid treated as Idle More... | |
} | csConf |
int8_t | rssiThr |
RSSI threshold. More... | |
uint8_t | numRssiIdle |
Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle. More... | |
uint8_t | numRssiBusy |
Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy. More... | |
uint16_t | corrPeriod |
Number of RAT ticks for a correlation observation periods. More... | |
struct { | |
uint8_t numCorrInv:4 | |
Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Idle to Invalid. More... | |
uint8_t numCorrBusy:4 | |
Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Invalid to Busy. More... | |
} | corrConfig |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | csEndTrigger |
Trigger classifier for ending the carrier sense. More... | |
ratmr_t | csEndTime |
Time used together with csEndTrigger for ending the operation. More... | |
Proprietary Mode Receive Command with Sniff Mode.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::__pad0__ |
uint8_t rfc_CMD_PROP_RX_SNIFF_s::address0 |
Address.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::address1 |
Address (set equal to address0
to accept only one address. If 0xFF, accept 0x00 as well)
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the RX queue.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAppendStatus |
If 1, append a status byte to the packet in the RX queue.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the RX queue.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAutoFlushCrcErr |
If 1, automatically discard packets with CRC error from RX queue.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAutoFlushIgnored |
If 1, automatically discard ignored packets from RX queue.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bChkAddress |
0: No address check
1: Check address
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bEnaCorr |
If 1, enable correlation as a criterion.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bEnaRssi |
If 1, enable RSSI as a criterion.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bIncludeHdr |
If 1, include the received header or length byte in the stored packet; otherwise discard it.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bRepeatNok |
0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bRepeatOk |
0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bUseCrc |
0: Do not check CRC
1: Check CRC
uint8_t rfc_CMD_PROP_RX_SNIFF_s::busyOp |
0: Continue carrier sense on channel Busy
1: End carrier sense on channel Busy
For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle
uint8_t rfc_CMD_PROP_RX_SNIFF_s::bVarLen |
0: Fixed length
1: Receive length as first byte
uint16_t rfc_CMD_PROP_RX_SNIFF_s::commandNo |
The command ID number 0x3808.
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::condition |
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::corrConfig |
uint16_t rfc_CMD_PROP_RX_SNIFF_s::corrPeriod |
Number of RAT ticks for a correlation observation periods.
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::csConf |
ratmr_t rfc_CMD_PROP_RX_SNIFF_s::csEndTime |
Time used together with csEndTrigger
for ending the operation.
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::csEndTrigger |
Trigger classifier for ending the carrier sense.
ratmr_t rfc_CMD_PROP_RX_SNIFF_s::endTime |
Time used together with endTrigger
for ending the operation.
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::endTrigger |
Trigger classifier for ending the operation.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::endType |
0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens
uint8_t rfc_CMD_PROP_RX_SNIFF_s::filterOp |
0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch
uint8_t rfc_CMD_PROP_RX_SNIFF_s::idleOp |
0: Continue on channel Idle
1: End on channel Idle
uint8_t rfc_CMD_PROP_RX_SNIFF_s::maxPktLen |
Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
uint8_t rfc_CMD_PROP_RX_SNIFF_s::numCorrBusy |
Number of subsequent correlation tops with maximum corrPeriod
RAT ticks between them needed to go from Invalid to Busy.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::numCorrInv |
Number of subsequent correlation tops with maximum corrPeriod
RAT ticks between them needed to go from Idle to Invalid.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::numRssiBusy |
Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::numRssiIdle |
Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::operation |
0: Busy if either RSSI or correlation indicates Busy
1: Busy if both RSSI and correlation indicates Busy
uint8_t rfc_CMD_PROP_RX_SNIFF_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::pktConf |
rfc_radioOp_t* rfc_CMD_PROP_RX_SNIFF_s::pNextOp |
Pointer to the next operation to run after this operation is done.
uint8_t* rfc_CMD_PROP_RX_SNIFF_s::pOutput |
Pointer to output structure.
dataQueue_t* rfc_CMD_PROP_RX_SNIFF_s::pQueue |
Pointer to receive queue.
int8_t rfc_CMD_PROP_RX_SNIFF_s::rssiThr |
RSSI threshold.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::rule |
Condition for running next command: Rule for how to proceed.
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::rxConf |
RX configuration.
ratmr_t rfc_CMD_PROP_RX_SNIFF_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_PROP_RX_SNIFF_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
uint32_t rfc_CMD_PROP_RX_SNIFF_s::syncWord |
Sync word to listen for.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::timeoutRes |
0: Timeout with channel state Invalid treated as Busy
1: Timeout with channel state Invalid treated as Idle
uint8_t rfc_CMD_PROP_RX_SNIFF_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_PROP_RX_SNIFF_s::triggerType |
The type of trigger.