Carrier Sense Command. More...
#include <rf_prop_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x3805. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bFsOffIdle:1 | |
0: Keep synth running if command ends with channel Idle 1: Turn off synth if command ends with channel Idle More... | |
uint8_t bFsOffBusy:1 | |
0: Keep synth running if command ends with channel Busy 1: Turn off synth if command ends with channel Busy More... | |
} | csFsConf |
uint8_t | __dummy0 |
struct { | |
uint8_t bEnaRssi:1 | |
If 1, enable RSSI as a criterion. More... | |
uint8_t bEnaCorr:1 | |
If 1, enable correlation as a criterion. More... | |
uint8_t operation:1 | |
0: Busy if either RSSI or correlation indicates Busy 1: Busy if both RSSI and correlation indicates Busy More... | |
uint8_t busyOp:1 | |
0: Continue carrier sense on channel Busy 1: End carrier sense on channel Busy For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle More... | |
uint8_t idleOp:1 | |
0: Continue on channel Idle 1: End on channel Idle More... | |
uint8_t timeoutRes:1 | |
0: Timeout with channel state Invalid treated as Busy 1: Timeout with channel state Invalid treated as Idle More... | |
} | csConf |
int8_t | rssiThr |
RSSI threshold. More... | |
uint8_t | numRssiIdle |
Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle. More... | |
uint8_t | numRssiBusy |
Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy. More... | |
uint16_t | corrPeriod |
Number of RAT ticks for a correlation observation periods. More... | |
struct { | |
uint8_t numCorrInv:4 | |
Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Idle to Invalid. More... | |
uint8_t numCorrBusy:4 | |
Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Invalid to Busy. More... | |
} | corrConfig |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | csEndTrigger |
Trigger classifier for ending the carrier sense. More... | |
ratmr_t | csEndTime |
Time used together with csEndTrigger for ending the operation. More... | |
Carrier Sense Command.
uint8_t rfc_CMD_PROP_CS_s::__dummy0 |
uint8_t rfc_CMD_PROP_CS_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_PROP_CS_s::bEnaCorr |
If 1, enable correlation as a criterion.
uint8_t rfc_CMD_PROP_CS_s::bEnaRssi |
If 1, enable RSSI as a criterion.
uint8_t rfc_CMD_PROP_CS_s::bFsOffBusy |
0: Keep synth running if command ends with channel Busy
1: Turn off synth if command ends with channel Busy
uint8_t rfc_CMD_PROP_CS_s::bFsOffIdle |
0: Keep synth running if command ends with channel Idle
1: Turn off synth if command ends with channel Idle
uint8_t rfc_CMD_PROP_CS_s::busyOp |
0: Continue carrier sense on channel Busy
1: End carrier sense on channel Busy
For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle
uint16_t rfc_CMD_PROP_CS_s::commandNo |
The command ID number 0x3805.
struct { ... } rfc_CMD_PROP_CS_s::condition |
struct { ... } rfc_CMD_PROP_CS_s::corrConfig |
uint16_t rfc_CMD_PROP_CS_s::corrPeriod |
Number of RAT ticks for a correlation observation periods.
struct { ... } rfc_CMD_PROP_CS_s::csConf |
ratmr_t rfc_CMD_PROP_CS_s::csEndTime |
Time used together with csEndTrigger
for ending the operation.
struct { ... } rfc_CMD_PROP_CS_s::csEndTrigger |
Trigger classifier for ending the carrier sense.
struct { ... } rfc_CMD_PROP_CS_s::csFsConf |
uint8_t rfc_CMD_PROP_CS_s::idleOp |
0: Continue on channel Idle
1: End on channel Idle
uint8_t rfc_CMD_PROP_CS_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
uint8_t rfc_CMD_PROP_CS_s::numCorrBusy |
Number of subsequent correlation tops with maximum corrPeriod
RAT ticks between them needed to go from Invalid to Busy.
uint8_t rfc_CMD_PROP_CS_s::numCorrInv |
Number of subsequent correlation tops with maximum corrPeriod
RAT ticks between them needed to go from Idle to Invalid.
uint8_t rfc_CMD_PROP_CS_s::numRssiBusy |
Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy.
uint8_t rfc_CMD_PROP_CS_s::numRssiIdle |
Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle.
uint8_t rfc_CMD_PROP_CS_s::operation |
0: Busy if either RSSI or correlation indicates Busy
1: Busy if both RSSI and correlation indicates Busy
uint8_t rfc_CMD_PROP_CS_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
rfc_radioOp_t* rfc_CMD_PROP_CS_s::pNextOp |
Pointer to the next operation to run after this operation is done.
int8_t rfc_CMD_PROP_CS_s::rssiThr |
RSSI threshold.
uint8_t rfc_CMD_PROP_CS_s::rule |
Condition for running next command: Rule for how to proceed.
ratmr_t rfc_CMD_PROP_CS_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
struct { ... } rfc_CMD_PROP_CS_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_PROP_CS_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
uint8_t rfc_CMD_PROP_CS_s::timeoutRes |
0: Timeout with channel state Invalid treated as Busy
1: Timeout with channel state Invalid treated as Idle
uint8_t rfc_CMD_PROP_CS_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_PROP_CS_s::triggerType |
The type of trigger.