BLE Scanner Command. More...
#include <rf_ble_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x1807. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
uint8_t | channel |
Channel to use 0–39: BLE advertising/data channel number 60–207: Custom frequency; (2300 + channel ) MHz255: Use existing frequency Others: Reserved More... | |
struct { | |
uint8_t init:7 | |
If bOverride = 1 or custom frequency is used:0: Do not use whitening Other value: Initialization for 7-bit LFSR whitener. More... | |
uint8_t bOverride:1 | |
0: Use default whitening for BLE advertising/data channels 1: Override whitening initialization with value of init More... | |
} | whitening |
rfc_bleScannerPar_t * | pParams |
Pointer to command specific parameter structure. More... | |
rfc_bleScannerOutput_t * | pOutput |
Pointer to command specific output structure. More... | |
BLE Scanner Command.
uint8_t rfc_CMD_BLE_SCANNER_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_BLE_SCANNER_s::bOverride |
0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init
uint8_t rfc_CMD_BLE_SCANNER_s::channel |
Channel to use
0–39: BLE advertising/data channel number
60–207: Custom frequency; (2300 + channel
) MHz
255: Use existing frequency
Others: Reserved
uint16_t rfc_CMD_BLE_SCANNER_s::commandNo |
The command ID number 0x1807.
struct { ... } rfc_CMD_BLE_SCANNER_s::condition |
uint8_t rfc_CMD_BLE_SCANNER_s::init |
If bOverride
= 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener.
uint8_t rfc_CMD_BLE_SCANNER_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
uint8_t rfc_CMD_BLE_SCANNER_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
rfc_radioOp_t* rfc_CMD_BLE_SCANNER_s::pNextOp |
Pointer to the next operation to run after this operation is done.
rfc_bleScannerOutput_t* rfc_CMD_BLE_SCANNER_s::pOutput |
Pointer to command specific output structure.
rfc_bleScannerPar_t* rfc_CMD_BLE_SCANNER_s::pParams |
Pointer to command specific parameter structure.
uint8_t rfc_CMD_BLE_SCANNER_s::rule |
Condition for running next command: Rule for how to proceed.
ratmr_t rfc_CMD_BLE_SCANNER_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
struct { ... } rfc_CMD_BLE_SCANNER_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_BLE_SCANNER_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
uint8_t rfc_CMD_BLE_SCANNER_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_BLE_SCANNER_s::triggerType |
The type of trigger.
struct { ... } rfc_CMD_BLE_SCANNER_s::whitening |