TI BLE Stack API Documentation
2.03.08
|
#include <l2cap.h>
Public Attributes | |
uint16 | mtu |
Maximum SDU size that can be received by local device. | |
uint16 | mps |
Maximum payload size that can be received by local device. | |
uint16 | initPeerCredits |
Number of LE-frames that peer device can send. | |
uint16 | peerCreditThreshold |
Low threshold for number of peer credits. | |
uint8 | maxNumChannels |
Maximum number of CO Channels supported by PSM. | |
uint8 | numActiveChannels |
Number of active CO Channels. | |
PSM information format.