|
#define | GAPCENTRALROLE_IRK 0x400 |
| Identity Resolving Key. Read/Write. Size is uint8_t[KEYLEN]. Default is all 0, which means that the IRK will be randomly generated.
|
|
#define | GAPCENTRALROLE_SRK 0x401 |
| Signature Resolving Key. Read/Write. Size is uint8_t[KEYLEN]. Default is all 0, which means that the SRK will be randomly generated.
|
|
#define | GAPCENTRALROLE_SIGNCOUNTER 0x402 |
| Sign Counter. Read/Write. Size is uint32_t. Default is 0.
|
|
#define | GAPCENTRALROLE_BD_ADDR 0x403 |
| Device's Address. Read Only. Size is uint8_t[B_ADDR_LEN]. This item is read from the controller.
|
|
#define | GAPCENTRALROLE_MAX_SCAN_RES 0x404 |
| Maximum number of discover scan results to receive. Default is 0, which means 0 results will be received.
|
|
#define | GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY 0x405 |
| Action taken on Link Param Update Request received. size is uint8_t. Default is GAPCENTRALROLE_PARAM_UPDATE_REQ_AUTO_ACCEPT.
|
|