|
#define | GAPBOND_PAIRING_MODE 0x400 |
| Pairing Mode: GAP Bond Manager Pairing Modes. Read/Write. Size is uint8. Default is GAPBOND_PAIRING_MODE_WAIT_FOR_REQ.
|
|
#define | GAPBOND_INITIATE_WAIT 0x401 |
| Pairing Mode Initiate wait timeout. This is the time it will wait for a Pairing Request before sending the Slave Initiate Request. Read/Write. Size is uint16. Default is 1000(in milliseconds).
|
|
#define | GAPBOND_MITM_PROTECTION 0x402 |
| Man-In-The-Middle (MITM) basically turns on Passkey protection in the pairing algorithm. Read/Write. Size is uint8. Default is 0(disabled).
|
|
#define | GAPBOND_IO_CAPABILITIES 0x403 |
| I/O capabilities. Read/Write. Size is uint8. Default is GAPBOND_IO_CAP_DISPLAY_ONLY GAP Bond Manager I/O Capabilities.
|
|
#define | GAPBOND_OOB_ENABLED 0x404 |
| OOB data available for pairing algorithm. Read/Write. Size is uint8. Default is 0(disabled).
|
|
#define | GAPBOND_OOB_DATA 0x405 |
| OOB Data. Read/Write. size uint8[16]. Default is all 0's.
|
|
#define | GAPBOND_BONDING_ENABLED 0x406 |
| Request Bonding during the pairing process if enabled. Read/Write. Size is uint8. Default is 0(disabled).
|
|
#define | GAPBOND_KEY_DIST_LIST 0x407 |
| The key distribution list for bonding. size is uint8. GAP Bond Manager Key Distribution. Default is sEncKey, sIdKey, mIdKey, mSign enabled.
|
|
#define | GAPBOND_DEFAULT_PASSCODE 0x408 |
| The default passcode for MITM protection. size is uint32. Range is 0 - 999,999. Default is 0.
|
|
#define | GAPBOND_ERASE_ALLBONDS 0x409 |
| Erase all of the bonded devices. Write Only. No Size.
|
|
#define | GAPBOND_AUTO_FAIL_PAIRING 0x40A |
| TEST MODE (DO NOT USE) to automatically send a Pairing Fail when a Pairing Request is received. Read/Write. size is uint8. Default is 0 (disabled).
|
|
#define | GAPBOND_AUTO_FAIL_REASON 0x40B |
| TEST MODE (DO NOT USE) Pairing Fail reason when auto failing. Read/Write. size is uint8. Default is 0x05 (SMP_PAIRING_FAILED_NOT_SUPPORTED).
|
|
#define | GAPBOND_KEYSIZE 0x40C |
| Key Size used in pairing. Read/Write. size is uint8. Default is 16.
|
|
#define | GAPBOND_AUTO_SYNC_WL 0x40D |
| Clears the White List adds to it each unique address stored by bonds in NV. Read/Write. Size is uint8. Default is FALSE.
|
|
#define | GAPBOND_BOND_COUNT 0x40E |
| Gets the total number of bonds stored in NV. Read Only. Size is uint8. Default is 0 (no bonds).
|
|
#define | GAPBOND_BOND_FAIL_ACTION 0x40F |
| Possible actions Central may take upon an unsuccessful bonding. Write Only. Size is uint8. Default is 0x02 (Terminate link upon unsuccessful bonding).
|
|
#define | GAPBOND_ERASE_SINGLEBOND 0x410 |
| Erase a single bonded device. Write only. Must provide address type followed by device address.
|
|
#define | GAPBOND_SECURE_CONNECTION 0x411 |
| Defines Secure Connections usage. Read/Write. size is uint8. Secure Connections only. GAPBOND_SECURE_CONNECTIONS_DEFINES.
|
|
#define | GAPBOND_ECCKEY_REGEN_POLICY 0x412 |
| Count of how many times an ECC keypair may be reused before regeneration. Write only. Range is 0-254. Default is 0. Secure Connections only. GAP Bond Manager ECC Re-use count before regeneration.
|
|
#define | GAPBOND_ECC_KEYS 0x413 |
| Use application requested public-private keypair for Secure Connections. Read/Write. size is gapBondEccKeys_t. Secure Connections only.
|
|
#define | GAPBOND_REMOTE_OOB_SC_ENABLED 0x414 |
| Secure Connections OOB data from remote device availabe. Read/Write. Size is uint8. Default is 0 (disabled). Secure Connections only.
|
|
#define | GAPBOND_REMOTE_OOB_SC_DATA 0x415 |
| Secure Connections OOB data. Read/Write. Size is gapBondOobSC_t. Default is all 0's. Secure Connections only.
|
|
#define | GAPBOND_LOCAL_OOB_SC_ENABLED 0x416 |
| Secure Connection local OOB data is available. Read/Write. Size is uint8. Default is 0 (disabled). Secure Connections only.
|
|
#define | GAPBOND_LOCAL_OOB_SC_DATA 0x417 |
| Local OOB Data. Read/Write. size uint8[16]. Default is all 0's. Secure Connections only.
|
|
#define | GAPBOND_LRU_BOND_REPLACEMENT 0x418 |
| Remote Least Recently Used Bond when newly bonded device is added and the all entries are full. Read/Write. size uint8. Default is FALSE.
|
|