|
#define | GAPROLE_PROFILEROLE 0x300 |
| Reading this parameter will return GAP Role type. Read Only. Size is uint8_t.
|
|
#define | GAPROLE_IRK 0x301 |
| Identity Resolving Key. Read/Write. Size is uint8_t[KEYLEN]. Default is all 0, which means that the IRK will be randomly generated.
|
|
#define | GAPROLE_SRK 0x302 |
| Signature Resolving Key. Read/Write. Size is uint8_t[KEYLEN]. Default is all 0, which means that the SRK will be randomly generated.
|
|
#define | GAPROLE_SIGNCOUNTER 0x303 |
| Sign Counter. Read/Write. Size is uint32_t. Default is 0.
|
|
#define | GAPROLE_BD_ADDR 0x304 |
| Device's Address. Read Only. Size is uint8_t[B_ADDR_LEN]. This item is read from the controller.
|
|
#define | GAPROLE_ADVERT_ENABLED 0x305 |
| Enable/Disable Advertising. Read/Write. Size is uint8_t. Default is TRUE=Enabled.
|
|
#define | GAPROLE_ADVERT_OFF_TIME 0x306 |
| Advertising Off Time for Limited advertisements (in milliseconds). Read/Write. Size is uint16_t. Default is 30 seconds.
|
|
#define | GAPROLE_ADVERT_DATA 0x307 |
| Advertisement Data. Read/Write. Max size is uint8_t[B_MAX_ADV_LEN]. Default is "02:01:01", which means that it is a Limited Discoverable Advertisement.
|
|
#define | GAPROLE_SCAN_RSP_DATA 0x308 |
| Scan Response Data. Read/Write. Max size is uint8_t[B_MAX_ADV_LEN]. Defaults to all 0.
|
|
#define | GAPROLE_ADV_EVENT_TYPE 0x309 |
| Advertisement Type. Read/Write. Size is uint8_t. Default is GAP_ADTYPE_ADV_IND (defined in GAP.h).
|
|
#define | GAPROLE_ADV_DIRECT_TYPE 0x30A |
| Direct Advertisement Address Type. Read/Write. Size is uint8_t. Default is ADDRMODE_PUBLIC (defined in GAP.h).
|
|
#define | GAPROLE_ADV_DIRECT_ADDR 0x30B |
| Direct Advertisement Address. Read/Write. Size is uint8_t[B_ADDR_LEN]. Default is NULL.
|
|
#define | GAPROLE_ADV_CHANNEL_MAP 0x30C |
| Which channels to advertise on. Read/Write Size is uint8_t. Default is GAP_ADVCHAN_ALL (defined in GAP.h)
|
|
#define | GAPROLE_ADV_FILTER_POLICY 0x30D |
| Filter Policy. Ignored when directed advertising is used. Read/Write. Size is uint8_t. Default is GAP_FILTER_POLICY_ALL (defined in GAP.h).
|
|
#define | GAPROLE_CONNHANDLE 0x30E |
| Connection Handle. Read Only. Size is uint16_t.
|
|
#define | GAPROLE_RSSI_READ_RATE 0x30F |
| How often to read the RSSI during a connection. Read/Write. Size is uint16_t. The value is in milliseconds. Default is 0 = OFF. Obsolete - Do not use.
|
|
#define | GAPROLE_PARAM_UPDATE_ENABLE 0x310 |
| Slave Connection Parameter Update Enable. Read/Write. Size is uint8_t. If TRUE then automatic connection parameter update request is sent. Default is FALSE.
|
|
#define | GAPROLE_MIN_CONN_INTERVAL 0x311 |
| Minimum Connection Interval to allow (n * 1.25ms). Range: 7.5 msec to 4 seconds (0x0006 to 0x0C80). Read/Write. Size is uint16_t. Default is 7.5 milliseconds (0x0006).
|
|
#define | GAPROLE_MAX_CONN_INTERVAL 0x312 |
| Maximum Connection Interval to allow (n * 1.25ms). Range: 7.5 msec to 4 seconds (0x0006 to 0x0C80). Read/Write. Size is uint16_t. Default is 4 seconds (0x0C80).
|
|
#define | GAPROLE_SLAVE_LATENCY 0x313 |
| Update Parameter Slave Latency. Range: 0 - 499. Read/Write. Size is uint16_t. Default is 0.
|
|
#define | GAPROLE_TIMEOUT_MULTIPLIER 0x314 |
| Update Parameter Timeout Multiplier (n * 10ms). Range: 100ms to 32 seconds (0x000a - 0x0c80). Read/Write. Size is uint16_t. Default is 1000.
|
|
#define | GAPROLE_CONN_BD_ADDR 0x315 |
| Address of connected device. Read only. Size is uint8_t[B_MAX_ADV_LEN]. Set to all zeros when not connected.
|
|
#define | GAPROLE_CONN_INTERVAL 0x316 |
| Current connection interval. Read only. Size is uint16_t. Range is 7.5ms to 4 seconds (0x0006 to 0x0C80). Default is 0 (no connection).
|
|
#define | GAPROLE_CONN_LATENCY 0x317 |
| Current slave latency. Read only. Size is uint16_t. Range is 0 to 499. Default is 0 (no slave latency or no connection).
|
|
#define | GAPROLE_CONN_TIMEOUT 0x318 |
| Current timeout value. Read only. size is uint16_t. Range is 100ms to 32 seconds. Default is 0 (no connection).
|
|
#define | GAPROLE_PARAM_UPDATE_REQ 0x319 |
| Slave Connection Parameter Update Request. Write. Size is uint8_t. If TRUE then connection parameter update request is sent.
|
|
#define | GAPROLE_STATE 0x31A |
| Reading this parameter will return GAP Peripheral Role State. Read Only. Size is uint8_t.
|
|
#define | GAPROLE_ADV_NONCONN_ENABLED 0x31B |
| Enable/Disable Non-Connectable Advertising. Read/Write. Size is uint8_t. Default is FALSE=Disabled.
|
|
#define | GAPROLE_BD_ADDR_TYPE 0x31C |
| Address type of connected device. Read only. Size is uint8_t.
|
|
#define | GAPROLE_CONN_TERM_REASON 0x31D |
| Reason of the last connection terminated event. Size is uint8_t.
|
|