TI BLE Stack API Documentation
2.03.05
|
Functions | |
bStatus_t | GAPCentralRole_StartDevice (gapCentralRoleCB_t *pAppCallbacks) |
Start the device in Central role. This function is typically called once during system startup. More... | |
bStatus_t | GAPCentralRole_SetParameter (uint16_t param, uint8_t len, void *pValue) |
Set a parameter in the Central Profile. More... | |
bStatus_t | GAPCentralRole_GetParameter (uint16_t param, void *pValue) |
Get a parameter in the Central Profile. More... | |
bStatus_t | GAPCentralRole_TerminateLink (uint16_t connHandle) |
Terminate a link. More... | |
bStatus_t | GAPCentralRole_EstablishLink (uint8_t highDutyCycle, uint8_t whiteList, uint8_t addrTypePeer, uint8_t *peerAddr) |
Establish a link to a peer device. More... | |
bStatus_t | GAPCentralRole_UpdateLink (uint16_t connHandle, uint16_t connIntervalMin, uint16_t connIntervalMax, uint16_t connLatency, uint16_t connTimeout) |
Update the link connection parameters. More... | |
bStatus_t | GAPCentralRole_StartDiscovery (uint8_t mode, uint8_t activeScan, uint8_t whiteList) |
Start a device discovery scan. More... | |
bStatus_t | GAPCentralRole_CancelDiscovery (void) |
Cancel a device discovery scan. More... | |
bStatus_t GAPCentralRole_CancelDiscovery | ( | void | ) |
Cancel a device discovery scan.
bStatus_t GAPCentralRole_EstablishLink | ( | uint8_t | highDutyCycle, |
uint8_t | whiteList, | ||
uint8_t | addrTypePeer, | ||
uint8_t * | peerAddr | ||
) |
Establish a link to a peer device.
highDutyCycle | - TRUE to high duty cycle scan, FALSE if not |
whiteList | - determines use of the white list: GAP White List Options |
addrTypePeer | - address type of the peer device: GAP_ADDR_TYPE_DEFINES |
peerAddr | - peer device address |
bStatus_t GAPCentralRole_GetParameter | ( | uint16_t | param, |
void * | pValue | ||
) |
Get a parameter in the Central Profile.
param | - profile parameter ID: GAP Central Role Parameters |
pValue | - pointer to buffer to contain the read data |
bStatus_t GAPCentralRole_SetParameter | ( | uint16_t | param, |
uint8_t | len, | ||
void * | pValue | ||
) |
Set a parameter in the Central Profile.
param | - profile parameter ID: GAP Central Role Parameters |
len | - length of data to write |
pValue | - pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type. |
bStatus_t GAPCentralRole_StartDevice | ( | gapCentralRoleCB_t * | pAppCallbacks | ) |
Start the device in Central role. This function is typically called once during system startup.
pAppCallbacks | - pointer to application callbacks |
bStatus_t GAPCentralRole_StartDiscovery | ( | uint8_t | mode, |
uint8_t | activeScan, | ||
uint8_t | whiteList | ||
) |
Start a device discovery scan.
mode | - discovery mode: GAP Device Discovery Modes |
activeScan | - TRUE to perform active scan |
whiteList | - TRUE to only scan for devices in the white list |
bStatus_t GAPCentralRole_TerminateLink | ( | uint16_t | connHandle | ) |
Terminate a link.
connHandle | - connection handle of link to terminate or GAP Special Connection Handles |
bStatus_t GAPCentralRole_UpdateLink | ( | uint16_t | connHandle, |
uint16_t | connIntervalMin, | ||
uint16_t | connIntervalMax, | ||
uint16_t | connLatency, | ||
uint16_t | connTimeout | ||
) |
Update the link connection parameters.
connHandle | - connection handle |
connIntervalMin | - minimum connection interval in 1.25ms units |
connIntervalMax | - maximum connection interval in 1.25ms units |
connLatency | - number of LL latency connection events |
connTimeout | - connection timeout in 10ms units |