CC26xx Driver Library
rfc_CMD_UPDATE_RADIO_SETUP_s Struct Reference

Update Radio Settings Command. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0001. More...
 
uint16_t __dummy0
 
uint32_t * pRegOverride
 Pointer to a list of hardware and configuration registers to override. More...
 

Detailed Description

Update Radio Settings Command.

Field Documentation

uint16_t rfc_CMD_UPDATE_RADIO_SETUP_s::__dummy0
uint16_t rfc_CMD_UPDATE_RADIO_SETUP_s::commandNo

The command ID number 0x0001.

uint32_t* rfc_CMD_UPDATE_RADIO_SETUP_s::pRegOverride

Pointer to a list of hardware and configuration registers to override.