#include <rf_ieee_cmd.h>
Data Fields | |
struct { | |
uint8_t corr:6 | |
The correlation value. More... | |
uint8_t bIgnore:1 | |
1 if the packet should be rejected by frame filtering, 0 otherwise More... | |
uint8_t bCrcErr:1 | |
1 if the packet was received with CRC error, 0 otherwise More... | |
} | status |
uint8_t rfc_ieeeRxCorrCrc_s::bCrcErr |
1 if the packet was received with CRC error, 0 otherwise
uint8_t rfc_ieeeRxCorrCrc_s::bIgnore |
1 if the packet should be rejected by frame filtering, 0 otherwise
uint8_t rfc_ieeeRxCorrCrc_s::corr |
The correlation value.
struct { ... } rfc_ieeeRxCorrCrc_s::status |