CC26xx Driver Library
I2SControlTable Struct Reference

A structure that defines an audio control table. Note: Memory for this structure must be initialized by user application. See detailed description! More...

#include <i2s.h>

Data Fields

uint16_t ui16DMABufSize
 Size of DMA buffer in number of samples. More...
 
uint16_t ui16ChBufSize
 Size of Channel buffer. More...
 
uint8_t ui8InChan
 Input Channel. More...
 
uint8_t ui8OutChan
 Output Channel. More...
 
uint16_t ui16MemLen
 Length of the audio words stored in memory. More...
 
uint32_t ui32InBase
 Base address of the input buffer. More...
 
uint32_t ui32InOffset
 Value of the current input pointer offset. More...
 
uint32_t ui32OutBase
 Base address of the output buffer. More...
 
uint32_t ui32OutOffset
 Value of the current output pointer offset. More...
 

Detailed Description

A structure that defines an audio control table. Note: Memory for this structure must be initialized by user application. See detailed description!

These fields are used by the I2S and normally it is not necessary for software to directly read or write fields in the table.

Note
The control table must be defined by the user as a global variable and the global pointer must then be assigned the address of the control table inside a user function (but before calling any I2S-function).
 I2SControlTable g_controlTable;    // Define global
 g_pControlTable = &g_controlTable; // Assign pointer (inside a function)

Field Documentation

uint16_t I2SControlTable::ui16ChBufSize

Size of Channel buffer.

Referenced by I2SBufferConfig(), I2SPointerUpdate(), and I2SSampleStampConfigure().

uint16_t I2SControlTable::ui16DMABufSize

Size of DMA buffer in number of samples.

Referenced by I2SBufferConfig(), I2SEnable(), and I2SPointerUpdate().

uint16_t I2SControlTable::ui16MemLen

Length of the audio words stored in memory.

Referenced by I2SAudioFormatConfigure(), and I2SPointerUpdate().

uint32_t I2SControlTable::ui32InBase

Base address of the input buffer.

Referenced by I2SBufferConfig(), I2SEnable(), and I2SPointerUpdate().

uint32_t I2SControlTable::ui32InOffset

Value of the current input pointer offset.

Referenced by I2SEnable(), and I2SPointerUpdate().

uint32_t I2SControlTable::ui32OutBase

Base address of the output buffer.

Referenced by I2SBufferConfig(), I2SEnable(), and I2SPointerUpdate().

uint32_t I2SControlTable::ui32OutOffset

Value of the current output pointer offset.

Referenced by I2SEnable(), and I2SPointerUpdate().

uint8_t I2SControlTable::ui8InChan

Input Channel.

Referenced by I2SChannelConfigure(), and I2SPointerUpdate().

uint8_t I2SControlTable::ui8OutChan

Output Channel.

Referenced by I2SChannelConfigure(), and I2SPointerUpdate().