#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_event.h"
#include "../inc/hw_adi.h"
#include "../inc/hw_adi_4_aux.h"
#include "../inc/hw_aux_anaif.h"
#include "rom.h"
Macros | |
#define | AUXADC_REF_FIXED (0 << ADI_4_AUX_ADCREF0_SRC_S) |
#define | AUXADC_REF_VDDS_REL (1 << ADI_4_AUX_ADCREF0_SRC_S) |
#define | AUXADC_FIFO_EMPTY_M (AUX_ANAIF_ADCFIFOSTAT_EMPTY_M) |
#define | AUXADC_FIFO_ALMOST_FULL_M (AUX_ANAIF_ADCFIFOSTAT_ALMOST_FULL_M) |
#define | AUXADC_FIFO_FULL_M (AUX_ANAIF_ADCFIFOSTAT_FULL_M) |
#define | AUXADC_FIFO_UNDERFLOW_M (AUX_ANAIF_ADCFIFOSTAT_UNDERFLOW_M) |
#define | AUXADC_FIFO_OVERFLOW_M (AUX_ANAIF_ADCFIFOSTAT_OVERFLOW_M) |
#define | AUXADC_TRIGGER_MANUAL (EVENT_AUXSEL0_EV_NONE) |
#define | AUXADC_TRIGGER_GPT0A (EVENT_AUXSEL0_EV_GPT0A) |
#define | AUXADC_TRIGGER_GPT0B (EVENT_AUXSEL0_EV_GPT0B) |
#define | AUXADC_TRIGGER_GPT1A (EVENT_AUXSEL0_EV_GPT1A) |
#define | AUXADC_TRIGGER_GPT1B (EVENT_AUXSEL0_EV_GPT1B) |
#define | AUXADC_TRIGGER_GPT2A (EVENT_AUXSEL0_EV_GPT2A) |
#define | AUXADC_TRIGGER_GPT2B (EVENT_AUXSEL0_EV_GPT2B) |
#define | AUXADC_TRIGGER_GPT3A (EVENT_AUXSEL0_EV_GPT3A) |
#define | AUXADC_TRIGGER_GPT3B (EVENT_AUXSEL0_EV_GPT3B) |
#define | AUXADC_TRIGGER_GPT0A_CMP (EVENT_AUXSEL0_EV_GPT0A_CMP) |
#define | AUXADC_TRIGGER_GPT0B_CMP (EVENT_AUXSEL0_EV_GPT0B_CMP) |
#define | AUXADC_TRIGGER_GPT1A_CMP (EVENT_AUXSEL0_EV_GPT1A_CMP) |
#define | AUXADC_TRIGGER_GPT1B_CMP (EVENT_AUXSEL0_EV_GPT1B_CMP) |
#define | AUXADC_TRIGGER_GPT2A_CMP (EVENT_AUXSEL0_EV_GPT2A_CMP) |
#define | AUXADC_TRIGGER_GPT2B_CMP (EVENT_AUXSEL0_EV_GPT2B_CMP) |
#define | AUXADC_TRIGGER_GPT3A_CMP (EVENT_AUXSEL0_EV_GPT3A_CMP) |
#define | AUXADC_TRIGGER_GPT3B_CMP (EVENT_AUXSEL0_EV_GPT3B_CMP) |
#define | AUXADC_SAMPLE_TIME_2P7_US 3 |
#define | AUXADC_SAMPLE_TIME_5P3_US 4 |
#define | AUXADC_SAMPLE_TIME_10P6_US 5 |
#define | AUXADC_SAMPLE_TIME_21P3_US 6 |
#define | AUXADC_SAMPLE_TIME_42P6_US 7 |
#define | AUXADC_SAMPLE_TIME_85P3_US 8 |
#define | AUXADC_SAMPLE_TIME_170_US 9 |
#define | AUXADC_SAMPLE_TIME_341_US 10 |
#define | AUXADC_SAMPLE_TIME_682_US 11 |
#define | AUXADC_SAMPLE_TIME_1P37_MS 12 |
#define | AUXADC_SAMPLE_TIME_2P73_MS 13 |
#define | AUXADC_SAMPLE_TIME_5P46_MS 14 |
#define | AUXADC_SAMPLE_TIME_10P9_MS 15 |
#define | AUXADC_FIXED_REF_VOLTAGE_NORMAL 4300000 |
#define | AUXADC_FIXED_REF_VOLTAGE_UNSCALED 1478500 |
Functions | |
void | AUXADCDisable (void) |
Disables the ADC. More... | |
void | AUXADCEnableAsync (uint32_t refSource, uint32_t trigger) |
Enables the ADC for asynchronous operation. More... | |
void | AUXADCEnableSync (uint32_t refSource, uint32_t sampleTime, uint32_t trigger) |
Enables the ADC for synchronous operation. More... | |
void | AUXADCDisableInputScaling (void) |
Disables scaling of the ADC input. More... | |
void | AUXADCFlushFifo (void) |
Flushes the ADC FIFO. More... | |
static void | AUXADCGenManualTrigger (void) |
Generates a single manual ADC trigger. More... | |
static uint32_t | AUXADCGetFifoStatus (void) |
Returns flags indicating the status of the ADC FIFO. More... | |
uint32_t | AUXADCReadFifo (void) |
Waits for and returns the first sample in the ADC FIFO. More... | |
uint32_t | AUXADCPopFifo (void) |
Returns the first sample in the ADC FIFO, without waiting. More... | |
static void | AUXADCSelectInput (uint32_t input) |
Selects internal or external input for the ADC. More... | |
int32_t | AUXADCGetAdjustmentGain (uint32_t refSource) |
Returns the gain value used when adjusting for ADC gain/offset. More... | |
int32_t | AUXADCGetAdjustmentOffset (uint32_t refSource) |
Returns the offset value used when adjusting for ADC gain/offset. More... | |
int32_t | AUXADCValueToMicrovolts (int32_t fixedRefVoltage, int32_t adcValue) |
Converts an "adjusted" ADC value to microvolts. More... | |
int32_t | AUXADCMicrovoltsToValue (int32_t fixedRefVoltage, int32_t microvolts) |
Converts a number of microvolts to corresponding "adjusted" ADC value. More... | |
int32_t | AUXADCAdjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset) |
Performs ADC value gain and offset adjustment. More... | |
int32_t | AUXADCUnadjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset) |
Performs the inverse of the ADC value gain and offset adjustment. More... | |